Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Craft a Festive LED Christmas Sweater Featuring the ATtiny416 -- Episode-634
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 21 Dec 2023 2:45 AM Date Created
  • Last Updated Last Updated: 21 Dec 2023 2:54 AM
  • Views 2481 views
  • Likes 10 likes
  • Comments 7 comments

Craft a Festive LED Christmas Sweater Featuring the ATtiny416 -- Episode-634

Hey, folks! In this super fun video, our buddy Mark Harris is taking the holiday spirit to a whole new level by blending colorful lights and those infamous ugly Christmas sweaters in an awesome E-Textiles project. Imagine a Christmas sweater decked out with custom LED boards – fun, right? Mark's got the lowdown on how to make it happen. It's all about good vibes and creativity! 

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Downloads and Links | Bill of Material | Discussion

image

Mark's on a mission to whip up a pocket-friendly blinky LED board with its own microcontroller. To do the job, he’s thinking about the Microchip ATtiny416, an affordable microcontroller with multiple PWM outputs for some seriously cool lighting effects. Mark jumps right into it, tackling the challenge of finding budget-friendly components, especially all the required LEDs. 

image

Next, Mark introduces a programming jig that makes it easy to test and program multiple boards. He also uses PlatformIO for Visual Studio Code, an extension that simplifies programming for both seasoned pros and those just dipping their toes into the maker waters. 

image

Now, for the fun part! Mark takes you step-by-step through the stitching process, which uses stainless steel conductive thread. He shares practical tips on thread spacing, dodging short circuits, and testing the LEDs. Even with the huge amount of time he invests in the intricate stitching, Mark stays positive, successfully creating a mesmerizing chasing LED display. 

image

As the video wraps up, Mark talks about how much his daughter loves the finished creation. He discusses future upgrades for a second version, teasing even more interactive features for those LED boards. This video isn't just a tutorial – it's an in-depth look into the world of festive wearables, inviting all the makers out there to jump in and create their own dazzling blinky LED boards! 

image

Downloads and Links:

  • Download CAD Files,  Code, and Schematics 

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
CAP CER 1UF 25V X7R 0603 Samsung 1 Buy Now
LED RGB MIXED 1.6(L)X1.6(W) MM Dialight 3 Buy Now
LED WHITE 1.6(L)X0.8(W) MM Dialight 1 Buy Now
IC MCU ATTINY416 8BIT 4KB FLASH 20VQFN Microchip 1 Buy Now
RES 330 OHM 1% 1/20W 0201 Panasonic 2 Buy Now
RES 150 OHM 5% 1/20W 0201 Panasonic 3 Buy Now
RES 10 OHM 1% 1/20W 0201 Panasonic 1 Buy Now
RES SMD 39 OHM 5% 1/20W 0201 Panasonic 6 Buy Now
Contact, Spring Probe, 2.54 mm, 60° Convex, 3 A, 33.3 mm Harwin 4 Buy Now
SBC, Arduino Nano, ATmega328, 8bit, 2KB RAM, 32KB Flash, 22 I/O pins Arduino 1 Buy Now
 

Additional Parts:

PCB Panel


element14 presents

element14 presents  | About Mark Harris |  Project Videos

  • Wearable Electronics Tutorial
  • Microcontroller E Textiles
  • Creative Conductive Thread Ideas
  • PlatformIO Visual Studio Code
  • Festive Wearable Tech
  • Holiday Maker Projects
  • ATtiny416 LED Design
  • Christmas Sweater LED Project
  • Blinking LED Board Tutorial
  • LED Project Tutorial
  • Ugly Sweater LED Lights
  • Festive Electronics Projects
  • Custom LED Board Programming
  • DIY LED Wearables
  • friday_release
  • Affordable LED Components
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 2 years ago +1
    So who's going to be first to create a multi-layer e-sweater ? It might be worth looking at embroidery stitching techniques and/or machine stitching to improve the conductivity. Also perhaps use strips…
Parents
  • beacon_dave
    beacon_dave over 2 years ago

    So who's going to be first to create a multi-layer e-sweater ?  Slight smile

    It might be worth looking at embroidery stitching techniques and/or machine stitching to improve the conductivity. Also perhaps use strips of  conductive fabric on the inside and stitch through it with the conductive thread. 

    It might also be worth embroidering the track layout onto a separate layer of fabric first and then place this on the inside of the sweater and then use the conductive thread as short vias to connect the LEDs to it. This should make it a lot easier to stitch as you can hold it in a frame and have access to front and back sides. Aligning the circuit fabric with the sweater for the final vias might be slightly tricky though. 

    Another thought is to perhaps embroider your own designs from scratch rather than to augment a existing knitted design. That way you can incorporate any necessary tracks into the design itself. (start with PCB art ?). You can get CNC embroidery machines which can likely lay down a lot of thread quickly and accurately to create intricate designs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 2 years ago

    So who's going to be first to create a multi-layer e-sweater ?  Slight smile

    It might be worth looking at embroidery stitching techniques and/or machine stitching to improve the conductivity. Also perhaps use strips of  conductive fabric on the inside and stitch through it with the conductive thread. 

    It might also be worth embroidering the track layout onto a separate layer of fabric first and then place this on the inside of the sweater and then use the conductive thread as short vias to connect the LEDs to it. This should make it a lot easier to stitch as you can hold it in a frame and have access to front and back sides. Aligning the circuit fabric with the sweater for the final vias might be slightly tricky though. 

    Another thought is to perhaps embroider your own designs from scratch rather than to augment a existing knitted design. That way you can incorporate any necessary tracks into the design itself. (start with PCB art ?). You can get CNC embroidery machines which can likely lay down a lot of thread quickly and accurately to create intricate designs.