Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Off-Grid Remote Generator Starter -- Episode-639
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 22 Jan 2024 3:30 PM Date Created
  • Last Updated Last Updated: 26 Jan 2024 3:04 PM
  • Views 3486 views
  • Likes 11 likes
  • Comments 11 comments

Off-Grid Remote Generator Starter -- Episode-639

Every once in a while, Kaleb’s generator needs a restart, which involves a trek outside. To minimize wading through the mud on rainy days, he decided to build a remote control that allows him to start and stop the generator, as well as display any relevant statistics. The project requires a microcontroller, relays, an LED display, and a handful of buttons and switches. Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

image

For the microcontroller, Kaleb opts for the Arduino Nano IoT 33, due to its Wi-Fi capabilities and ample IO. The four-digit displays, previously used in a clock project, are used to convey information. Driving the displays are MAX7221 LED controllers, known for their compatibility with Arduino and stackability. Kaleb also incorporates momentary switches for start and stop functions, along with a rocker switch to conserve power when the system is not in use. 

image 

The project involves two circuits – one for the house and another for the remote location near the generator. The house circuit includes buttons, LEDs, and a switch, while the remote circuit has relays to control the generator’s start and enable functions. Kaleb demonstrates the functioning of the system, which allows remote starting and stopping of the generator, displaying wattage generated, and other relevant information. 

image

In the code overview, Kaleb explains the key elements, including button handlers, MQTT communication, and display toggling. The code, along with design files, will be available on GitHub for the element14 Community. The completed project works successfully, giving Kaleb a convenient and efficient way to control the generator remotely, saving him from unpleasant treks out to the generator in unfavorable weather conditions. 

image

Downloads and Links:

  • Code and CAD Files: Episode 639 Resources  
  • Github Mirror:  https://github.com/KalebTheMaker/GeneratorRemote

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Arduino NANO IOT33 Wifi ABX00032 2 Buy Now
LED 7-SEG DISPLAY, COM CATHOD, GRN TDCG1060M 6 Buy Now
MAX7221ENG+ Display Dirver 8 digit MAX7221ENG+ 4 Buy Now
Rocker Switch SRJ22A3BBBNN 2 Buy Now
SWITCH, SPST-NO, 0.4A, 32VAC, ROUND, RED 59-112 4 Buy Now
 

element14 presents

element14 presents  |  About Kaleb |  Project Videos

  • Seven-segment display controls
  • Remote Start
  • Remote device management
  • Smart home generator control
  • Home automation innovations
  • Microcontroller IoT applications
  • Creative electronic solutions
  • Wireless generator operation
  • diy
  • Electronic circuitry for home use
  • Energy-efficient control system
  • generator
  • DIY IoT electronics
  • Innovative Arduino projects
  • arduino iot projects
  • Remote generator start
  • off-grid
  • arduino
  • e14p_KC
  • DIY remote device activation
  • Honda EU-7000is
  • friday_release
  • Generator automation technology
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • balajivan1995
    balajivan1995 over 2 years ago +1
    Nice article. Although some part of the code makes my eyes twitch. 1. if(gen_start) { Serial.println("Starting Generator"); digitalWrite(gen_start_pin, HIGH); digitalWrite(led_start, HIGH); } else if…
Parents
  • dougw
    dougw over 2 years ago

    I used to find studs by drilling small holes that can be easily filled when they miss...now I have a couple of stud finders, one of which actually works well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • KalebTheMaker
    KalebTheMaker over 2 years ago in reply to dougw

    Hi Doug, I *thought* I had a stud finder that I thought worked well, until it didn't! Oh well, I am going to fix that mess with a larger wooden plate I will make once I get the CNC router up. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • KalebTheMaker
    KalebTheMaker over 2 years ago in reply to dougw

    Hi Doug, I *thought* I had a stud finder that I thought worked well, until it didn't! Oh well, I am going to fix that mess with a larger wooden plate I will make once I get the CNC router up. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 2 years ago in reply to KalebTheMaker

    Well you will need space for the engine RPM and the fuel gage readout at some point...  Slight smile

    I've been watching contractors here turning a wall into 'Swiss cheese' trying to pull 70+ cables in through an older building. Hollow sounding walls have turned out to have a 5mm air gap and then concrete pillars or additional timber framing left by previous work behind them.