Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Make Your Own CNC Pyrography Wood Burner -- Episode 359
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 13 Sep 2018 2:16 PM Date Created
  • Last Updated Last Updated: 14 Sep 2018 7:24 AM
  • Views 2902 views
  • Likes 6 likes
  • Comments 3 comments

Make Your Own CNC Pyrography Wood Burner -- Episode 359

image
Make Your Own CNC Pyrography Wood Burner

element14 Presents  |  MAYER MAKES VCP Profile  |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Clem tries to convert his cheap tiny CNC machine that never really worked into an easy to use tool. The tiny CNC should use the same worflow and software like a standard 3d printer does. There is one rule that always applies, „ If you buy cheap random stuff from unknown sources- you are in for a bad time“ The Struggle is real, but the result is a CNC Woodburning machine!

 

 

Product NameManufacturerQuantity
Buy Kit

A000067 -  Development Board, Arduino Mega 2560, ATmega2560 MCU, 54 3.3V I/O, 16 Analogue Inputs, 4 UARTs

Arduino1Buy Now

TMCM-TRAMS -  Evaluation Board, Trinamic RepRap Arduino Mega Shield, 3D-Printers with TMC5130 Motor Controller

Trinamic1Buy Now



  • 3d printer
  • halloween 2018
  • woodburning
  • trinamic
  • e14presents_mayermakes
  • cura for cnc
  • cnc
  • arduino shield
  • vcp_arduino
  • ardexpert
  • element14 presents
  • evaluation board
  • atmega2560
  • arduino
  • friday_release
  • tmcm-trams
  • motor controller
  • arduino mega
  • mayermakes
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • phoenixcomm
    phoenixcomm over 7 years ago +1
    cool, but I need a foam cutter that can handle a 4x8 foot sheets and would have X/Y/Z normal axis, with maybe an additional axis for spindle tilt. Since my foam ranges from 1 to 4 inches in thickness,…
Parents
  • phoenixcomm
    phoenixcomm over 7 years ago

    cool, but I need a foam cutter that can handle a 4x8 foot sheets and would have X/Y/Z normal axis, with maybe an additional axis for spindle tilt. Since my foam ranges from 1 to 4 inches in thickness, I will most likely have to hold the foam down with some sort of vacuum system, and a separate vacuum for sucking up the blizzard of snow!

    It would also be nice to have two spindles on two different gantries so that I can cut this at a) twice the speed b) two items at the same time.

    Why the 4x8 requirement? Its used in experimental aircraft construction. image

    If you want to double down on this hardware there are "pin-locks", powered by air that can be mounted on the gantry to remove the spindle and the mounts. then replace it with maybe a laser? or a drill, etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 7 years ago

    cool, but I need a foam cutter that can handle a 4x8 foot sheets and would have X/Y/Z normal axis, with maybe an additional axis for spindle tilt. Since my foam ranges from 1 to 4 inches in thickness, I will most likely have to hold the foam down with some sort of vacuum system, and a separate vacuum for sucking up the blizzard of snow!

    It would also be nice to have two spindles on two different gantries so that I can cut this at a) twice the speed b) two items at the same time.

    Why the 4x8 requirement? Its used in experimental aircraft construction. image

    If you want to double down on this hardware there are "pin-locks", powered by air that can be mounted on the gantry to remove the spindle and the mounts. then replace it with maybe a laser? or a drill, etc.