Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Macroscope Soldering Tool -- Episode 379
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 19 Dec 2018 4:12 AM Date Created
  • Last Updated Last Updated: 1 Feb 2019 8:24 AM
  • Views 3160 views
  • Likes 8 likes
  • Comments 8 comments

Macroscope Soldering Tool -- Episode 379

image
Macroscope Soldering Tool

element14 Presents  |  MAYER MAKES VCP Profile  |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

It is hard to solder tiny components while filming it. To proved better footage for YOU  the viewers, Clem builds a CNC controlled machine that allows him to solder without having to touch the workpiece or the soldering Iron himself. The Foundation for a fully automated soldering robot!

 

Bill of Material:

 

PartManufacturerQuantityBuy Kit

Arduino Uno

ARDUINO1Buy Now

Arduino Nano

ARDUINO1Buy Now
Silentstepstick Breakout boardTRINAMIC3Buy Now
Stepper Motor, High Torque, DC, 0.09 N-m, 1.4 A, Two Phase, 2 ohm, 1.6 mHNANOTEC3Buy Now
Soldering Gun Kit, Gun, Desoldering Pump, Safety Stand, SolderDURATOOL1Buy Now
oystick, 2, 6 A, 250 V, 4 PositionAPEM1Buy Now
Pushbutton Switch, Off-(On), SPST-NC, 115 V, 28 V, 5 A, SolderOTTO Controls1Buy Now
Protoboard, RBP Strip, Epoxy Paper, 100mm x 220mmCIF1Buy Now

 

Additional Parts:

 

Product Name

CNC shield by Protoneer

Cheap Crosstable bought at a  hardware store

Attachments:
Bonus Content_E379.zip
  • e14presents_mayermakes
  • macroscope soldering tool
  • friday_release
  • mayermakes
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • ghinessey
    ghinessey over 7 years ago +2
    can you automate it to work with a sensor to keep it focused on the work while staying out of your way
  • DAB
    DAB over 7 years ago +2
    Great Build Clem. I have a similar use for an X,Y,Z stage to capture micro-photographs, so I was very happy to see your build. thanks DAB PS, I would like to see an automated soldering robot built out…
  • mayermakes
    mayermakes over 7 years ago in reply to DAB +1
    I also was thinking of using it for focus stacking in macro photography!
Parents
  • msebok
    msebok over 7 years ago

    With the lever action on the soldering tip, are you noticing any solder leaving the tip as it lifts? It would be a shame if a blob ended up elsewhere on your work piece or camera lens after going to this trouble.

     

    Awesome build!

     

     

    ..never mind just watched it again and it didn't look like the tip was moving as fast as I thought it was..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • msebok
    msebok over 7 years ago

    With the lever action on the soldering tip, are you noticing any solder leaving the tip as it lifts? It would be a shame if a blob ended up elsewhere on your work piece or camera lens after going to this trouble.

     

    Awesome build!

     

     

    ..never mind just watched it again and it didn't look like the tip was moving as fast as I thought it was..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mayermakes
    mayermakes over 7 years ago in reply to msebok

    it is moving pretty slow, but of course if you overload on solder a blob might leave it anyway.
    the key is to be conservative on adding solder. depending on the application I use it manually or automated(depending on if I have a hand free)