Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Raspberry Pi Stop Motion Machine -- Episode 395
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 19 Dec 2018 5:40 AM Date Created
  • Last Updated Last Updated: 24 May 2019 7:24 AM
  • Views 5815 views
  • Likes 7 likes
  • Comments 23 comments

Raspberry Pi Stop Motion Machine -- Episode 395

image
Raspberry Pi Stop motion Machine

element14 Presents | MAYER MAKES' VCP Profile | Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Clem dreams of making his own Stop motion movie, just like the claymation films he loved as a kid. But creating these kinds of movies is very difficult and tedious. So he builds a machine that makes it much easier, is controlled with his smartphone and even moves on its own to make the stunning Hollywood shots he dreams of!

 

 

Bill of Materials

 

Product NameManufacturerQuantityBuy Kit
Raspberry Pi 3 A+Raspberry pi1Buy Now
TQ2-3V Relaypanasonic2Buy Now
TMC2208 SILENTSTEPSTICKTrinamic/Watterott2Buy Now
Din 5 Plug MA 50 SHirschmann1Buy Now
Din 5 Connector MA 50 SHirschmann3Buy Now
2214S-40SG-85 -  CONNECTOR, RCPT, 40POS, 2.54MMMulticomp1Buy Now
INTEGRAL  Integral 16gb MicroSD Card with AdapterINTEGRAL/ utility+1Buy Now
NANOTEC  Stepper Motor, High Torque, DC, 0.28 N-m, 1.8 A, Two Phase, 1.1 ohm, 1.85 mHNANOTEC2Buy Now
XP POWER  AC/DC Power Supply, ITE, 2 Output, 42 W, 5 V, 5 A, 12 V, 2 AXP POWER1Buy Now

 

 

Additional Parts:

 

Product NameQuantity
DSLR Camera (Nikon D3300)1
Remote Control for the Camera1

Aluminum Extrusion Scrap Piece

1
Attachments:
SupplementalContent.zip
  • krita animation tutorial for beginners
  • film look
  • animation
  • krita
  • timelapse
  • how to export animation in krita
  • dslr stopmotion
  • photoshop
  • how-to
  • how to animate
  • stop-motion
  • how to get the filmlook
  • e14presents_mayermakes
  • paper-cutout animation
  • how to animta
  • the neverhood
  • basics of stopmotion
  • how to do stop motion
  • raspberry pi
  • ecogeeks
  • stopmotion tutorial
  • stop motion
  • claymation
  • how to make a movie
  • camera
  • object-motion
  • stopmotion
  • filmmaking
  • pixilation
  • friday_release
  • nikon
  • rob nelson
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 7 years ago in reply to mayermakes +4
    You may want to take a look at some of the Kessler equipment for ideas/inspiration: e.g. Shuttle Dolly + CineDrive: https://vimeo.com/237424857 Website at: https://www.kesslercrane.com/cinedrive
  • thedanaaddams
    thedanaaddams over 7 years ago +3
    Okay, this is awesome, and an incredible start! As a professionally trained animator and film graduate, I have a number of suggestions for improvement which could take it from great, to a pro-grade tool…
  • fmilburn
    fmilburn over 7 years ago +2
    Hi Clem, I have been thinking of doing something along these lines but you have far exceeded what I had in mind. Extremely well done... Frank
Parents
  • thedanaaddams
    thedanaaddams over 7 years ago

    Okay, this is awesome, and an incredible start!

    As a professionally trained animator and film graduate, I have a number of suggestions for improvement which could take it from great, to a pro-grade tool that self-produced stop motion animators would actively want to use!

     

    You've got a dolly which is great - from there, you would want a riser with a boom arm to put the camera on.

     

          x|________C

            |

            |

    ---O-------O---

     

    So, you want the boom arm to move up and down on the riser. (Rack & pinion system?)

    The riser mast should rotate to swing the arm around.

    At the point x, where the boom arm meets the riser mast, you want it to rotate to crane up and down.

    The boom arm should also be able to extend and retract to telescope in and out.

    Point C is where the camera rests, and should have its own pan and tilt to rotate left/right and up/down.

     

    I also think that instead of a smartphone interface, physical controls would be better - perhaps the wireless connection could be used to relay the viewfinder to a viewing monitor?

    Most stop motion cameras I've seen have been rigged up to take the shot with a stomp switch, like you might use in a guitar FX pedals setup.

     

    Also, regarding your setup of the framerates... technically, that's not how it should be done - you're always producing your animation at either 24fps (film), 25fps (PAL TV), or 30fps (NTSC TV).

    If you see reference to "12fps" for example, that is a matter of duplicate frames - in animation, we use terms like "on ones" and "on twos" to refer to how many times a single unchanged frame is captured for playback at the target framerate.

    Really, you want to have a choice of those framerates, and take duplicate frames manually, or enable options to take multiples by default, with the option to adjust multiples on the fly. (Since in animation, we don't just stick to twos for everything - we typically switch between twos and ones as the action requires.)

     

    A really nice feature to have would be a way to define a start and end position for the camera mechanism (to block out your shots to the storyboard) then set an amount of time between the start and end points, and advance the position per frame along customised spline paths for each axis, to allow for easing into and out of the defined points.

    It could even allow complex and beautiful camera motions to be perfected and defined before any puppet animation begins, leaving you free to focus on that aspect of the art when the camera is locked in and ready!

     

    Hopefully this wall of text doesn't seem too nitpicky; again, this is a really awesome start, but I can see so much potential for an incredible professional-grade tool, here!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to thedanaaddams

    Hi Dana, thank you very much fro your feedback!

    The design currently supports two axis automated movement, you can choose whatever axis fits your need and just attach stepper and belts there(on any kind of crane, slider ,dolly or whatever you prefer)
    I originally wanted to use a jib but a dolly seemed more relateable to most viewers.

     

    I chose the smartphone controls because it is very flexible and free to position away from the camera. My first iteration had a stomp switch but I removed it to avoid ramping up the partcount (i want to keep the cam and RPI isolated to avoid damage)

     

    On framerate: interesting insight into your realsm! thanks, I just added common framerates without much concern. (jsut looked up common framerates in animation on google)

     

    I'd love to develop this project into a pro-grade tool, all the features you mentioned coan be implemented it is just a matter of adapting the code.
    Please share the page with your peers in animation/film,
    the code is free to download under the video and I will likely create a repo for collaborative developement.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • thedanaaddams
    thedanaaddams over 7 years ago in reply to mayermakes

    Glad my info could help!
    Really excited to see where this goes from here!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • thedanaaddams
    thedanaaddams over 7 years ago in reply to mayermakes

    Glad my info could help!
    Really excited to see where this goes from here!