Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents First Person View RC Car with PS1 Steering Wheel -- Episode 391
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 2 Mar 2019 7:05 PM Date Created
  • Last Updated Last Updated: 26 Apr 2019 7:24 AM
  • Views 8458 views
  • Likes 11 likes
  • Comments 34 comments

First Person View RC Car with PS1 Steering Wheel -- Episode 391

image
First Person View RC Car with PS1 Steering Wheel

element14 presents  |  MAYER MAKES' VCP Profile |  Project Videos

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Clem scored a broken Steering Wheel for the PlayStation 1 (yes the first one) at a flea market.Thankfully it is broken so he decided to turn it into an RC transmitter for his old Remote controlled Car! Learn how to use the Arduino MKR Wifi 1010 to make your own Transmitter and Receiver from scratch! It even supports FPV head tracking! What features would you like to add into the system? Tell us here in the discussion thread.

 

 

Extended cuts of the racing footage:

  • Real Life Initial D FPV RC Racing
  • FPV RC Night Rallye

 

Bill of Materials

 

Product NameManufacturerQuantityBuy Kit
Arduino MKR wifi 1010ARDUINO2Buy Now
Linear Voltage RegulatorOn Semiconductor1Buy Now

 

 

 

Additional Parts:

 

Product Name/Description
RC Car  ( Cars used in the Episode: Hirobo Rock‘n Vega witch Toyota Levin body  / AMR Mini Scud with Mini Cooper Body)
The glue used to repair the plastic parts is Aprintapro Printaglue (designed to glue 3d printed parts)
Attachments:
FPVCarUDPHost.zip
FPVCarUDPReceiver.zip
  • fpv
  • episode 391: first person view rc car with ps2 steering
  • e14presents_arduino1010
  • e14presents_mayermakes
  • car racing
  • e14 presents mkr 1010
  • arduino
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Sean_Miller
    Sean_Miller over 7 years ago +3
    Clem, great work on this one from both a production and a build. You've really got your coding notched up. XBee devices may be of interest to you as well. That tech let's you get some major distances …
  • DAB
    DAB over 7 years ago in reply to mayermakes +3
    Hi Clem, Have you considered adding GPS and then put up a navigation screen on the video? When you go FPV, you sometimes lose track of where you are so that you can return safely. DAB
  • mcherry
    mcherry over 7 years ago +3
    Cool Stuff. Next step is to add some force-feedback to the steering wheel using and Accelerometer and Gyroscope in the RC Car and some motors in the wheel to mimic the surface that the car is running on…
Parents
  • zheng97hong
    zheng97hong over 6 years ago

    I am now doing a similar project, however the steering wheel, paddle and break is connect to pc. Is there any chance to send the signal from pc to wifi 1010?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 6 years ago in reply to zheng97hong

    yes,there is.

    I suppose they are USB devices, If so you can pipelione the commands over the pc to an Arduino also connected  per usb.
    this would need soem custo mcode running on the PC, but you might already find some code that reads out usb data form a steering wheel.

     

    the other version is to read the Wheels data directly either liek I did in the video or using a USB host shield and reverse engineer the protocoll (there might be a library already for some wheels)

    If you want to be quick I'd suggest doing like I did in the video, but if you want to keep the wheel unchanged, there is more work involved.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 6 years ago in reply to zheng97hong

    yes,there is.

    I suppose they are USB devices, If so you can pipelione the commands over the pc to an Arduino also connected  per usb.
    this would need soem custo mcode running on the PC, but you might already find some code that reads out usb data form a steering wheel.

     

    the other version is to read the Wheels data directly either liek I did in the video or using a USB host shield and reverse engineer the protocoll (there might be a library already for some wheels)

    If you want to be quick I'd suggest doing like I did in the video, but if you want to keep the wheel unchanged, there is more work involved.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • zheng97hong
    zheng97hong over 6 years ago in reply to mayermakes

    Thanks for the reply and advise, the project I am working right is involve game engine so I think I will stick to the USB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 6 years ago in reply to zheng97hong

    In that case you may want to lok out around GameDev foruims as they usually have software to monitor USB (gamepad/keyboard/(mouse)) commands in realtime to measure latency and debug. so you might be able to just use one of those tools and repeat every command over another USB serial port to get it to the MKR Wifi