Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents The Ultimate Raspberry Pi Stress Test -- Episode 400
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 2 Mar 2019 7:11 PM Date Created
  • Last Updated Last Updated: 28 Jun 2019 7:24 AM
  • Views 3904 views
  • Likes 6 likes
  • Comments 7 comments

The Ultimate Raspberry Pi Stress Test -- Episode 400

image
The Ultimate Raspberry Pi Stress Test

element14 presents  |  AirborneSurfer's VCP Profile |  Project Videos

 

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

We all know how the Raspberry Pi is a great little gem of a single-board computer--a "Jeep" of a board that can go nearly anywhere and does nearly anything--but how well does it work under these abusive conditions? Are the Raspberry Pi's advertised specs accurate? How well will the Raspberry Pi perform in "The Real World"? In this video, Matt puts the Raspberry Pi through a series of grueling tests designed to push it to its operational limits and see just how well it performs under pressure...and fire...and cold.

 

  • Episode 354: Tiny Vacuum Forming Machine

 

Bill of Materials

 

 

Product Name Manufacturer Quantity Buy Kit
RPI3-MODBP - Single Board Computer, Raspberry Pi 3 Model B+, BCM2837B0 SoC, IoT, PoE Enabled Raspberry Pi 4 Buy Now

 

 

Additional Parts:

 

Product Name Quantity
Liquid Nitrogen 1
Propane Torch 1

Hydraulic Press(12 ton)

1
  • raspberry pi stress test
  • e14presents_airbornesurfer
  • raspberry pi gauntlet
  • raspberry pi operational limitations
  • raspberry pi operating temperature
  • raspberry pi
  • raspberry pi operating limits
  • element14 presents
  • raspberry pi radioactive
  • e14p_MAS
  • raspberry pi liquid nitrogen
  • raspberry pi 3b+ temperature limits
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • airbornesurfer
    airbornesurfer over 7 years ago +1
    Now that we're versed on the Pi 3's operating limits, how do you think it compares to the Pi 4?
Parents
  • shirokuma
    shirokuma over 7 years ago

    Relay interesting video - I enjoy seeing equipment being pushed to its limits. I've spent a bunch of my career in testing and qualifying electronics for use in electrical substation environments, and I've made more than one manufacturer cry by the end of testing image

     

    Some tests that I think are relatively easy to be done in the home shop...

    • Power up from cold soak. It's one thing to cool down a piece of electronic kit that's already running; it's a totally different thing to power the unit down, let it drop to a low temperature, and then turn it on. There are all sorts of problems that can arise with the sequencing of various power rails that can really cause havoc with a cold-start power up. Put the RPi into the liquid nitrogen bath with the power off, let it sit for a bit to let it reach steady state temperature (or as cold as you're willing to try), and then turn the power on.
    • High altitude simulation: Put the RPi in a vacuum chamber and drop the ambient pressure as low as it will go.
    • High magnetic field: Big, tight coil of wire with lots of turns per meter, with a RPi in the centre, rotated through different orthogonal orientations. Try low frequency (50-60 Hz - easy with a wall supply) and if possible, higher frequencies (e.g. 400 Hz - typical shipboard/marine applications) although it might be difficult to get a power supply to do 400 Hz. Wait a minute - this is Element14...
    • Torsional board loading: Rather than a "uniform" pressure across the board, try different bending/twisting loads. Cantilever the board over the edge of a table and try hanging progressively heavier weights either from both corners or a single corner. Looking for solder cracking or PCB trace delamination.
    • Shake...: See if you can bodge together a simple vibration table (Orbital sander, sawzall, or ideally a couple of pieces of heavy plate steel, some heavy duty springs, and a reciprocating motor). Bolt the RPi to it (again, different orthogonal mounting orientations) and see what shakes loose.
    • ...And Bake: Get a toaster oven, set the temperature to 150-200C, put a couple of RPis in and see how long they will run until failure - long reliability is important too, and this gives at least some gauge as to how long a RPi would last under more typical environmental conditions (we typically require a hot soak of 16 hours at 85C as part of a Highly Accelerated Stress Screen (HASS) protocol for equipment prior to shipping to weed out any infant mortality).

     

    Also,  I think the increased temperature in your radiation test is just the combination of poor coefficient of heat transfer between the CPU and GPU cases and the paper towel (instead of air), and the loss of pretty much all convective cooling of the components from the restricted airflow. If you didn't have any of the tests failing (particularly the memory test) it's unlikely that radiation had anything to do with the temperature rise. Simple way to prove this would be to use a block of pretty much anything else (non-radioactive) in lieu of the ADF with the same paper towel and see the result.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • airbornesurfer
    airbornesurfer over 7 years ago in reply to shirokuma

    Thanks! I know that there's a ton of other tests I could do to this (or, really, any) board, so perhaps a follow-up is in order?

     

    I think you're probably right about the temperature rise during the radiation test. If I try it again, I'll likely build a small rig to suspend the source above the board and run more memory-intensive tests for that particular battery. I expected some temperature difference with the paper towel in place, but I hadn't anticipated that much, which is probably the reason for my surprise more than the (lack of) effect of radiation bombardment. Hooray peer review! image

     

    My shopmate just built a Lego sorter based on a reciprocating motor, so it might be a good opportunity to perform those shake tests.

     

    Stay tuned....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • L14
    L14 over 3 years ago in reply to airbornesurfer

    Hello:

    Nice project, but ...

    Just *where* is the link to the test script?

    Cannot seem to find it, not in the description (?).

    Thanks in advance.

    Best,

    L14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to L14

    While it isn't available as a downloadable script, you can recreate it from the 1080p video footage https://youtu.be/1bgkInAIG7Y?t=112 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • cstanton
    cstanton over 3 years ago in reply to L14

    While it isn't available as a downloadable script, you can recreate it from the 1080p video footage https://youtu.be/1bgkInAIG7Y?t=112