Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Multi-Line Telephone Intercom -- Episode 392
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: rjena
  • Date Created: 30 Apr 2019 4:30 PM Date Created
  • Last Updated Last Updated: 3 May 2019 7:24 AM
  • Views 12266 views
  • Likes 10 likes
  • Comments 20 comments

Multi-Line Telephone Intercom -- Episode 392

image

Multi-Line Telephone Intercom

element14 Presents  |   Derek Brodeur's VCP Profile  |  Project Videos

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Modern smart phones have become so ubiquitous these days that old analog phones are getting left in the dust. However, you may still have a few of these old phones hanging around your house collecting cobwebs or you may have seen some lingering on the shelves at your local thrift shop. Now’s your chance to put them to good use. In this video, Derek takes you back to a time when stretching a phone cord across the room was the norm by creating a 4-line telephone intercom system with basic ringing capability. The circuit surrounds a DTMF decoder IC which handles keypress detection, a simple AC inverter to handle the ringing and a current source which allows analog communication between multiple phones.

 

 

Bill of Materials

 

Product Name Manufacturer Quantity Buy Kit
0.1uF 25v Capacitor 5 Buy Now
1uF 50v Capacitor 2 Buy Now
20pF Capacitor 2 Buy Now
2.2uF 250V Capacitor 1 Buy Now
1N4001 Diode 5 Buy Now
IRF540N N-Channel MOSFET 2 Buy Now
2N2904 NPN Transistor 5 Buy Now
HT9170D DTMF Decoder Holtek 1 Buy Now
CD4047 Multivibrator Texas Instruments 1 Buy Now
DC/DC Converter 5v / 1A RECOM 1 Buy Now
LM317T Adjustable Voltage Regulator ON Semiconductor 1 Buy Now
3.579545MHz Crystal ABL 1 Buy Now
DPDT Relay OMRON 5 Buy Now
75k 1/4 Watt Resistor 1 Buy Now
220 Ohm 1/4 Watt Resistor 2 Buy Now
22 Ohm 1/4 Watt Resistor 1 Buy Now
56k 1/4 Watt Resistor 2 Buy Now
100k 1/4 Watt Resistor 1 Buy Now
150k 1/4 Watt Resistor 1 Buy Now
68k 1/4 Watt Resistor 1 Buy Now
1k 1/4 Watt Resistor 5 Buy Now
300k 1/4 Watt Resistor 1 Buy Now

 

 

Additional Parts:

 

Product Name Quantity
RJ11 Telephone Jack - right angle 5
120V / 18V Center Tap Transformer 1
Prototyping PCB 2
PCB Standoffs + Screws 4
Metal Enclosure 1
SOP-20 Breakout board 1
Attachments:
image Derek Brodeur - Schematic.pdf
  • derek_episode
  • derek_brodeur
  • plain old telephone
  • e14presents_derekbrodeur
  • multi-line
  • intercom
  • telephone intercom
  • telephone
  • pots intercom
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 7 years ago +1
    I thought it was appropraite your block diagram has a current source in it. Also, I think I forgot how to DTMF worked! I knew there two tones, but I didn't know they are determined by the phone pad's matrix…
  • adedayoolumide
    adedayoolumide over 7 years ago +1
    Am a student I need your help in how to make this as a project, so I need you to put me though and some journal I can read about to make the project possible. THANKS
  • e14 Contributor
    e14 Contributor over 4 years ago in reply to shabaz

    Thank you for pointing this error out. You are correct, and it will be addressed shortly!

    -Derek

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to shabaz

    I can't edit the comment, but sorry I meant R4,  not R22. R4 is 22 ohm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jprochniak
    jprochniak over 4 years ago in reply to shabaz

    Thanks for clarifying all of that. I really appreciate it!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to jprochniak

    Hi,

    From what I can tell (I've only looked at the circuit for a minute or two):

    1. I feel this isn't an error, it is normal for analog systems to have a subscriber-to-circuit ratio that doesn't allow all possible callers to be able to connect simultaneously. It's like when you dial from a landline, and you hear a busy tone - that doesn't necessarily mean the remote side is using the phone (although usually that is the case), it can also mean that there are no spare circuits for your call to go through, because many other people are using their phones. This design has one circuit for up to 4 phones, which seems reasonable. It just means that if the circuit is in use, then the third person will need to wait. All other things being equal, it would be only a 33 percent chance anyway, that the third person wished to contact the only remaining person who isn't already in a call.

    2. The resistor R22 controls that, but actually it's set to about 55mA from what I can tell, not 75 mA. If you increase R22 slightly, then it will reduce the current. I think it will be fine as-is, but I'm not super-familiar with this area unfortunately.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jprochniak
    jprochniak over 4 years ago in reply to shabaz

    After doing a bit of digging, that's kind of what I figured. Thanks! I also saw the following comments with the YouTube posting of this video:

    1. This project is a beautiful but an error is hidden in the circuit of this multi-line telephone. Here is the error: phone 4 calls phone 2 and at the same time phone 4 is communicating with phone 2, calls phone 1, phone 3. For telephones 1 and 3 the line is occupied by telephones 4 and 2. and they cannot communicate at the moment With this circuit only 2 telephones can be called and the other telephones are blocked until the end of the calls of telephone 4 and telephone 2 In order for it to have two instantaneous communications at the same time, the circuit should be modified; and

    2. 75mA output is a little hot. Standard lines are spec'd at 32-37. Too hot and you can burn up components in the phones. Probably won't hurt the old electro mechanical phone, but those electronic phones and cordless phones won't like 75mA for too awful long.

    Any validity to these? My knowledge of component-level electronics is basically non-existent so I have no way of chasing these claims down one way or the other.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to jprochniak

    Hi, it looks like a typo, it will be 2N3904, because that's an NPN transistor in the schematic (the 2N2904 part code is for PNP, which this circuit isn't designed for).

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jprochniak
    jprochniak over 4 years ago

    Can you confirm which transistor should be used? The BOM calls for 2N2904 but the schematic calls out a 3N3904.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zylvancelestion
    zylvancelestion over 5 years ago

    I don’t really know what I’m doing when it comes to electronics and I’m not sure where to source all of these materials as it says some are unavailable but if I can find them all I’m sure going to try! Now if only I could figure out how to build something like this but with a toggle switch system that overrides the need for keypads and DTMF tones  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • a3a21971
    a3a21971 over 5 years ago

    I have moved into an apartment with a phone system intercom. The system doesn’t work because I am to acquire a home phone line which I assume provides the power to the system. Connecting my phone tracer which provides the cct with 9v which allows me to hear  button pushing at the front door intercom but not enough to provide a ring or voice.

    would you recommend this cct to provide the Ring for my phone for the front door to call my suite?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bkay
    bkay over 5 years ago

    Hello everyone. This is 2021 and I'm trying to make this as my project, but I have a few questions.
    First, a 110v transformer doesn't seem to be available as we use 220/240v. What do you all think i can do?
    Secondly, for the ringer circuit, can all phones take in the 100v AC?

    I'm using the Panasonic  kx-t2375 telephone.

    Thank you all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>