Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY Toothbrush Timer -- Episode 480
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 30 Dec 2020 2:51 PM Date Created
  • Last Updated Last Updated: 8 Jan 2021 8:24 AM
  • Views 5878 views
  • Likes 7 likes
  • Comments 13 comments

DIY Toothbrush Timer -- Episode 480

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Do you make sure you brush for 2 minutes each time you brush your teeth? Today I’m making a timer to ensure I do! However rather than just coding it on a dev board, why not do it entirely microcontroller free and design it as a circuit using 555s and 74 series logic?

Bill of Material:

Product Name Manufacturer Quantity Buy KitBuy Kit
 IC, TIMER, 555, PDIP8 TEXAS INSTRUMENTS 1 Buy Now
Shift Register, 74HC594, Serial to Parallel, 1 Element, 8 bit, DIP, 16 Pins TEXAS INSTRUMENTS 2 Buy Now
Logic IC, Inverter, Hex, 1 Inputs, 14 Pins, DIP, 74HC04 TEXAS INSTRUMENTS 1 Buy Now
Signal Relay, 3 VDC, DPDT, 2 A, P2/V23079 Series, Through Hole, Latching Dual Coil AXICOM - TE CONNECTIVITY 1 Buy Now
2N3904, Bipolar (BJT) Single Transistor, NPN, 40 V, 200 mA, 625 mW, TO-92, Through Hole MULTICOMP PRO 1 Buy Now
 LED, Red, Through Hole, T-1 3/4 (5mm), 20 mA, 2.1 V, 630 nm CREE 12 Buy Now
Industrial Pushbutton Switch, 15.2 mm, SPST, Off-(On), Round, Blue MULTICOMP PRO 1 Buy Now
MF25 2K7, Through Hole Resistor, 2.7 kohm, MF25 Series, 250 mW, ± 1%, Axial Leaded, 250 V MULTICOMP PRO 12 Buy Now
MF25 3K, Through Hole Resistor, 3 kohm, MF25 Series, 250 mW, ± 1%, Axial Leaded, 250 V MULTICOMP PRO 1 Buy Now
Through Hole Resistor, 1 kohm, MCRE Series, 125 mW, ± 5%, Axial Leaded, 200 V MULTICOMP PRO 1 Buy Now
MCF 0.25W 10K, Through Hole Resistor, 10 kohm, MCF Series, 250 mW, ± 5%, Axial Leaded, 250 V MULTICOMP PRO 4 Buy Now
 Through Hole Resistor, 3 Mohm, MRS25 Series, 600 mW, ± 1%, Axial Leaded, 350 V VISHAY 1 Buy Now
Electrolytic Capacitor, 4.7 µF, 35 V, MCGPR Series, ± 20%, Radial Leaded, 2000 hours @ 85°C MULTICOMP PRO 1 Buy Now
Electrolytic Capacitor, 10 µF, 35 V, MCGPR Series, ± 20%, Radial Leaded, 2000 hours @ 85°C MULTICOMP PRO 1 Buy Now
Multilayer Ceramic Capacitor, 0.1 µF, 50 V, Mono-Kap Series, ± 10%, Radial Leaded, X7R VISHAY 5 Buy Now
Multilayer Ceramic Capacitor, 10000 pF, 50 V, Goldmax, 300 Series, ± 10%, Radial Leaded, X7R KEMET 1 Buy Now
1N4001+, Standard Recovery Diode, 50 V, 1 A, Single, 1.1 V, 30 A MULTICOMP PRO 2 Buy Now
IC & Component Socket, 8 Contacts, DIP Socket, 2.54 mm, 2227MC Series, 7.62 mm, Phosphor Bronze MULTICOMP PRO 1 Buy Now
 IC & Component Socket, 16 Contacts, DIP Socket, 2.54 mm, 2227MC Series, 7.62 mm, Beryllium Copper MULTICOMP PRO 2 Buy Now
IC & Component Socket, 14 Contacts, DIP Socket, 2.54 mm, 2227MC Series, 7.62 mm, Beryllium Copper MULTICOMP PRO 1 Buy Now
LED Housing, 9.5 mm x 12.5 mm, Black, Plastic, 5mm / T1 3/4 LEDs KINGBRIGHT 12 Buy Now
Plastic Enclosure, Multipurpose, Plastic, 120 mm, 80 mm, 59 mm, IP54 HAMMOND 1 Buy Now
2465, Battery Holder, AA x 3, Wire Leads KEYSTONE 1 Buy Now
Prototyping Board, FR2, Epoxy Paper, 1.5mm, 100mm x 160mm ROTH ELEKTRONIK 1 Buy Now
221-612, Pluggable Terminal Block, 2 Ways, 20AWG to 10AWG, 6 mm², Push In Lock, 41 A WAGO 4 Buy Now

 

Additional Parts:

 

Product Name
AA Batteries (3)
Attachments:
ToothbrushTimer_Resources.zip
element14 presents
DIY Toothbrush Timer

element14 presents  |  About Katie |  Project Videos

  • 74 series logic
  • shift register
  • axicom
  • lcd
  • e14p_KD
  • e14presents_kdumont
  • toothbrush
  • bistable relay
  • 555 timer
  • inverter
  • element14 presents
  • katie
  • shift registers
  • multicomp
  • signal relay
  • cree
  • bjt
  • toothbrushing
  • friday_release
  • 555
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 5 years ago +3
    Great job with the 555-based design! While watching, I forgot you built the entire circuit without a microcontroller. So when you mentioned not having feedback after pressing the start button, I first…
  • hifromkatie
    hifromkatie over 5 years ago in reply to baldengineer +3
    The Wago connectors are brill, I was somewhere a year or 2 ago and spotted someone using them and decided I need to get some. I go through lots when doing activities with school children as they make it…
  • kmikemoo
    kmikemoo over 5 years ago +2
    Yeah! Everything with a 555 timer is cool! Nice job, Katie. I wonder if I have any shift registers laying about...
  • danceman83
    danceman83 over 5 years ago

    I have some problems with the schematic file.

    I've got the error :

    Line 1, column 1: Opening element expected.

     

    Has anyone had the same problem and solved it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 5 years ago

    I really like the power off on this project - a well designed and useful end product image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • airbornesurfer
    airbornesurfer over 5 years ago

    Always love any excuse to use a Triple Nickel! Well done!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 5 years ago in reply to baldengineer

    The Wago connectors are brill, I was somewhere a year or 2 ago and spotted someone using them and decided I need to get some. I go through lots when doing activities with school children as they make it so easy for them to make a secure connection themselves.
    Have to admit I was initially just putting them in this to check everything was working, and had planned to solder and heat-shrink once I'd checked I had the order correct, however I still haven't gone back and tbh they work well if you don't mind the bulk.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago

    Great job with the 555-based design! While watching, I forgot you built the entire circuit without a microcontroller. So when you mentioned not having feedback after pressing the start button, I first thought: "well why not...<do stuff that would be easy with a MCU." Because there isn't one! duh.

     

    Also, I really like seeing those Wago connectors. I haven't used them yet, but they look like they would really make the initial fit and function checks a snap. (see what I did there?)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 5 years ago in reply to Jan Cumps

    Oh yes, it would have been! I hadn't thought of that image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 5 years ago in reply to DAB

    Thanks image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 5 years ago in reply to beacon_dave

    That'd be a good mod! Maybe a 556, the second 555 with a different frequency to do the different length of time.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 5 years ago in reply to kmikemoo

    Thanks! They're probably hiding in the bottom of a drawer image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago

    This would be a good project for the Project14 Making Time

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>