Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Make The Ultimate Phone Charging Camping Flashlight -- Episode 486
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 16 Feb 2021 6:05 PM Date Created
  • Last Updated Last Updated: 19 Feb 2021 8:24 AM
  • Views 4735 views
  • Likes 9 likes
  • Comments 17 comments

Make The Ultimate Phone Charging Camping Flashlight -- Episode 486

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Carrying around a rechargeable torch and power bank when out and about at night or whilst camping? Why not combine them into one easy to carry unit? Here’s how I do it.

 

Supplemental Content:

 

  • Episode 486: Bonus Content: Make The Ultimate Phone Charging Camping Flashlight

 

Bill of Material:

 

Product Name Manufacturer Quantity Buy Kit
PICPALNB126 Rechargeable Battery, 14.4 V, Lithium Ion, 3.35 Ah, 18650, Connector Panasonic 1 Buy Now
CC094 USB Connector, USB Type A, Socket, 2 Ways, Chassis Mount, Horizontal Velleman SA 1 Buy Now
0523405 Carpoint Socket Outlet, 12V Carpoint 1 Buy Now
48-782 Marine Grade Weatherproof 12V Cigarette Lighter Socket Philmore 2 Buy Now
Connector Housing, KK 254 2695, Receptacle, 2 Ways, 2.54 mm Molex 1 Buy Now
08-50-0032 Contact, KKRegistered 254, KK 254 4809 Series, Socket, Crimp, 22 AWG, Tin Plated Contacts Molex 1 Buy Now
Quick Disconnect Terminal, FASTON 250 Series, Female Quick Disconnect, 6.35mm x 0.81mm AMP – TE CONNECTIVITY 1 Buy Now
1614 10 DC Power Connector, Jack, 2 A, 2.35 mm, Panel Mount, Solder Lumberg 1 Buy Now
LED Housing, 9.5 mm x 12.5 mm, Black, Plastic, 5mm / T1 3/4 LEDs KINGBRIGHT 7 Buy Now
Pushbutton Switch, 20.2 mm, DPST, Off-On, Round Raised, Black Multicomp Pro 2 Buy Now
Pushbutton Switch, 20.2 mm, DPST, Off-(On), Round Raised, Black Multicomp Pro 1 Buy Now

 

Additional Parts:

 

Product Name

27W 12V DC Round LED Work Lamp

Plastic box with handle

Attachments:
UltimateFlashlightResources.zip
element14 presents
Make The Ultimate Phone Charging Camping Flashlight

element14 presents  |  About Katie |  Project Videos

  • traveling
  • katie dumont
  • carpoint
  • molex
  • usb power bank
  • e14p_KD
  • lumberg
  • e14presents_kdumont
  • panasonic
  • te connectivity
  • velleman
  • element14 presents
  • kingbright
  • lithium ion charger
  • katie
  • multicomp
  • torch
  • camping
  • rechargeable battery
  • night walks
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • hifromkatie
    hifromkatie over 5 years ago in reply to baldengineer +4
    I came across the buttons whilst searching, but they are really neat. Going to keep them on my go to parts list! The OpenSCAD is a bit of a fragile relationship, when I get my head around an idea then…
  • baldengineer
    baldengineer over 5 years ago +2
    Unexpected OpenSCAD (@ 9:20)! You are definitely more skilled with it than I am. I can, just barely, edit pre-existing designs. Also, I didn't know Multicomp Pro had those panel mount push buttons. I need…
  • koudelad
    koudelad over 5 years ago +2
    Nice build! The output luminosity is huge I was also impressed by the OpenSCAD. Do you have an estimation of the battery life while powering just the lamp? I would suggest to do some basic (PWM?) regulation…
Parents
  • koudelad
    koudelad over 5 years ago

    Nice build! The output luminosity is huge image I was also impressed by the OpenSCAD.

     

    Do you have an estimation of the battery life while powering just the lamp? I would suggest to do some basic (PWM?) regulation (100 %. 66 %, 33 % or similar) - not only to save battery life, but also not to get blind image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 5 years ago in reply to koudelad

    Thanks.
    I've done some quick calculations it worked out as drawing 19.46W whilst the torch was illuminated (Interesting, seeing as the LED unit claims 27W). The battery is 48Wh, so should be around 148 minutes of battery life.image

     

    Good call with PWM idea, I was aiming to see how bright I could make it, but it wouldn't be a bad idea to reduce it down. Having it selectable could be useful.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 5 years ago in reply to hifromkatie

    My guess is that 27 W is absolute maximum power consumption when powered by a car battery that is charged by an alternator. This can easily be 14.8 V (which is 1.23 times more than 12 V) and then 19.46 W * 1.23 = 24 W , which is closer.

     

    imageimage

    Here is a typical measurement on a car battery when not being charged and while running the engine.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 5 years ago in reply to koudelad

    Good call, hadn't thought about that image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hifromkatie
    hifromkatie over 5 years ago in reply to koudelad

    Good call, hadn't thought about that image