Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Keyboard Shortcuts Keypad with Raspberry Pi Pico -- Episode 494
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 12 Apr 2021 4:33 PM Date Created
  • Last Updated Last Updated: 16 Apr 2021 7:24 AM
  • Views 14932 views
  • Likes 14 likes
  • Comments 61 comments

Keyboard Shortcuts Keypad with Raspberry Pi Pico -- Episode 494

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Frequently used programs which have shortcuts/macros to save you time, but forget what they are? Here's a shortcut keypad for quick and easy access, with a helpful screen to remind you where the location of each.

 

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
Raspberry Pi Pico Raspberry Pi 1 Buy Now
4D systems PIXXILCD-25P4 4D Systems 1 Buy Now
Rotary Encoder PEC12R-4225F-S0024 BOURNS 1 Buy Now
MX1A-11NW Tactile Switch CHERRY 12 Buy Now
2.85mm BLACK PLA Filament FILAMENTIVE 1 Buy Now
 

Additional Parts

Product Name Manufacturer Quantity
Keycaps n/a 12


Attachments:

image

wiring.txt :
Switches (all)

Pico					To
GP0 (Pin1)		SW1(pin1)
GP1 (Pin2)		SW2(pin1)
GP2 (Pin4)		SW3(pin1)
GP3 (Pin5)		SW4(pin1)
GP4 (Pin6)		SW5(pin1)
GP5 (Pin7)		SW6(pin1)
GP6 (Pin9)		SW7(pin1)
GP7 (Pin10)		SW8(pin1)
(Pin11)				Screen(pin??)
(Pin12)				Screen(pin??)
GP10 (Pin14)		SW9(pin1)
GP11 (Pin15)		SW10(pin1)
GP12 (Pin16)		SW11(pin1)
GP13 (Pin17)		SW12(pin1)

Pin1 as above
Pin2 to +3.3v (Pico pin 36)					



Rotary Encoder

PinA					Pico GP14 (Pin19)
PinC					GND (Pico Pin 38)
PinB					Pico GP15 (Pin20)

Pin1					Pico GP16 (Pin21)
Pin2					+3.3v (Pico pin 36)

See datasheet for pin labeling on rotary encoder
But looks like this:

		1		2
	A		C		B
	
	

Screen using gen4 InterfaceBoard

+5V				+5V Pico(Pin40)
TX				Pico UART1 RX/GP9 (Pin12)
RX				Pico UART1 TX/GP8 (Pin11)
GND				GND (Pico Pin 38)
RES				Not Connected


Code and 3D Printable STL Files

  • Episode 494 Resources

element14 presents
Keyboard Shortcuts Keypad with Raspberry Pi Pico

element14 presents  |  Katie Dumont's VCP Profile |  Project Videos

  • shortcut keypad
  • rpi pico
  • shortcuts
  • keypad
  • e14presents_kdumont
  • macros
  • e14presents_katiedumont
  • time saving
  • element14 presents
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 5 years ago +9
    Raise your hand if you'd like to see an OpenSCAD tutorial from Katie!
  • airbornesurfer
    airbornesurfer over 5 years ago in reply to baldengineer +4
  • adamsoileau1
    adamsoileau1 over 5 years ago +2
    Fantastic project! This seems like it would be incredibly useful in day-to-day work. Also, nice usage of the Pico! I've been needing to buy one and try it out
Parents
  • Beemot
    Beemot over 4 years ago

    WOW!!! This project is wanderfull! Slight smile

    This link not work "4D systems PIXXILCD-25P4"

    Is this? https://it.farnell.com/4d-systems/sk-pixxilcd-25p4/starter-kit-display-grafico-2/dp/3534729?st=sistemi%204d%20pixxilcd-25p4

    Thankyou!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 4 years ago in reply to Beemot

    Yes, that's the right part, part order code 3534729.

    It looks like the links have changed since this was published.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Beemot
    Beemot over 4 years ago in reply to hifromkatie

    Perfect! Is there a wiring diagram of all the wiring somewhere? I couldn't find it in the project documentation.
    I am not a programmer nor an electronic but I would love to try my hand at this construction.

    But ... Maybe a very stupid question ... Can I record new macros in addition to the ones already in the code? Sweat smile

    I'd like to use it for CAD and various photo editing programs.

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 4 years ago in reply to Beemot

    There is a fritzing file, but it is on github, however I'm going to write it up as a document and upload it later today, as i've been asked a few times, and the fritzing was the first (and still last) time I've used it, so probably wasn't as polished as it should be!
    For new macros, I've used the adafruit_hid library, so in theory you could use any keys the library has for creating your own macros by changing the line in shortcuts.txt for that button.
    However the library I wrote to link the adafruit lib and my code only links the following keys:
    CTRL, SHIFT, SPACE, TAB, Super/windows, ALT, HOME, END, +. -, =, F1, F2, F3, F4. F5, F6, F7, F8, F9, F10, F11, F12, 1, 2, 3, 4, 5, 6, 7, 8, 9, 0, A, B, C, D, E, F, G, H, I, J, K. L, M, N, O, P, Q, R, S, T, U, V, W, X, Y, Z So it would need extra coding if you wanted to use for that those.

    Also it does multiple keypresses at one time to run the shortcut, so if a macro you wanted was a series of keypresses instead, then i'm not sure how it would handle this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hifromkatie
    hifromkatie over 4 years ago in reply to Beemot

    There is a fritzing file, but it is on github, however I'm going to write it up as a document and upload it later today, as i've been asked a few times, and the fritzing was the first (and still last) time I've used it, so probably wasn't as polished as it should be!
    For new macros, I've used the adafruit_hid library, so in theory you could use any keys the library has for creating your own macros by changing the line in shortcuts.txt for that button.
    However the library I wrote to link the adafruit lib and my code only links the following keys:
    CTRL, SHIFT, SPACE, TAB, Super/windows, ALT, HOME, END, +. -, =, F1, F2, F3, F4. F5, F6, F7, F8, F9, F10, F11, F12, 1, 2, 3, 4, 5, 6, 7, 8, 9, 0, A, B, C, D, E, F, G, H, I, J, K. L, M, N, O, P, Q, R, S, T, U, V, W, X, Y, Z So it would need extra coding if you wanted to use for that those.

    Also it does multiple keypresses at one time to run the shortcut, so if a macro you wanted was a series of keypresses instead, then i'm not sure how it would handle this.