Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Super 8 Camera Digitizer -- Episode 505
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 29 Jun 2021 5:49 PM Date Created
  • Last Updated Last Updated: 2 Jul 2021 7:24 AM
  • Views 11451 views
  • Likes 14 likes
  • Comments 21 comments

Super 8 Camera Digitizer -- Episode 505

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In a previous episode, Clem has built a proof of concept to convert a Super 8 film camera into a digital camcorder without any modifications to the camera itself. Many of you asked for a Kit or if a digital drop-in Film Cartridge replacement was possible! Finally, Clem has the chance to revisit the project and uses the New Raspberry PI compute Module 4 and the HQ camera module to build a crazy compact cartridge that is a major stepping stone towards a real product! And during the project, he even had to start his own 3D printer Resin brand just to obtain a material that is up to the task for this project!

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
AMPHENOL ICC FFC / FPC Board Connector, 1 mm, 15 Contacts, Receptacle, FCI 58RF SFW-R series, Surface Mount, Top AMPHENOL ICC 1 Buy Now
MULTICOMP PRO FFC / FPC Cable, 15 Core, 1 mm, Same Sided Contacts, 1.97 ", 50 mm, White 1 Buy Now
HIROSE(HRS) Mezzanine Connector, Receptacle, 0.4 mm, 2 Rows, 100 Contacts, Surface Mount, Phosphor Bronze HIROSE(HRS) 2 Buy Now
Raspberry Pi Compute Module 4, with 4GB RAM, 32GB eMMC, Wireless, BCM2711, ARM Cortex-A72 RPI 1 Buy Now
molex Board Connector FFC / FPC Board 1 mm, 15 Contacts, Receptacle, Easy-On 52610, Surface Mount molex 2 Buy Now
molex Premo Flex Jumper FFC / FPC Cable, 14 Core, 1 mm, Same Sided Contacts, 12 ", 305 mm, White molex 1 Buy Now
Additional Parts Manufacturer Quantity
Glas prism 10x10mm
MAYER MAKES Engineering Resin 1kg
 
Attachments:
Super 8_Resources.zip
element14 presents
Super 8 Camera Digitizer

element14 presents  |  About Clem |  Project Videos07W6532

  • clem
  • raspberry pi compute module
  • pi compute
  • super 8
  • e14presents_mayermakes
  • photography
  • compute
  • raspberry pi 4
  • raspberry pi
  • amphenol
  • multicomp
  • hirose
  • raspberry pi 4 compute module
  • friday_release
  • compute module
  • mayermakes
  • module
  • e14p_CMM
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mayermakes
    mayermakes over 5 years ago in reply to dougw +6
    Thanks for asking. I call it " MAYER MAKES Engineering Resin ". As seen in the video it is extremely tough and impact resistant. In my quick iterations I often use resin prints that I oversize and while…
  • fmilburn
    fmilburn over 5 years ago +4
    Material science, mechanical, optical, electronic, and power challenges. That is really Impressive work on an interesting and super challenging project.
  • ralphjy
    ralphjy over 5 years ago +3
    That's an incredible packaging accomplishment - great electromechanical design (plus the optical path). Makes me want to try a resin printer . It seems like trying to get that much power into an unmodified…
Parents
  • dougw
    dougw over 5 years ago

    Tell us more about this fancy resin....

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 5 years ago in reply to dougw

    Thanks for asking.

    I call it "MAYER MAKES Engineering Resin".

    As seen in the video it is extremely tough and impact resistant.
    In my quick iterations I often use resin prints that I oversize and while trying them out mechanically adjusting them to fit (by milling turning or carving), once they fit I get measurements and adjust the cad model.
    While I could make fits and shapes perfectly with standard Resin , they would not hold up to actual use as mechanical parts or cases. I usually had to make them with PETG on my Filament Printers.
    On this project PETG was quickly ruled out as it was not accurate enough and stable to allow for the tight tolerances and forces involved (resin got cracked by the internal clamping mechanism of my camera)

    So I used my contacts into my old Job as dev at a 3D printing material company to see ,if it was possible to develop a resin that would fit my needs.
    And after some iterations the outcome was better than expected.
    Very impact resistant and tough.
    once printed it is flexible and yellowish.
    After curing in Full UV spectrum (daylight) it is stiffer and gets fully clear transparent (a great bonus for Cases!!)
    Behaves like machining plastic on the lathe and mill.
    I might replace some stuff I previously made in aluminium with resin prints thanks to my Engineering Resin.

    Of course It would not be viable to just make a bit of resin for me, so I basically had to start my own Resin brand and make it accessible to the public, Ordering the raw materials in bigger batches gets the price down to a competitive level and we all can benefit from it.
    Currently a tiny prototyping batch is in use by myself but another possibly improved batch is in the works. Soon I should be able to send out review samples to some experts/influencers.
    I plan on two other varaints for the future :
    very Flexible (for softtouch surfaces and compliant structures)
    High Temperature
    Let's hope I can get this to market
    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to mayermakes

    Good luck getting this to market.  I'd love to have a material that I could print that had mechanical strength.  I'd vote for the High Temp variant if you had to choose which one to work on next.

     

    Then, I'd definitely have to get a resin printer image...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 5 years ago in reply to mayermakes

    Good luck getting this to market.  I'd love to have a material that I could print that had mechanical strength.  I'd vote for the High Temp variant if you had to choose which one to work on next.

     

    Then, I'd definitely have to get a resin printer image...