Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Design for Manufacturing - Project to Product by Modifying Off-the-Shelf Cases -- Episode-651
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 18 Apr 2024 5:23 PM Date Created
  • Last Updated Last Updated: 19 Apr 2024 12:59 PM
  • Views 2564 views
  • Likes 9 likes
  • Comments 12 comments

Design for Manufacturing - Project to Product by Modifying Off-the-Shelf Cases -- Episode-651

In a past element14 presents episode, Clem created a Universal Debugging Screen. This project sparked interest and many, many queries about its availability as an actual product! Well, what a good opportunity to investigate how to do that, in this episode Clem investigates enclosure options and how to customize them to turn a project into a product with items from Hammond Manufacturing. 

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Occasionally, a project posted on the internet prompts people to respond with questions about its availability as a kit, or as a product for purchase. One such project is the Universal Debugging Screen made by Clem in a previous episode of element14 presents. The universal Debugging screen turned out to be a handy tool for quick checks of serial data while working on a project. You could liken it to using a multi-meter that you can quickly whip out to check voltages or amperage. This handy device instantly shows you data flowing on the serial bus in letters and numbers, not variable voltages and in a human readable form. 

While Clem’s initial version consisted of leftover parts from previous projects (which demonstrates the value of keeping a stockpile of components around). A kit or product would need to be built from available still manufactured parts or designed with purpose. In the journey to transition from project to product, Clem has changed key components. Most notably of these are that Clem switched the user interface from individual buttons to a single rotary encoder. This change with a completely new form factor allows the device to be used one-handed in an ambidextrous manner by those who are left or right-handed. 

While Clem analyses the available approaches to a customized case, Clem explains how individually 3d printing case parts for such a project would consume too much time and introduce an element of risk due to quality control, especially having to do so at scale from a small business setup. 

image

Instead, the best approach has been decided to modify a ready-made enclosure as it would control costs and make certification of the final product much easier. After reviewing what products are available, Clem decided to use a handheld case from Hammond Manufacturing. With a penchant for it being blue in colour, having fancy soft over-moulding and a battery hatch that will fit a very specific purpose in the design! 

The battery compartment in the off-shelf enclosure is designed to hold a 9V cell block or 2 AA batteries. While Clem could run the device on a single 14,500 Lithium-Ion cell that fits the compartment, he decided to place a ‘pouch LiPo’ into a remining cavity in the enclosure and use the battery hatch to store the breakout cables needed to operate the device. A handy approach to keeping everything together and accessible for the user. 

image

While using the enclosure as a basis for the design, Clem proceeds to leverage the manufacturer supplied data sheets and specifications into a combined workflow of FreeCAD (Ondsel version) and KiCad to design and derive the ideal PCB shape to make sure that all the components tightly fit into the desired enclosure. Using Boolean subtraction to generate case versions with the required cutouts and ensuring to test out multiple ways of producing the modified cases ‘in house’. While designing the changes to the enclosure, Clem notes that eventually it would be more economical to order the cases pre-modified from the manufacturer or similar service to be able to produce the product at scale, using CAD designs can ensure that the measurements taken are appropriate to be passed on for such changes. 

The same data can also be used to create instructions for machines accessible to the casual and more professional maker. A simple way would be to just 3d print the modified parts and combine them with the readymade enclosures. Clem recommends that resin printing should be considered for this approach due to its high level of detail and accuracy as well as sturdiness (given the right resin is used). Unless you have a specifically designed resin for this purpose (such as MayerMakes Engineering Resin – totally not a product placement). Though after assessing these options, Clem instead focuses on the less common methods such as laser cutting and CNC milling. 

image

Using Lightburn to generate the instructions for a Fiber laser engraver, and a CO2 laser, Clem highlights the difficulty in choosing the right method as it greatly depends on the material that is being cut (while emphasising safety and user protection). The milling CAM that Clem uses is generated with the FreeCAD Path workbench and executed by a tiny 3020 CNC router commanded by LinuxCNC. to exactly position the cutouts in respect to the already manufactured enclosure holders and mounting templates were used that reference the machines 0,0 home position to allow for repeatable cuts. 

While the Laser approach showed promise, it demonstrated that it needs a lot of experimentation, appropriate masking, and preparation to find the ideal settings to prevent damage and repeatable results. The CNC milling yielded a usable result from the first try from the perspective of cut quality, but the enclosure shifted due to the cutting forces imposed on it, so this approach needs a better prepared workpiece mount. 

image

Overall, Clem has demonstrated that this part of design for manufacturing is only one in many steps you will need to consider when taking a project into a marketable product. Iteration and testing is still significantly important, and Clem shows that even on a small scale, you can create the necessary adjustments to move onto producing at scale. 

image

Links and Downloads:

  • Case Files for all versions
  •  All-Purpose Debugging: A Practical Universal Screen with LCD Displays -- Episode-631  

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
HAMMOND 1553BTBUBKBAT Hammond 1 Buy Now
BOURNS PEC12R-2220F-S0024 Bourns 1 Buy Now
MIKROELEKTRONIKA MIKROE-1120 Mikroelektronika 1 Buy Now
 
  • Precision Laser Cutting for Production
  • Streamlining Production Processes
  • Project to Product Transformation
  • Flexible Design for Custom Products
  • Laser Cutting and CNC Milling Strategies
  • Fiber Laser Cutting for Small Batch Manufacturing
  • case modification
  • Efficient Prototyping for Production
  • cnc
  • Small Scale Manufacturing Solutions
  • Design for manufacturing
  • pre made cases
  • Practical Storage Solutions for Devices
  • dfm
  • DIY Product Development Methods
  • Resin Printing for Prototyping Precision
  • Enclosure Modification for Production
  • laser cut
  • Manufacturer Supply Data Utilization
  • friday_release
  • e14p_CMM
  • CNC Milling for Enclosure Modification
  • Cost-Effective Enclosure Customization
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 2 years ago +1
    Those enclosures are really nice. It's possible to get a very clean milled result, the method is to always have the enclosure surface flat against a hard waste material, e.g. a sheet of MDF (wood fiberboard…
  • dougw
    dougw over 2 years ago in reply to javagoza

    It isn't hoarding - it is just your clever predictive recycling (CPR) strategy....another efficient green initiative ....Thumbsup

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 2 years ago

    Great that you share your experiences machining Hammond boxes.

    I am currently participating in the Extreme Environment Experimentation Design Challenge sponsored by Hammond, so I am learning how to machine Hammond polycarbonate enclosures.

    Currently my preference is to cut with Dremel plastic or PVC discs or spiral cutting bits at low speeds between 12,000 and 15,000 rpm. The trick is to continually lubricate the drill bit or disc and the cutting area with dish soap. Don't apply too much pressure with the tool and stop if it gets hot. For drilling, use a drill bit with a sharp tip, less than 60º, well lubricated with dishwashing detergent or another lubricant that dissipates heat and always rest the surface on a wooden block so that it does not tear when the drill tip comes out. 

    I haven't tried it yet with the Hammond enclosure supplied for the challenge, I'm trying it with recovered material, I also suffer from massive hoarding syndrome. Grinning

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<