Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY Jig for your Laser Cutter with Custom Arduino Automation -- Episode-656
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: cstanton
  • Date Created: 13 Jun 2024 12:04 PM Date Created
  • Last Updated Last Updated: 14 Jun 2024 1:47 PM
  • Views 3863 views
  • Likes 7 likes
  • Comments 5 comments

DIY Jig for your Laser Cutter with Custom Arduino Automation -- Episode-656

If you have spent any amount of time working with a laser cutter, At your local hack(er)space, makerspace or maybe in your line of work. Perhaps you are even fortunate to have one at home in your workshop? You will know that working with repeated tasks can come with its own challenges. Especially if you need continuity between cuts and you are cutting a lot of the same pieces. Clem, having experienced the same, decided to take matters into their own hands and produce a solution to help, watch the episode and read along and perhaps you will also find it useful!

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

For Clem, it quickly becomes tedious and frustrating to have to constantly swap pieces out when working on them in the laser cutter, not to mention error-prone to do the same task repeatedly and ensure that quality is maintained. Having to load and unload workpieces into their CO2 laser cutter, needing to deactivate the safety interlocks and ensure that each new material was played accurately to ensure that it was engraved correctly, this multi-step process requires a lot of concentration and time, which invites misalignment from a variety of factors.

Enclosure wiring

The Problem with Traditional Jigs

Why not simply use a ‘jig’? If you are unfamiliar with the term, it is effectively a template or layout for the piece being worked on to sit securely in the same position and layout every time. Usually, you would do this when you need what you are working on not to move, but its shape is unconventional and this becomes difficult to use with clamps. A jig has its limitations:

  • They usually depend on flat, mountable parts.
  • Alignment tolerances are a concern with multiple items.
  • The solution is either suitable for one component worked on regularly, or mass production, but is not adaptable for smaller-scale production/alterations.

Getting Jiggy With It

Clem's Rotating Drum Solution

As Clem found that a traditional approach to a jig is not suitable for their needs, they sought a more adaptable solution that can work with different types of workpieces, permitting individual clamping and no special preparation. Considering when working with the laser cutter with the Lightburn software, it has a consistent origin point for the tooling to do its job, this means that Clem’s solution will offer significant flexibility.

Clem’s solution involves the ‘classic’ project parts that should be familiar to any maker:

  • An Arduino Uno
  • Trinamic TMC2100 stepper driver
    • With Corresponding stepper motor
  • Prototyped on a protoboard with hand-soldered wires.

Put together, this would develop into a four-sided rotating drum mechanism that uses interchangeable slides, designed for each type of workpiece. These slides are quick to 3D print, and they can be shaped to fit even the most unusually shaped workpieces, including those without flat sides.

Spin Me Right Round

Simplifying Stepper Motor Wiring

Using six leads, Clem demonstrates an easy method to identify the correct wires on a stepper motor. With the help of two wires and turning the motor, resistance can indicate the appropriate ends of the same coil. When no resistance is felt, the wires belong to different coils, this process which you can follow along with Clem in the video can take no time at all with a little practice.

Rotating

Considerations when Designing the Drum Solution

Measure twice, design once. Clem quickly discovers that their design had a design flaw: it was too tall to fit inside the laser cutter. On reflection, this is due to deliberately leaving enough clearance for the mounting of thick workpieces, this revelation resulted in a clear design improvement. Clem switched to a rotary table design, allowing it to feature a switchable magnet system. This is like the design of magnet bases used in machining shops! This means that Clem’s 3D printed design aligns magnets to create a magnetic lock. Three magnet pairs have the north pole aligned upwards with one in the opposite direction, the plate can then be easily lifted off by rotating it ninety degrees which causes the magnets to repel one another.

Cutty Cut Cut

Reaping the Rewards of Design Iteration and Automation

Clem demonstrates the final solution, recording it from inside the CO2 laser cutter which shows the entire process in all its glory. An external cable remote helps the process by allowing quarter turns of the turntable.

The project is a clear reminder of the importance of automation and identifying repetitive tasks and where time can be saved, or frustrations reduced, allowing you to focus on the task at hand where necessary. It helps to have multiple tooling solutions to aid with designing the solution. Clem’s innovative approach is a prime example of how automation can help and enhance your efficiency and accuracy.

Downloads & Links:

  • Download the Code and CAD files

Parts and Bill of Materials

Product Name Manufacturer Quantity Buy Kit
Arduino UNO SMD Rev3, ARDUINO 1 Buy Now
stepper Motor, Dual Shaft, 42 Nanotec 1 Buy Now
TMC2100 Silentstepstick Trinamic 1 Buy Now
MULTICOMP 3D Printer Filament, 1.75mm Multicomp 1 Buy Now
BRAUER Toggle Clamp, Vertical, 70 N Brauer 4 Buy Now
Black Rocker Switch, Multicomp pro 3 Buy Now
 

Additional Parts

Product Name
Protoborad, 2,54mm pin headers. Wiring.
4 pin “aviation connectors”

element14 presents

element14 presents  |  About Clem  |  Project Videos 

  • rotating drum mechanism
  • improving laser cutter accuracy
  • engrave series parts
  • diy laser
  • magnetic lock system design
  • Laser cutter automation
  • arduino laser cutter project
  • laser upgrade
  • automating repetitive tasks
  • maker projects with arduino
  • 3d printed jig alternatives
  • enhancing laser cutter precision
  • custom stepper driver setup
  • diy laser cutter enhancements
  • prototyping with arduino
  • workpiece changing
  • laser cutter efficiency tips
  • automate movement
  • friday_release
  • stepper motor wiring guide
  • co2 laser cutter modifications
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mayermakes
    mayermakes over 2 years ago +1
    What would you like to automate in your life?
  • genebren
    genebren over 2 years ago +1
    Very cool automation project! Another enjoyable project video.
  • DAB
    DAB over 2 years ago +1
    interesting build Clem. You clearly demonstrated the term "measure twice and cut once!"
Parents
  • mayermakes
    mayermakes over 2 years ago

    What would you like to automate in your life?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Mikeatencio
    Mikeatencio over 2 years ago in reply to mayermakes

    My wife for cleaning the house...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Mikeatencio
    Mikeatencio over 2 years ago in reply to mayermakes

    My wife for cleaning the house...