Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents From Kit to Custom Design: Building a Tube-Based FM Radio -- Episode 680
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: cstanton
  • Date Created: 28 Aug 2025 2:28 PM Date Created
  • Last Updated Last Updated: 29 Aug 2025 9:50 AM
  • Views 13843 views
  • Likes 9 likes
  • Comments 10 comments

From Kit to Custom Design: Building a Tube-Based FM Radio -- Episode 680

Mark takes on the challenge of building a fully functional FM superheterodyne radio without transistors or SDR, relying instead on vacuum tubes and a custom PCB design. After finding major flaws in a DIY kit, he scraps the schematic and creates his own design from scratch, covering everything from oscillator design and frequency mixing to tuning and final testing. Follow along as he assembles, debugs, and tunes the radio into a working stereo receiver.

Watch the Episode

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Building a modern FM radio receiver is usually straightforward. A single chip like the TDA7000 or a software-defined radio (SDR) module can handle most of the work with just a few supporting components. But where’s the fun in that? Using ready-made solutions means missing out on the design process, sourcing unique parts, building prototypes, and debugging problems. To make this project more challenging, Mark decided to design and build a vacuum tube FM receiver without transistors.

(Note: Mark did use a stereo decoder IC, though it’s optional. For mono audio, it can be skipped. He also included an LM7809 regulator, which of course contains transistors internally.)

image

The Kit That Wasn’t

To get started, Mark ordered a DIY tube radio kit from AliExpress. It cost around $220, including shipping, and came with essential components such as vacuum tubes, intermediate frequency (IF) coils, and a variable capacitor. The idea was that it would save him time tracking down parts.

When the kit arrived within two weeks, he quickly found issues: the power transformer was missing, and one resistor was broken. The supplier promised replacements in a later shipment, but the bigger problem was the documentation. The manual was only four pages long, entirely in Chinese. After running it through Google Translate, it became clear there were no instructions on tuning or adjusting the frequency stages. Worse, the schematic had errors: pin numbers were swapped, some required connections were missing, and the PCB contained components not even listed in the bill of materials. At that point, Mark knew the kit was unusable.

Still, it wasn’t a complete loss. He had the critical parts he needed such as tubes, coils, and the capacitor. The rest he would redesign himself.

image

Designing From Scratch

Looking at the salvaged components, Mark concluded he could make the radio work by replacing or adjusting capacitors and resistors while reusing the tubes. With that decided, he set out to design a proper superheterodyne receiver from scratch.

Input Band Filter

The first stage is a band-pass filter that limits the antenna input to the desired frequency range. This filtered signal is then amplified before being sent to the mixer.

The Oscillator

Next, Mark designed a Hartley oscillator to generate a tunable sine wave frequency. To tune a station at 95 MHz, the oscillator can be set to either 105.7 MHz (station + 10.7 MHz) or 84.3 MHz (station – 10.7 MHz). He found that using the lower frequency provided better results with less interference from nearby airband signals.

Mixing the Signals

The mixer combines the input signal with the oscillator signal, creating several outputs: fInput, fOscillator, fInput ± fOscillator. The only one of interest is the difference (fOscillator – fInput), which falls into the intermediate frequency (IF) range.

Intermediate Frequency (IF) Stages

The mixed output is filtered at 10.7 MHz, which is the standard IF for FM receivers. Multiple stages of filtering improve selectivity. In Mark’s build, four stages are used, with the final one incorporating an FM detector.

FM Detector

Finally, the IF signal is demodulated to recover the original audio. This is done with a dual-diode detector known as a Foster-Seeley discriminator, which produces the audio signal that can then be amplified.

image

Reflections

What started as a faulty DIY kit turned into a rewarding scratch-build. Along the way, Mark revisited many fundamentals of analog design such as oscillators, mixers, filtering, and FM detection. The end result is a working vacuum tube FM superheterodyne receiver, built from a mix of salvaged and custom-sourced components. Despite the frustrations, it was a valuable reminder that sometimes the best projects are the ones that don’t go as planned.

Supporting Links and Downloads

- Schematics and Bill of Materials

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
Multilayer Ceramic Capacitor, 47 pF, 50 V, ± 5%, Radial Leaded, C0G / NP0, 5 mm Vishay 7 Buy Now
CAPACITOR, 10PF, SL, 1KV, RADIAL TDK 1 Buy Now
Multilayer Ceramic Capacitor, 18 pF, 50 V, ± 5%, Radial Leaded, C0G / NP0, 5 mm Vishay 1 Buy Now
CAP, 4700PF, 1 KV, 10%, X7R Vishay 17 Buy Now
CAP, TRIMMER, 3-10PF, 150V Vishay 2 Buy Now
CAP, 1000PF, 50V, 5%, C0G/NP0 Vishay 1 Buy Now
CAP, 2PF, 100V, MLCC, RADIAL TDK 1 Buy Now
Electrolytic Capacitor, 3.3 µF, 50 V, ± 20%, Radial Leaded Multicomp Pro 1 Buy Now
CAP, 120µF, 450V, 20% Rubycon 3 Buy Now
CAP, 100PF, 50V, 5%, C0G/NP0 Vishay 1 Buy Now
CAP, 0.1µF, 520V, 10%, PP, RADIAL Yageo 2 Buy Now
Electrolytic Capacitor, 1 µF, 50 V, ± 20%, Radial Leaded Multicomp Pro 2 Buy Now
Multilayer Ceramic Capacitor, 56 pF, 50 V, ± 5%, PC Pin, C0G Mulitcomp 1 Buy Now
Aluminium Electrolytic Capacitor, AM Series, 10 - F, - 20%, 50 V Panasonic Industrial 3 Buy Now
CAP, 33PF, 50V, 5%, C0G/NP0 Vishay 1 Buy Now
Electrolytic Capacitor, 1000 µF, 25 V, ± 20%, Radial Leaded Panasonic 2 Buy Now
Multilayer Ceramic Capacitor, 0.015 µF, 50 V, ± 10% TDK 2 Buy Now
TB, WIRE TO BRD, R/A, 9WAY, 12AWG Multicomp Pro 1 Buy Now
Pin Header, Signal, Wire-to-Board, 2.54 mm, 1 Rows, 4 Contacts Molex 1 Buy Now
RF / Pin Diode, Single, 100 V, DO-7, 2 Pin, 0.8 pF Solid State 2 Buy Now
Zener Single Diode, 100 V, 5 W, 017AA, 2 Pins ONSEMI 1 Buy Now
LED, RED, 15MCD, 629NM, 3MM Multicomp Pro 1 Buy Now
Standard Recovery Diode, 1 kV, 1 A, Multicomp Pro 4 Buy Now
INDUCTOR, 3.3µH, 20%, RADIAL LEADED Multicomp Pro 10 Buy Now
TINNED COPPER WIRE, TCW, 16 SWG Multicomp Pro 1 Buy Now
Wire, Enamelled, PU, Transparent, 23 AWG, 0.246 mm² Multicomp Pro 1 Buy Now
Through Hole Metal Film Resistor, MRS25 Series, 47 kohm, 600 mW Vishay 3 Buy Now
Through Hole Resistor, 3.9 kohm, MCF Series, 250 mW Multicomp Pro 1 Buy Now
Through Hole Resistor, 100 kohm, MF25 Series, 250 mW Multicomp Pro 3 Buy Now
Through Hole Resistor, 68 ohm, MF25 Series, 250 mW Multicomp Pro 1 Buy Now
Through Hole Metal Film Resistor, MF25 Series, 270 kohm, 250 mW Multicomp Pro 1 Buy Now
Through Hole Resistor, 1 kohm, MF25 Series, 250 mW Multicomp Pro 2 Buy Now
Through Hole Resistor, 220 kohm, MF25 Series, 250 mW Multicomp Pro 1 Buy Now
Through Hole Metal Film Resistor, MF25 Series, 9.1 kohm, 250 mW Multicomp Pro 1 Buy Now
Through Hole Resistor, 3.3 kohm, MF25 Series, 250 mW Multicomp Pro 2 Buy Now
Through Hole Resistor, 100 kohm, MF50 Series, 500 mW Multicomp Pro 6 Buy Now
Through Hole Resistor, 330 kohm, MF50 Series, 500 mW Multicomp Pro 1 Buy Now
Through Hole Resistor, 220 kohm, MF50 Series, 500 mW Multicomp Pro 1 Buy Now
Through Hole Metal Film Resistor, MF50 Series, 62 kohm, 500 mW Multicomp Pro 1 Buy Now
Through Hole Resistor, 2 kohm, MF50 Series, 500 mW Multicomp Pro 1 Buy Now
Through Hole Metal Film Resistor, MCMF Series, 33 ohm, 600 mW Multicomp Pro 1 Buy Now
Through Hole Metal Film Resistor, MCMF Series, 470 kohm, 600 mW Multicomp Pro 2 Buy Now
Through Hole Resistor, 1 kohm, MF50 Series, 500 mW Multicomp Pro 2 Buy Now
RES, 47K, 1W, AXIAL, METAL OXIDE Multicomp Pro 2 Buy Now
RES, 2K, 3W, AXIAL, METAL FILM Vishay 1 Buy Now
Through Hole Resistor, 10 kohm, MOR Series, 3 W Multicomp Pro 2 Buy Now
Through Hole Metal Film Resistor, SQM Series, 1 kohm, 5 W TT Electronics / Welwyn 1 Buy Now
Through Hole Metal Film Resistor, SQM Series, 6.8 kohm, 5 W TT Electronics / Welwyn 1 Buy Now
Trimmer, Multi Turn, Cermet, Top Adjust, 50 kohm Bourns 1 Buy Now
PCB Test Point, Multipurpose, Yellow Keystone 15 Buy Now
PCB Test Point, Multipurpose, Black Keystone 10 Buy Now
PCB Test Point, Miniature, Orange Keystone 4 Buy Now
Linear Voltage Regulator, 7809 STMICROELECTRONICS 1 Buy Now
Phone Audio Connector, 5 Contacts, Jack, 3.5 mm Cliff 1 Buy Now
 

Additional Parts

Product Name Manufacturer Quantity
PCB For Tube Radio V1.0 Tindie 1
6-26pf Air Capacitor (Double) Aliexpress 1
TA7343AP MD Aliexpress 1
BALUN_4PIN Aliexpress 4
BALUN_5PIN Aliexpress 1
Radio Tube 6N3 Aliexpress 1
Radio Tube 6K4 Aliexpress 2
Radio Tube 6J4 Aliexpress 2
Radio Tube 6Z4 Aliexpress 1
Radio Tube 6C11 Aliexpress 1
Radio Tube 6n2 Aliexpress 1
Transformer Aliexpress 1
Tube Socket 7p Other 5
Tube Socket 9 p Other 3
  • diy fm receiver
  • variable capacitor radio
  • vacuum tube electronics
  • building fm radio from scratch
  • 10.7 mhz intermediate frequency
  • DIY electronics project
  • hartley oscillator fm
  • fm radio with tubes
  • analogue electronics project
  • diy pcb radio
  • vacuum tube fm radio
  • superheterodyne radio build
  • fm radio kit trouleshooting
  • fm discriminator design
  • tube radio schematic
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • donnersm
    donnersm over 1 year ago +1
    This Build was nothing less then amazing! If you have any questions, feel free to drop me a line. I'll get back to you ASAP
Parents
  • dougw
    dougw over 1 year ago

    Great project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 1 year ago

    Great project.