Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents When Your Body Becomes the Instrument: Clem Builds the “Dröne” Synth -- Episode 685
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: cstanton
  • Date Created: 8 Oct 2025 1:09 PM Date Created
  • Last Updated Last Updated: 9 Oct 2025 3:58 PM
  • Views 6835 views
  • Likes 6 likes
  • Comments 4 comments

When Your Body Becomes the Instrument: Clem Builds the “Dröne” Synth -- Episode 685

Clem (MakerMakes) takes inspiration from Tom Morello of Rage Against the Machine to build Dröne, a DIY body-controlled synth that recreates Morello’s famous “cable tip” sound. By using his body as part of the circuit, Clem explores how capacitance and inductance can create controllable, evolving tones. What starts as an experiment becomes a playable instrument that reacts to touch, proximity, and movement, even burning out a vintage speaker in the process. Watch how Clem turns a strange guitar trick into a full-blown electronic music project.

Watch the Project

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Building Dröne: Turning Tom Morello’s Guitar Trick into a Synth Experiment

When Clem sees something unusual in the world of sound, he just can’t resist trying to understand it—and then taking it further. This time, inspiration came from Tom Morello of Rage Against the Machine. During some live performances, Morello pulls off a strange trick: he unplugs his guitar cable, touches the tip, and creates an otherworldly drone sound. The artist himself doesn’t offer a technical explanation, just the technique with his effects pedal setup.

“Have you ever seen Rage Against the Machine live? Tom Morello sometimes does this weird thing where he unplugs the guitar and touches the tip — and it makes weird drone sounds. I think what he's doing here is not magic, but electronics-related.” - Clem

Clem suspects the human body is more than a random noise source here. His working theory? The body acts as a capacitor to ground, forming a low-pass filter in the signal path. This explains the tonal shifts when touching the cable tip. But what if this effect could be amplified and tamed? What if it could become an instrument in its own right?

image

From Idea to Circuit

The result of this investigation was Dröne — a DIY oscillator-based synth that combines inductors, capacitors, and resistors into a tone generator influenced by the human body.

Clem designed the circuit as a hybrid LC/RC oscillator, similar in principle to those found in electric guitars or old analog tone generators. The oscillation depends partly on the performer’s capacitance to ground, meaning the sound changes when Clem touches, steps, or even moves near the circuit.

“So I can now tune the low-pass and high-pass filters of my circuit. But I also want to tune the pitch of the tone I’m producing… my body is the capacitor, so I put a potentiometer in series with myself.”

The circuit consists of three major parts:

  1. Custom inductors (coils) ,  hand-wound by Clem to act as tunable components in the oscillator.

  2. Filter network,  high-pass and low-pass filters, each controlled by a potentiometer.

  3. The player’s body,  acting as the variable capacitor in the circuit, modulating pitch and tone.

Clem also included a mix control to adjust between filtered and unfiltered signal paths, allowing him to blend tonal characteristics dynamically.

imageimage

Adding Control: The Handpiece

To give the player even more influence, Clem builds a “handpiece”—essentially a connector with an exposed wire attached to a ten-turn potentiometer. Why external? Because fitting such a chunky component inside the compact case would be impossible. This setup allows Clem to pre-set a pitch or frequency range, then dynamically alter the tone simply by touching the handpiece.

Even footwear matters. Touching the wire barefoot vs. in shoes? Totally different tonal character! You can even stomp rhythms into the sound—true analog body modulation.

image

First Test: Big Drones, Big Trouble

For the maiden test, Clem hooks Dröne (that’s what he calls his creation) up to a vintage 1970s turntable speaker and an in-store amplifier. The results? Thick, evolving drones with an eerie, almost vocal quality. Everything is going great—until the speaker starts smoking! Looks like the old driver couldn’t handle the sustained resonance. One brave speaker gave its life for the cause.
A Happy Accident: Contactless Playing

While experimenting, Clem stumbles onto something fascinating: at certain frequencies, he can change the sound without touching anything. Simply moving his hand near the speaker couples his body into the field, altering the tone like a capacitive sensor. Suddenly, Dröne behaves like a theremin, but built on completely different principles. Or is it that different, after all?

image

The Future of Dröne

What started as a recreation of Tom Morello’s trick has become a prototype for a whole new instrument concept. A modular synth that responds to the player’s physical presence and touch? That sounds like something the world hasn’t seen before.

Stay tuned, Clem’s already thinking about version two. And maybe next time, the speakers will survive.

image

Supporting Files and Links

- Video of Tom Morello Explaining his Trick

-  Episode 685 Resources  

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
ECW0.5 winding wire enamel Multicomp pro 1 Buy Now
KLBM 3 Connectors Lumberg 3 Buy Now
MC001131 Case Multicomp pro 1 Buy Now
ALNICO500 4X19MM Magnets STANDEXMEDER 8 Buy Now
Potentiometer 10k
3d printed Spool parts (stl provided in downnloads)
Knobs for potentiometers
 

  • capacitive audio circuit
  • diy electronic instrument
  • tom morello guitar trick
  • cable tip guitar sound
  • body controlled synthesizer
  • electronic music experiment
  • DIY drone synth
  • rage against the machine guitar effect
  • lc rc oscillator
  • oscillator circuit build
  • experimental sound device
  • DIY synth build
  • capacitive touch sound
  • how to make a drone synth
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • mayermakes
    mayermakes over 1 year ago

    I wonder what could be doen by passing such a device into a modular synth..so yourself dancing could alter the controll voltage for a clean VCO

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 1 year ago in reply to mayermakes

    I enjoyed your video, sort of a mad scientist vibe going on.  There were a few moments where it seemed like you were getting close to something, but mostly it seemed like you were getting a bunch of 50 and 100Hz (line voltage).

    I like your idea of building something that could plug into a modular synth, but I would think that you could get so much more mileage with something like an accelerometer or maybe some sort of video-based body position device where you could generate multiple CV outputs that could drive a few VCOs, sort of like making each hand/arm, leg/foot and head into separate instruments.

    Still, yet another fun video!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 1 year ago in reply to mayermakes

    I enjoyed your video, sort of a mad scientist vibe going on.  There were a few moments where it seemed like you were getting close to something, but mostly it seemed like you were getting a bunch of 50 and 100Hz (line voltage).

    I like your idea of building something that could plug into a modular synth, but I would think that you could get so much more mileage with something like an accelerometer or maybe some sort of video-based body position device where you could generate multiple CV outputs that could drive a few VCOs, sort of like making each hand/arm, leg/foot and head into separate instruments.

    Still, yet another fun video!