Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Raspberry Pi Smart Water Dispenser -- Episode 498
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 10 May 2021 5:35 PM Date Created
  • Last Updated Last Updated: 14 May 2021 7:24 AM
  • Views 5353 views
  • Likes 6 likes
  • Comments 9 comments

Raspberry Pi Smart Water Dispenser -- Episode 498

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

So much time wasted every day standing at my sink filling water bottles. I finally decided that I need to automate this process. I am going to use a Raspberry PI, some custom water valves driven by a servo, a water filter and instant hot water heater to make my own automatic hot and cold water dispenser with presets so I can walk away while the water bottle, coffee or French press fills itself!  

Supplemental Content:

  • Download code from Github:  https://github.com/KalebTheMaker/Water-Dispenser

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
ADAFRUIT Add-On Board, PiTFT Plus Raspberry Pi HAT, 2.8" LCD Screen, 320 x 240, Capacitive Touchscreen ADAFRUIT 1 Buy Now
DELKIN DEVICES Flash Memory Card, MLC, MicroSDHC Card, UHS-1, Class 10, 16 GB, Utility MicroSD Series DELKIN DEVICES 1 Buy Now
MCM 5V Trigger Relay Module For Arduino And Raspberry Pi MCM 1 Buy Now
Industrial Pushbutton Switch, 59 Series, 13.6 mm, SPST-NO-DB, Momentary, Round, Blue ITW SWITCHES 1 Buy Now
SWITCH, SPST-NO, 0.4A, 32VAC, ROUND, RED ITW SWITCHES 2 Buy Now
RASPBERRY-PI Single Board Computer, Raspberry Pi 3 Model B+, BCM2837B0 SoC, IoT, PoE Enabled RASPBERRY-PI 1 Buy Now
XP POWER AC/DC Enclosed Power Supply (PSU), ITE, 1 Outputs, 50 W, 5 V, 10 A XP POWER 1 Buy Now
Wire-To-Board Terminal Block, 5.08 mm, 2 Positions, 26 AWG, 16 AWG, 1.5 mm², Screw PHEONIX CONTACT 4 Buy Now
Un-Filtered IEC Power Entry Module, C14 Inlet, IEC C14, Medical, 8 A, 250 VAC, 2-Pole Switch SCHURTER 1 Buy Now

 

Additional Parts: 

Product Name

2x 25kg RC Digital Servo

2x 1/4 Turn Shutoff valve, 3/8 MIP

1x 3/8' brass TEE fitting

Waterdrop 10UA-UF Water Filter

Westinghouse 40-WH-1500-SS Instant Hot Water Dispenser (Tank Only)
1/4" ID silicone tubing
12" 3/8 connector hose
male header pins
3mm P90 Acrylic
female extension cord end
3mm Hex cap screws and bolts
Attachments:
Episode_498_CAD-Files.zip
element14 presents
Raspberry Pi Smart Water Dispenser

element14 presents  |  About Kaleb |  Project Videos

  • flow control
  • kaleb
  • e14presents_kalebclark
  • schurter
  • mcm
  • hydration
  • diy
  • raspberry_pi
  • raspberry pi
  • element14 presents
  • delkin devices
  • itw switches
  • friday release
  • adafruit
  • e14p_KC
  • friday_release
  • xp power
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • KalebTheMaker
    KalebTheMaker over 5 years ago in reply to bob5731 +2
    You are right, the link is not there. I am including a link to github and Ill work on getting it in the proper place. https://github.com/KalebTheMaker/Water-Dispenser All the STL's are included in the…
  • kmikemoo
    kmikemoo over 5 years ago +1
    I'm surprised that there's a servo that will turn a 1/4 turn valve. Those beasts are stiff. Nice build.
  • KalebTheMaker
    KalebTheMaker over 5 years ago in reply to kmikemoo +1
    Hi Mike, Thank you, Those 25kg servos are pretty great. I did have to use the XP power 5v DC supply to get enough current to run them with the valve, but they have no problem with it at all.
Parents
  • bob5731
    bob5731 over 5 years ago

    I don't see the source code files yet.

    Can you upload 3D printer files don't have a laser cutter available to me

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • KalebTheMaker
    KalebTheMaker over 5 years ago in reply to bob5731

    You are right, the link is not there. I am including a link to github and Ill work on getting it in the proper place.

    https://github.com/KalebTheMaker/Water-Dispenser

     

    All the STL's are included in the zip file above for the 3d printed parts. There is a folder called LaserCutFiles that has all the DXF's in it. You can use those to extrude out a 3mm part for 3d printing. Also included is the fusion360 source file which has all the parts extruded and can be exported as STL's.

     

    -Kaleb https://github.com/KalebTheMaker/Water-Dispenser

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • KalebTheMaker
    KalebTheMaker over 5 years ago in reply to bob5731

    You are right, the link is not there. I am including a link to github and Ill work on getting it in the proper place.

    https://github.com/KalebTheMaker/Water-Dispenser

     

    All the STL's are included in the zip file above for the 3d printed parts. There is a folder called LaserCutFiles that has all the DXF's in it. You can use those to extrude out a 3mm part for 3d printing. Also included is the fusion360 source file which has all the parts extruded and can be exported as STL's.

     

    -Kaleb https://github.com/KalebTheMaker/Water-Dispenser