The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents Basic Tools & Wire -- The Learning Circuit 04
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 7 Dec 2017 8:14 PM Date Created
  • Last Updated Last Updated: 10 Jan 2018 8:24 AM
  • Views 4195 views
  • Likes 14 likes
  • Comments 14 comments
Related
Recommended

Basic Tools & Wire -- The Learning Circuit 04

image

element14's The Ben Heck Show

Join Karen as she shares her enthusiasm for teaching STEM subjects, gives you what you need to know to get started on electronics projects, and more.

Back to The Ben Heck Show homepage image

The Learning Circuit
Featured Bonus Content
See All Episodes

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Karen goes over wires and wire tools, and gives advice on selecting the right hand tools to get you started making circuits. Wire is the artery through which electricity flows. Wires come in two types, stranded and solid.  If your application requires flexibility, such as in a robotic arm, stranded wire is ideal when the wire needs to be moved frequently.  If little or no movement is required, such as when you are prototyping circuits on a breadboard, solid wire is easier to push through.

Karen's Toolkit:

 

Product NamePart Link
Hook Up Wire, Black, 22 AWG, 25 ft, strandedBuy NowBuy Now
Hook Up Wire, Red, 22 AWG, 25 ft, strandedBuy NowBuy Now
Hook Up Wire, Red, 22 AWG, 25 ft, solid
Buy NowBuy Now
Hook Up Wire, Black, 22 AWG, 25 ft, solid
Buy NowBuy Now
Duratool 7" Diagonal Cutters
Buy NowBuy Now
Duratool Flush Cutters
Buy NowBuy Now
Duratool Mini Side CuttersBuy NowBuy Now
Wire strippers, Duratool 10-22 AWGBuy NowBuy Now
Wire strippers, Duratool 18-30 AWGBuy NowBuy Now
Wire strippers, Klein 11046, 16-26AWGBuy NowBuy Now
Wire strippers, Duratool 5-in-1, Automatic Wire StripperBuy NowBuy Now
Duratool Wire Stripper, Parrot-Type, Automatic, 0.2-6mm, 25mm LengthsBuy NowBuy Now
Small Breadboard - 170 PinBuy NowBuy Now
Small Breadboard w/ Power Rails, 30 rowsBuy NowBuy Now
Large Breadboard w/ Power Rails, 60 rowsBuy NowBuy Now
Needle nose pliers, long, skinny noseBuy NowBuy Now
Needle nose pliers, heavy w/ teethBuy NowBuy Now

 

 

Solid wire consists of a single strand or core of wire, insulated with non-conductive material.    Its cheaper to manufacture and provides mechanical ruggedness, due to less surface area to be exposed to corrosives or environment. A stranded wire tends to be a better conductor than solid wire as the individual wires comprise a greater surface area.  It’s good for connections between circuit boards where rigidity could cause stress due to movement.

Electrical wire typically has an insulative cover that has to be removed to access the conductive metal inside.  Conductors are materials characterized by their low opposition to electrical flow. Conductive means that electricity can flow through like with metals.  Insulators are known for their capacity to stop the flow of current.   Electrons flowing through a conductor or wire tend to generate heat.  Thicker wires handle the heat better than thinner wires.  Thinner wires can even burn up if too much electricity flows through them.   Rubbers and plastics used as insulative materials.

Karen goes over different examples of needle-nose pliers.  For doing electronics work, small and narrow pliers work best.  They allow you to get into tight spots in circuits and they make it easier to manipulate parts and wire.   If using very small components, such as surface mount components, you may decide to use tweezers for a more precise grip.  However, you may find that using needle nose pliers will give you a stronger, more secure grip on those same parts.  The heavy-duty needle nose pliers also come with a built in wire cutter that can be pretty handy.  Wire cutters are also referred to as snips, side-angle cutters, or flush cutters. With flush cutters, the blades come together in a manner where they cut flush.  The rest of these are side angle cutters. You can see that the blades do not come together at the face of the cutter. For electronics, again, smaller tends to be better.

Large pairs give you more leverage, making it easier to cut thick wire.  Smaller pairs allow you to get in closer to your circuit making it easier to trim off the little bits. Breadboards come in different sizes but pretty much function the same.  Wire strippers, are the simplest and least expensive. They can function as both wire cutters and wire strippers.   On the side there are two columns which are each connected.  The negative blue column is all connected and the red positive column is all connected.  These are intended to be used for power and ground.  In the center there are rows, most often with five holes, where all five holes in each row are connected.  Breadboards come in different sizes but they all pretty much function the same.

  • needle-nose pliers
  • stranded wire
  • stem_projects
  • tlc
  • diagonal cutters
  • current
  • circuits
  • side cutters
  • conductive
  • flush cutters
  • non-conductive material
  • electrical wire
  • duratool
  • solid wire
  • e14presents_makerkaren
  • conductive metal
  • hook up wire
  • mini side cutters
  • heckwithkaren
  • karen corbeill
  • circuit
  • electrical flow
  • the learning circuit
  • theheckwithkaren
  • breadboard
  • insulators
  • electrons
  • wire strippers
  • insulated
  • conductors
  • thelearningcircuit
  • awg
  • beginner
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago in reply to jw0752 +5
    For some tools with such direction, I've stuck on a label on one side of the tool with the writing "insulation" : ) That way I always know if I'm holding the tool right, because I put the end that will…
  • jw0752
    jw0752 over 8 years ago in reply to shabaz +5
    I am pleased to hear that I am not the only one with a labeling obsession. John
  • jw0752
    jw0752 over 8 years ago in reply to mcb1 +4
    Excellent technique Mark. As I have gotten older and have more pain in my hands I have taken to holding the wire with a needle nose and using it as a lever against the cutter to pry the insulation off…
Parents
  • beacon_dave
    beacon_dave over 8 years ago

    When talking about breadboard, you may want to mention that the power rails along the edges aren't always continuous. A number of larger breadboard designs have a break halfway along the power rails, which has to be bridged with a link to continue the power rail onto the second half. Always a good idea to check for this if your circuit doesn't appear to be working as expected as it catches a lot of learners out.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 8 years ago in reply to beacon_dave

    I haven't encountered that. Thanks for the tip!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • makerkaren
    makerkaren over 8 years ago in reply to beacon_dave

    I haven't encountered that. Thanks for the tip!