The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents Wigglebots -- The Learning Circuit 03
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 7 Dec 2017 11:27 PM Date Created
  • Last Updated Last Updated: 20 Dec 2017 8:24 AM
  • Views 5123 views
  • Likes 19 likes
  • Comments 7 comments
Related
Recommended

Wigglebots -- The Learning Circuit 03

image

element14's The Ben Heck Show

Join Karen as she shares her enthusiasm for teaching STEM subjects, gives you what you need to know to get started on electronics projects, and more.

Back to The Ben Heck Show homepage image

The Learning Circuit
Featured Bonus Content
See All Episodes

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Now that it's the holidays, kids will be at home all day, looking for something to do.  Karen shows you some projects that you can do with your kids or if you are around someone else's kids.  Wigglebots, are so much fun, you can even do them yourself if no kids are available.  Sure, there are toys on the market that wiggle, such as hex bugs, but why buy it if you can build it yourself!

Make Your Own!

Parts & Products:

Product NamePart Link
Supercapacitor, 5 F, 2.7 VBuy NowBuy Now
Mini Breadboard - 25 pointBuy NowBuy Now
Small Breadboard - 170 PinBuy NowBuy Now
Small Breadboard w/ Power RailsBuy NowBuy Now
2 AA Battery Holder
Buy NowBuy Now
Black Vinyl Electrical Tape
Buy NowBuy Now
Male/Male Jumper Wires
Buy NowBuy Now
Head Pin Jumper
Buy NowBuy Now
CR2032 3V Battery w/ PinsBuy NowBuy Now

 

Parts Not Sold by element14

Product NameSupplierPart Link
Vibrating Mini Motor DiscAdafruitProduct Link
Bristlebot Kit (4pk)AdafruitProduct Link
Battery-powered Toothbrush w/ vibrating motor
Dollar TreeProduct Link

 

 

To build your own Wigglebot, all you need is a battery and a motor.  Karen pulls out some DC motors that she's taken out of some common objects.  She's pulled a DC motor out of a cheap electric toothbrush that she found at the dollar store, some motors from video game controllers lying around the shop, a motor from a cell phone, and a computer fan. The computer fan won’t work as is, they’ll need to break some of the fan blades off so that it’s off balance. Vibrating motors work like DC motors, but a weight is placed on the end causing it to vibrate when it spins. Once you've found your motor, make sure that your battery has enough voltage to make it run. A lot of motors have an optimal rating, but a lot of times you can use a different voltage, such as a 9 volt battery to run a 12 volt fan. When you are connecting your motor to your battery pack, make sure your ends are long and stripped. Once your wires are twisted together be sure to cover it in electrical tape. This will keep it together and help prevent red wires from touching black wires.  You don't want the red wires touching the black wires because that will cause a short and make it not work.  You can then decorate your Wigglebot using stuff around the house such as pipe cleaners, pom-pom balls, popsicle sticks, paper clips, and googly eyes. You can even use electrical parts like old resistors, whatever you have lying around the house.

For kids looking to do more, kick it up a notch by adding a capacitor.  Both capacitors and batteries store electrical energy but work in completely different ways. Batteries have two terminals, chemical reaction inside the batteries produce electrons on one terminal and absorb electrons on the other terminal. Capacitors cannot produce electrons, they can only store them.  Capacitors usually have two ratings, voltage and something called farads, a unit of measurement of capacitance.  For this project, select a capacitor that is rated for approximately the voltage you'll be using, and has high capacitance.  For example, Karen is using a capacitor that’s rated for 5 farads and 2.7 volts.  In this new circuit, they’re going to replace the battery with the capacitor. Because the capacitor only stores energy, they'll need to get energy to it by hooking up a battery to their circuit.  They can then connect the capacitor to the motor.

To build the circuit they're going to use a breadboard.  Karen pulls out three different types of breadboards.  The first one is a tiny breadboard with the numbers 1 2 3 at the bottom of the columns.  This is there so that you know that each of the columns is connected.  The next one has five holes that are connected on the left side and 5 that are connected on the right.  The left side and the right side are not connected.  A more traditional breadboard has power rails on the side. They still have their rows of 5 holes connected on the left and the right side but up the far sides there are power rails. On this breadboard, all of the holes in the column next to the red line are connected and all of the holes next to the blue line are connected.  They are intended to be used for power and ground.

She’s going to use the tiny breadboard for her circuit.  She’s plugs in the motor and then the capacitor.  She wants one of the leads of the capacitor to be in the same row as one of the leads from the motor. Using two jumper wires, she plugs one into the same row as the second lead of the capacitor. The other one she’s going to plug into the second lead of the motor.  She can then use a jumper to connect the two of them to complete the circuit when she’s ready to use her capacitor as her power source.  Once her circuit is all set up all she needs to do is plug a jumper on to connect the two wires.  Before she does that she needs to make sure that she charges up her capacitor so that it can actually power the motor. She plugs the leads of the battery into the breadboard to charge the capacitor.

  • capacitor
  • breadboards
  • e14presents_makerkaren
  • dc motors
  • circuit
  • resistors
  • holiday projects
  • the learning circuit
  • theheckwithkaren
  • battery
  • voltage
  • holidayspecialch
  • capacitance
  • stem projects
  • vibrating motors
  • thelearningcircuit
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • ninjatrent
    ninjatrent over 8 years ago +5
    Great video. These wigglebots look like more fun than the commercially produced ones at the store. A build your own wigglebot kit would make an excellent gift for kids. Karen's Dinosaur Sweater is the…
  • DAB
    DAB over 8 years ago +5
    Very good episode. Karen did a good job of describing the circuits and showing many build options. Well done. DAB
  • fmilburn
    fmilburn over 8 years ago +2
    Thanks Karen, I am off to the dollar store to look for toothbrushes!
Parents
  • ibfonz
    ibfonz over 6 years ago

    I have never learning quite like this

     

     

    Thank you karen

    Thank you element 14

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ibfonz
    ibfonz over 6 years ago

    I have never learning quite like this

     

     

    Thank you karen

    Thank you element 14