• Products and Partners
    Products and Partners
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
The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents Basic Soldering Tools -- The Learning Circuit 06
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 27 Feb 2018 9:51 PM Date Created
  • Last Updated Last Updated: 28 Feb 2018 8:24 AM
  • Views 3583 views
  • Likes 14 likes
  • Comments 10 comments
Related
Recommended

Basic Soldering Tools -- The Learning Circuit 06

image

element14's The Ben Heck Show

Join Karen as she shares her enthusiasm for teaching STEM subjects, gives you what you need to know to get started on electronics projects, and more.

Back to The Ben Heck Show homepage image

The Learning Circuit
Featured Bonus Content
See All Episodes

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Ben joins Karen to discuss soldering. In past episodes, Karen has shown you tools and techniques needed to make projects that have temporary electrode connections. In electronics, for permanent connections you use a process called soldering. 

Karen's Toolkit:

 

Product Name

Part Link

Duratool Solder Wire, 60/40 .032"

Product LinkProduct Link

Tenma Solder Wire, 60/40 leaded, 1mm/.04", 6oz

Product LinkProduct Link

Tenma Solder Wire, 60/40 leaded, 1mm/.04", 1lb

Product LinkProduct Link

Tenma 40W Soldering Pencil

Product LinkProduct Link

Tenma 50W Soldering Station

Product LinkProduct Link

Tenma 60W Soldering Station w/ LCD Display

Product LinkProduct Link

Duratool Soldering Tip Cleaner w/ Brass Sponge

Product LinkProduct Link

Duratool Helping Hands

Product LinkProduct Link

Chemtronics Solder Wick Bobbin

Product LinkProduct Link

Duratool Aluminum Body Desoldering Pump

Product LinkProduct Link
Tenma Vacuum Desoldering IronProduct LinkProduct Link
Tip Tinner/CleanerProduct LinkProduct Link

 

 

The main options for soldering tools are soldering pencils and soldering stations.  If you’re just getting started soldering or if you’re on a budget, you can start with a cheap handheld soldering iron.  Ben cautions on going too cheap on a soldering iron.  They start at around 15 watts and can go up to 80 watts, more wattage than you'd want to use for electronics.  According to Ben, 20 to 40 watts is probably the sweet spot.  Wattage refers to the current your soldering tool draws, letting you know how much power it has in order to melt solder. The higher the wattage, the more solder it can melt or the faster it will melt it.  One thing you need to check for is that the plug for your soldering iron has a ground pin.   If a device has exposed metal then it’s good for it to have a grounded plug because that allows static to discharge into the earth instead of building up on your tool. Reasons you’d want to get a soldering pencil is that they are cheaper, they are easier to store, and they come with a stand which you want to be sure to use.   You don’t want to set a soldering pencil on the table.  Some of the drawbacks include the fact that they don’t have a variable temperature control.

Ben and Karen take a look at three different models of soldering stations.  If you’re using a soldering station, you always have a place to store your soldering iron, and many of them come with a place to put a sponge or a brass pad.  Each station has some sort of temperature control, how fine that is will depend on the model.  The 21-7945 Tenma Soldering Station21-7945 Tenma Soldering Station uses knob control that goes from yellow up to red, so you don’t get the exact temperature.  The 21-10115 Tenma Soldering Station21-10115 Tenma Soldering Station has a digital display.  Karen likes it because it gives you three preset temperatures but also allows you to fine-tuning of the temperature.  Ben notices that it has a transformer in it.  This is good because a transformer allows you to have higher current faster, allowing it to heat up quickly.   If a soldering iron is “heavy” that means it has a nice transformer in it which is going to get you up to temperature quickly.  The next soldering station that they look at is the Weller WD 1000Weller WD 1000. Ben uses a Weller with digital knob control at his desk because he likes the tip options on it.  He appreciates the digital readout on the Weller WD because oftentimes he will go back and forth between set temperatures.

Once you select your soldering tool, you’re going to want to make sure you get some spare tips. Its important to have a good clean tip when soldering and if you’re a beginner, it’s really easy to accidentally corrode and ruin your tips.  But it’s not just about replacing tips if they go bad.  You’re going to also want to have different tips for different applications.  A finer point tip can be used for detailed work while a larger tip is used to transfer heat more quickly.  Recently, Felix has been using a tip that is tapered and kind of like a blade.   This is nice because it offers more surface area and heats pads really well.   Karen goes over some additional things you should look for when selecting your soldering tip. Make sure you get a tip that matches the tool you have because tips can vary wildly by manufacturer.

As mentioned earlier, keeping your soldering tip clean is important in soldering. There are two main products you can use to do this.  You can get a sponge which you can get damp or you can get a brass pad. Ben prefers to use a sponge because he can actually see everything coming off.  If you need more than a sponge or a brass pad you can purchase tip tinner and cleaner.  You could also use soldering paste flux on the tip. You can also purchase solder that has flux in it. There are two main types of solder are leaded solder and lead-free solder.  Leaded solder is kind of the old fashioned way of doing it’s sometimes a little bit easier because lead has a lower melting point than the lead-free solder.  However, there’s a slight health risk as lead is not good for you. If you’re going to be using it then make sure you’re not touching your face, eating or drinking while using it, and wash your hands when you are done.  Sometimes you need a little more than a sponge or a brass pad to clean your tip.

  • weller
  • soldering tip
  • lead-free solder
  • duratool
  • vacuum desoldering
  • e14presents_makerkaren
  • soldering station
  • solder tip wire
  • tenma
  • soldering paste flux
  • thelearningcircuit
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 8 years ago +5
    Top tip - always pick up the soldering iron by its handle and not by the hot end !
  • jw0752
    jw0752 over 8 years ago +3
    Hi Karen, Excellent job of going over the basics of soldering tools and tip maintenance. John
  • beacon_dave
    beacon_dave over 8 years ago in reply to shabaz +3
    Yes, I thought it was a bargain. The 'minor cosmetic damage' turned out to be a 20mm rip in its cardboard box. I recall its predecessor. This one has been streamlined somewhat, but retains some of the…
Parents
  • magiotcz
    magiotcz over 7 years ago

    Thanks for the video. Do you have any experience with this?

    https://www.coldheat.com/. Does it work ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • magiotcz
    magiotcz over 7 years ago

    Thanks for the video. Do you have any experience with this?

    https://www.coldheat.com/. Does it work ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • makerkaren
    makerkaren over 7 years ago in reply to magiotcz

    Hm, I hadn't heard of that type before. Sounds interesting. I'd love to try one out!