• Products and Partners
    Products and Partners
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
The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents How Diodes Work -- The Learning Circuit 23
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 25 Sep 2018 5:00 PM Date Created
  • Last Updated Last Updated: 26 Sep 2018 7:24 AM
  • Views 3567 views
  • Likes 13 likes
  • Comments 4 comments
Related
Recommended

How Diodes Work -- The Learning Circuit 23

image

element14 Presents

Learn basic electronics, explore STEM subjects, get what you need to know to get started on electronics projects, and more.

Back to element14 Presents homepage image

The Learning Circuit
sudo Sergeant
The Ben Heck Show

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Karen goes over how diodes work and shows you what happens when you hook it up to a power supply in a circuit. Diodes have two axial leads coming out of both ends with a stripe in the middle to indicate which end is the cathode, or the negative end.    A diode is an electrical component that allows current to flow in one direction but not the other.  Diodes are made with a semiconductor material, mostly silicon but sometimes other materials such as germanium, selenium, or gallium arsenide.  .

 

Additional Resources:

 

Diodes and Bipolar Junction Transistors (BJTs) - Measuring the Temperature Coefficient


Semiconductors typically have four valence electrons in their outer shell.  Silicon, being a semiconductor, also has four outer valence electrons.  This outer shell can hold up to eight electrons. Electrons are most stable when their outer valence shell has eight electrons, a rule known as the octet rule. Each silicon atom shares an electron to its neighboring silicon atom in order to satisfy the octet rule.  When silicon atoms form covalent bonds they crystallize into a very strong structure known as a crystal or a lattice.

imageimage

 

In the P-type region silicon is doped with boron or gallium.  Boron and Silicon have only three outer electrons.  When mixed to a silicon lattice, they form “holes” in the crystal structure electron has nothing to bond to.  The absence of electrons gives it a positive charge.  In the N-type region silicon is doped with antimony, phosphorus, or arsenic. The fifth electron becomes a free electron.  It is free to go wherever the current takes it.  These free electrons are negative charge carriers.

The point where the N-Region and the P-Region meet is called the PN Junction. Near the junction the positive charges and the negative charges, having opposing charges are drawn to each other like magnets. The free electrons in the N-type region migrate over and fill the holes in the P-type region.  Because of the charged particles moving around, the area near the junction in the P-type region becomes slightly negatively charged while the area near the junction in the N-type region becomes slightly positively charged.  This area is known as the depletion zone. Eventually, the depletion zone becomes charged enough to stop electron migration. In a silicon diode this happens at around .7 Volts.

 

  • stem_projects
  • tlc
  • boron
  • e14presents_makerkaren
  • semiconductors
  • circuit
  • gallium
  • doping
  • battery
  • n-type region
  • susbstitution box
  • silicon
  • pn junction
  • diodes
  • p-type region
  • thelearningcircuit
  • depletion zone
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 8 years ago +5
    Hi Karen, Nice tutorial Here is a simple circuit that uses two diodes: Solar Bubble Blaster One to prevent current leakage back through the solar cell and a zener to prevent overvoltage in the supercapacitors…
  • hds0405
    hds0405 over 8 years ago +2
    Karen, this is an excellent overview and one of the best tutorials on how PN junctions in diodes work. I like that you took the time to illustrate 'why' they perform that way instead of asking the audience…
  • spark23ca
    spark23ca over 6 years ago +1
    i'm not very advanced ....i'm just working on a simple snowmobile ..like all newer things it has an ecm or computer ..someone was helping me fix it ..and bless them they hooked the battery up backwards…
Parents
  • spark23ca
    spark23ca over 6 years ago

    i'm not very advanced ....i'm just working on a simple snowmobile ..like all newer things it has an ecm or computer ..someone was helping me fix it ..and bless them they hooked the battery up backwards...blew a few fuses ..and a diode i found doesn't have continuity on either side ..i bought a new diode and it has continuity on one side as its supposed to ..i assume its there to protect the computer from getting over charged when using the starter which will draw up to 15 volts when its cold outside ..funny thing is ..the engine still starts but the lights have a delay after the engine starts ..almost like it has to build up enough volts to power go to the lights ....i don't know its one thing thats wrong i hope this fixes it ..this has given me some clues of the sporadic behavior of the lights ..i thank you very much

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • spark23ca
    spark23ca over 6 years ago

    i'm not very advanced ....i'm just working on a simple snowmobile ..like all newer things it has an ecm or computer ..someone was helping me fix it ..and bless them they hooked the battery up backwards...blew a few fuses ..and a diode i found doesn't have continuity on either side ..i bought a new diode and it has continuity on one side as its supposed to ..i assume its there to protect the computer from getting over charged when using the starter which will draw up to 15 volts when its cold outside ..funny thing is ..the engine still starts but the lights have a delay after the engine starts ..almost like it has to build up enough volts to power go to the lights ....i don't know its one thing thats wrong i hope this fixes it ..this has given me some clues of the sporadic behavior of the lights ..i thank you very much