The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents Making Logic Gates From Discrete Components -- The Learning Circuit 51
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rjena
  • Date Created: 23 Jul 2019 3:05 PM Date Created
  • Last Updated Last Updated: 24 Jul 2019 7:24 AM
  • Views 8251 views
  • Likes 9 likes
  • Comments 14 comments
Related
Recommended

Making Logic Gates From Discrete Components -- The Learning Circuit 51

image
Making Logic Gates From Discrete Components

The Learning Circuit | element14 presents |  Project Videos | VCP Biography: Karen

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In the previous lesson, Karen explained the logic behind AND, NAND, OR, NOR, NOT, XOR, and XNOR logic gates. In that episode, we also learned that logic gates are typically contained in IC chips, with multiple gates within each chip. For this episode’s project, Karen has decided to throw out the ICs, and instead, use transistors to create each logic gate, further demonstrating how the logic of each gate type works. Follow along to continue the journey of understanding logic gates through the use of transistors. Solder along and you’ll end up with a tidy little project contained within a couple of Altoid tins! In the end, Karen dares you to try your hand at creating the more complicated XOR and XNOR gates out of transistors. Are you up to the challenge?         

 

 

 

image

 

 

 

 

image

 

 

 

image

 

 

 

image

 

 

image

 

 

Bill of Materials

 

Product NameManufacturerQuantityBuy KitBuy Kit
Prototype Board, 25 x 15 grid, 1.6 mm, 72 mm, 47 mmMulticomp1Buy NowBuy Now
Prototype Board, Phenolic, 30 x 25 grid, 1.6 mm, 94 mm, 71 mmMulticomp1Buy NowBuy Now
Transistor, BC547, NPNMulticomp9Buy NowBuy Now
Hook Up Wire, Blue, 22 AWG, 25 ft, solidNTE ELECTRONICS1Buy NowBuy Now
Resistor Set, 480pcs, 16 x E3 Series Values, 1/4W Through Hole (1kohm, (2) 10kohm)Velleman1Buy NowBuy Now
Tactile Switch, 10mm, Blue, 24 VDC, 50mA, 2.54mmNKK SWITCHES2Buy NowBuy Now
Slide Switch, SPDT, 2.5mm, Through Hole, 6 pinE-SWITCH1Buy NowBuy Now
LED, Red, Through Hole, T-3 (10mm), 20 mA, 1.8 V, 640 nmClear Lens1Buy NowBuy Now
Board-To-Board Connector, 2.54 mm, 4 Contacts, Female-Receptacle, 1 RowsMulticomp10Buy NowBuy Now
Board-To-Board Connector, 2.54 mm, 4 Contacts, Male-Header, 1 RowsMulticomp2Buy NowBuy Now
9V battery snap, flexibleMulticomp1Buy NowBuy Now
Battery, 9 V, PP3, AlkalinePro Elec1Buy NowBuy Now

 

Additional Parts:

 

Product Name
Altoid Tins
  • transistor
  • element14 presesents
  • nor
  • e14presents_makerkaren
  • logic gates
  • nand
  • led
  • and
  • inverter
  • not
  • or
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +4
    Nice episode. When I started learning electronics back in the late 1960's, I purchased some surplus circuit boards that turned out to be Resistor-Transistor Logic (RTL) boards. I learned about logic design…
  • makerkaren
    makerkaren over 7 years ago in reply to ihaag +4
    This is something I found, but did not make myself. Give it a try and let us know how it turns out!
  • makerkaren
    makerkaren over 7 years ago in reply to clem57 +4
    I got the idea for the episode here. https://www.instructables.com/id/Logic-Gates-with-NPN-transistors/ But redrew all the schematics.
Parents
  • jloesel
    jloesel over 5 years ago

    Really great material. I really liked the modular design. So much so that I decided to use the idea to make an SR Latch. - Using 2 of the NOR gates.  Just be sure to insert second NOR gate reversed. i.e. The wiring is reverse for one of the NOR gates.  Otherwise, you will short one out very quickly..... and have to build another one.

     

    imageimageimage

     

     

     

     

     

    Finally, I decided to use the original base design and create a SR Latch component that plugs into the original base component from this tutorial. It was only slightly more complex than the gates in that you had to find space to solder an LED onto the board (which is pretty small already).  But the two builds together make a great demonstration of building an SR Latch from gates as well as directly from transistors.

    imageimage

     

    Great video and the component way of creating each of these circuits is perfect way to create projects in a school setting.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 5 years ago in reply to jloesel

    That's amazing! Thank you for sharing your project! And also thank you for sharing what you figured out NOT to do. Always helpful to learn from others' mistakes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • makerkaren
    makerkaren over 5 years ago in reply to jloesel

    That's amazing! Thank you for sharing your project! And also thank you for sharing what you figured out NOT to do. Always helpful to learn from others' mistakes.