WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Blog Are you still using 7400-Series Logic, if so, where?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: baldengineer
  • Date Created: 9 Dec 2020 7:50 PM Date Created
  • Views 9943 views
  • Likes 11 likes
  • Comments 37 comments
  • 7400 logic chips
Related
Recommended

Are you still using 7400-Series Logic, if so, where?

baldengineer
baldengineer
9 Dec 2020

Over the past several months, I have been learning about and repairing 8-bit computer and video game systems. So far, I have worked on the VIC-20, C64, ZX-81, Apple II, and have been learning about the TI 99/A.

 

It always amazes how much of these early computer systems were built almost entirely with standard 7400-series (LS and HC) chips.

 

Occasionally, I need to replace a 7400-series chip. (I always hope it is one of those and not one of the ASICs!) While looking for modern replacements, I have noticed the trend that they are becoming more scarce. The LS-series is almost entirely gone--and with good reason. While HC and HCT continue to be somewhat available, they are usually only available in surface-mount packages.

 

That leads me to the question: Who is still using the venerable 7400-series logic chips today?

 

To me, there are three groups that might be using them:

  1. Learning. Students and hobbyist learning about digital logic
  2. New Design. Hardware that needs glue-logic. Are these using multi-gate chips or the single-gate variants?
  3. Repair. Older electronics in need of replacements. Here is where I mostly sit.

 

Do you fit into one of those categories? If not, where do you land?

 

And THEN, which chips are the must-have on-hand?

Obviously, the answer depends on how you might be using them. But, I'm curious to know how you use 7400-series chips and which ones would you keep in stock?

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 5 years ago +13
    The high spot of my 74xxx design works was about 1987 when I designed this beastie. Subsequent designs used FPGAs or micro-controllers. I was lucky enough to find one on Ebay recently, not quite working…
  • shabaz
    shabaz over 5 years ago +8
    Here an electronics chain called Maplin was selling 74-series TTL right until 2018, when it closed for good! I guess people were still buying them, perhaps to repair old equipment. I think this is the…
  • ralphjy
    ralphjy over 5 years ago +7
    I just used a couple of 4000 series logic chips in the Pong game that I rebuilt. And I have an assortment of 74 and 74LS (even some 54 mil grade parts) from the late 70s and early 80s when I did a lot…
Parents
  • koudelad
    koudelad over 5 years ago

    I have never used nor seen these logic chips in anything I disassembled that was designed in last 10 years or more. I personally used micro-controllers, but as other say, high speed designs need CPLD or an FPGA.

    One great alternative is a PSoC or other MCUs with some kind of configurable logic cells.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ajcc
    ajcc over 5 years ago in reply to koudelad

    You might just not have seen them, as an example and because it's right next to me, there are a handful of 74-series logic ICs on the BeagleBone Black. The BBB is open source hardware so the full schematic is available for download.

     


    Green ring is a SN74LVC1G07 Single Buffer/Driver With Open-Drain Output
    Red ring is a SN74LVC1G06 Single Inverter Buffer/Driver With Open-Drain Outputimage

     

    image

    Yellow ring is a SN74AUC1G74 Single Positive-Edge-Triggered D-Type Flip-Flop with Clear and Preset

    Blue ring is a SN74LVC2G241 Dual Buffer and Driver With 3-State Outputs

     

    Now the packages doesn't say 74-something on them, instead they have catchy names like cf5, CV5 or C14b.

     

    While searching for the parts I even found a nice sales brochure from Texas Instrument that talks about how their Little Logic ICs can be used in modern applications.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ajcc
    ajcc over 5 years ago in reply to koudelad

    You might just not have seen them, as an example and because it's right next to me, there are a handful of 74-series logic ICs on the BeagleBone Black. The BBB is open source hardware so the full schematic is available for download.

     


    Green ring is a SN74LVC1G07 Single Buffer/Driver With Open-Drain Output
    Red ring is a SN74LVC1G06 Single Inverter Buffer/Driver With Open-Drain Outputimage

     

    image

    Yellow ring is a SN74AUC1G74 Single Positive-Edge-Triggered D-Type Flip-Flop with Clear and Preset

    Blue ring is a SN74LVC2G241 Dual Buffer and Driver With 3-State Outputs

     

    Now the packages doesn't say 74-something on them, instead they have catchy names like cf5, CV5 or C14b.

     

    While searching for the parts I even found a nice sales brochure from Texas Instrument that talks about how their Little Logic ICs can be used in modern applications.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • koudelad
    koudelad over 5 years ago in reply to ajcc

    Thank you for a great example and the sales brochure! I definitely didn't want to sound like there is no place for logic chips, just that they are more and more integrated to save board space and cost.

     

    It is not 100 % related, but there is also a TI's app note / brochure that suggested replacing all other small chips with their MSP430 - for example various timers, slow logic circuits, debouncers for buttons etc. The goal is to have fewer unique parts on a BOM (even more that one piece). I just can't find it right now.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ajcc
    ajcc over 5 years ago in reply to koudelad

    Things are getting more integrated indeed. On the BBB they are used for inverting and buffering reset signals, disconnecting TX and RX when the unit is powered off, dividing and buffering a clock signal and voltage translating a 3v3 power good signal down to 1v8. So they are all used for solving some issue.

     

    I love the MSP430 and I have a couple of LaunchPads, so if anyone knows where to find that app note / brochure I'd love to have it. I should really do more projects with the MSP430 anyway.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago in reply to koudelad

    When you can get an MCU for $1 or a PSoC4 on a card with all programming infrastructure and free development tools all for $4, there really is a case to be made to dump discrete logic. Although I have to say I like designing with logic gates and chips and optimizing digital designs. One could argue that FPGAs are the way to go, but I still haven't found FPGA tools I like.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 5 years ago in reply to ajcc

    I had to google for about an hour to find the right keywords, but... here it is!

     

    It is called Enhance simple analog and digital functions for $0.25

    • Cancel
    • Vote Up +3 Vote Down