WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays

Blog

  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Simple Analog Discovery 3 3D printable model

    Making an Analog Discovery 3 prop to "tear down."

    baldengineer
    baldengineer
    In Workbench Wednesdays #76, I looked at Diglent's Analog Discovery 3. This device is a long-anticipated, by me anyway, update to their incredibly powerful and useful Analog Discovery 2. One of the first things that struck me about the AD3 is that th...
    • 26 Jul 2023
  • oscilloscope videos

    Bald Engineer’s Oscilloscope Videos

    baldengineer
    baldengineer
    Every oscilloscope video (and tutorial) created by Bald Engineer (James). Learn about acquisition modes, trigger types, and more. There are also "application" videos where you can see scope measurements on real circuits.
    • 28 Feb 2023
  • Selecting electrolytic capacitor replacements (for a TRS-80 Model 100) [Full Video]

    Selecting electrolytic capacitor replacements (for a TRS-80 Model 100) [Full Video]

    baldengineer
    baldengineer
    In the "How to Pick Replacement Electrolytic Capacitors" video, I went through the process I use for selecting replacement aluminum electrolytic capacitors. My focus was why electrolytic wear out (or fail) AND what to consider when choosing a new one...
    • 28 Feb 2023
  • Solderable Protoboard Examples

    Op Amp Proto Board (SOIC-8)

    baldengineer
    baldengineer
    In the Slew Rate vs Rise Time video, I used this little breakout board. The bottom side is a continuous copper plane. On the top, the square pins have solder pads that you can connect to the top and bottom copper pour. The idea is to provide as much ...
    • 25 Jan 2023
  • Automated bode plot with a Pi 400, SCPI, and Python

    Automated bode plot with a Pi 400, SCPI, and Python

    baldengineer
    baldengineer
    In the Bode Plots episode, I used The Intern to measure multiple frequency points. The process is not only time-consuming, but it is also very error-prone. Originally, I wanted to show a Python script that automates the entire measurement in that vid...
    • 29 Nov 2022
  • I need your ideas on how to test flux!

    baldengineer
    baldengineer
    I have been thinking about an episode that compares different types of flux. Primarily I want to compare rosen, water-soluble, and no clean. I need your help with at least two aspects. First, what to cover. The two key areas I am thinking about are ...
    • 25 May 2022
  • 7 reasons why I like the ATmega128Dx MCUs

    baldengineer
    baldengineer
    Microchip introduced the ATmega128Dx in three variants: -DA, -DB, and -DD. These 8-bit microcontrollers can run at 5 volts and have several compelling features. While no "official" Arduino board exists based on these chips, an open-source p...
    • 16 Jun 2021
  • Quick: what's your best desoldering braid/wick tip or trick?

    baldengineer
    baldengineer
    Since last March 2020, I have been live-streaming three days a week. My streams are all electronics related but include retro computer repairs, soldering kits, Arduino coding, explaining measurements, and other electronics stuff. Several of the recen...
    • 1 Feb 2021
  • Are you still using 7400-Series Logic, if so, where?

    baldengineer
    baldengineer
    Over the past several months, I have been learning about and repairing 8-bit computer and video game systems. So far, I have worked on the VIC-20, C64, ZX-81, Apple II, and have been learning about the TI 99/A. It always amazes how much of these...
    • 9 Dec 2020
  • What are the most important parts to have in your electronics kit?

    baldengineer
    baldengineer
    This weekend I went to build a circuit for use in an upcoming video. There were two components I was confident that were in my parts kit: a 555 timer and a counter. Now, I did not know which counter I had, but I assumed I must have at least one decad...
    • 29 Jul 2020
  • Reverse engineering the MP730026 DMM's BLE data packets

    baldengineer
    baldengineer
    The MP730026 DMMMP730026 DMM supports BLE communication. However, I quickly learned that the software offered by Multicomp Pro has significant limitations. So I set out to find a cross-platform solution, which leads me to Python. In the MP730026 DMM ...
    • 9 Mar 2020
  • MP730026 DMM BLE Tutorial using Python

    baldengineer
    baldengineer
     At a glance, the Multicomp Pro MP730026 seems like a typical DMM. And it is! It measures voltage, current, frequency, temperature (with included K-Type thermocouple), and even features a white LED to act as a work light. The non-typical feature...
    • 9 Mar 2020
  • How are linear regulators and switching supplies different?

    baldengineer
    baldengineer
    Every electronic device includes a DC-DC converter for its power supply. That supply might come from a USB port, a "brick", a wall-wart, or in larger systems, there could be multiple point-of-load converters scattered around a single circuit board.&n...
    • 19 Dec 2019
  • SAR vs. Sigma-Delta ADC -- What is the difference anyway?

    baldengineer
    baldengineer
    Analog-to-digital converters (ADCs) enable a wide range of electronics applications. They make it possible for devices to interact with their environment. Most sensors convert a physical quantity into a voltage.  While it is certainly possible t...
    • 9 Oct 2019
  • Reading MOSFET Curves

    baldengineer
    baldengineer
    Semiconductor Measurementselement14 Presents  |  Bald Engineer: James Lewis' VCP Profile |  Workbench Wednesdays A good MOSFET datasheet is excellent when it contains detailed information. However, too much information might mea...
    • 4 Aug 2019
  • Measuring an aluminum electrolytic capacitor's ESR

    baldengineer
    baldengineer
    One of my hobbies is collecting vintage computers. Computers in my collection include the Apple IIgs, Atari 400, TI 99/4A, Commodore 64 and Sinclair ZX-81 to name a few of the popular ones. Like all electronics, these systems contain capacitors. Anyo...
    • 19 Jun 2019
  • Picking aluminum polymer electrolytic capacitors for the C64

    baldengineer
    baldengineer
    Capacitor Replacement on a Commodore 64 - A Lesson in Through-Hole SolderingWorkBench Wednesdays |  Bald Engineer: James Lewis' VCP Profile |  Project Videos  In WorkBench Wednesdays , one of my mini-projects was to replace the...
    • 13 Mar 2019