WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Blog Are you still using 7400-Series Logic, if so, where?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: baldengineer
  • Date Created: 9 Dec 2020 7:50 PM Date Created
  • Views 9561 views
  • Likes 11 likes
  • Comments 37 comments
  • 7400 logic chips
Related
Recommended

Are you still using 7400-Series Logic, if so, where?

baldengineer
baldengineer
9 Dec 2020

Over the past several months, I have been learning about and repairing 8-bit computer and video game systems. So far, I have worked on the VIC-20, C64, ZX-81, Apple II, and have been learning about the TI 99/A.

 

It always amazes how much of these early computer systems were built almost entirely with standard 7400-series (LS and HC) chips.

 

Occasionally, I need to replace a 7400-series chip. (I always hope it is one of those and not one of the ASICs!) While looking for modern replacements, I have noticed the trend that they are becoming more scarce. The LS-series is almost entirely gone--and with good reason. While HC and HCT continue to be somewhat available, they are usually only available in surface-mount packages.

 

That leads me to the question: Who is still using the venerable 7400-series logic chips today?

 

To me, there are three groups that might be using them:

  1. Learning. Students and hobbyist learning about digital logic
  2. New Design. Hardware that needs glue-logic. Are these using multi-gate chips or the single-gate variants?
  3. Repair. Older electronics in need of replacements. Here is where I mostly sit.

 

Do you fit into one of those categories? If not, where do you land?

 

And THEN, which chips are the must-have on-hand?

Obviously, the answer depends on how you might be using them. But, I'm curious to know how you use 7400-series chips and which ones would you keep in stock?

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 5 years ago +13
    The high spot of my 74xxx design works was about 1987 when I designed this beastie. Subsequent designs used FPGAs or micro-controllers. I was lucky enough to find one on Ebay recently, not quite working…
  • shabaz
    shabaz over 5 years ago +8
    Here an electronics chain called Maplin was selling 74-series TTL right until 2018, when it closed for good! I guess people were still buying them, perhaps to repair old equipment. I think this is the…
  • ralphjy
    ralphjy over 5 years ago +7
    I just used a couple of 4000 series logic chips in the Pong game that I rebuilt. And I have an assortment of 74 and 74LS (even some 54 mil grade parts) from the late 70s and early 80s when I did a lot…
Parents
  • dougw
    dougw over 5 years ago

    I still have some 7400 parts but I have more 4000 (CMOS) series parts. I only use them when I am breadboarding since they are DIPs (almost all my newer stuff is SMT). I actually use PCBs for prototypes, so it is a bit rare for me to build circuits on a breadboard.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago in reply to dougw

    Are 7400HC the same as 4000-series? Or are there different gates in the 4000-series?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 5 years ago in reply to baldengineer

    I think 74C series is the equivalent of 4000-series, with a broad power supply voltage 3-15 V. However, HC is high speed and typically operates at 2 - 5 V.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago in reply to baldengineer

    4000 series had equivalent logic functions to 7400 but usually different pinout. 74C series retained the 7400 pinouts but used CMOS logic levels and voltages. Each series had some unique parts. I like 4000, 4500 and 74C series parts because they were much lower power and operated over a much wider range of voltages. 4000 series parts were not quite as fast as LS or S parts. One of the parts I used a lot and sill use is a 4040 ripple counter. Another would be 40106 which is equivalent to a 74C14 hex Schmitt trigger inverter. It is funny how I can still remember the logic function of many part numbers.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 5 years ago in reply to baldengineer

    4000 series had equivalent logic functions to 7400 but usually different pinout. 74C series retained the 7400 pinouts but used CMOS logic levels and voltages. Each series had some unique parts. I like 4000, 4500 and 74C series parts because they were much lower power and operated over a much wider range of voltages. 4000 series parts were not quite as fast as LS or S parts. One of the parts I used a lot and sill use is a 4040 ripple counter. Another would be 40106 which is equivalent to a 74C14 hex Schmitt trigger inverter. It is funny how I can still remember the logic function of many part numbers.

    • Cancel
    • Vote Up +4 Vote Down