WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Forum What’s an example of where you picked the wrong Op-Amp … and why?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 113 subscribers
  • Views 5843 views
  • Users 0 members are here
  • op amp
  • operational amplifier
  • multimeter
Related

What’s an example of where you picked the wrong Op-Amp … and why?

baldengineer
baldengineer over 3 years ago

I’m working on an episode about Op Amps and measuring some basic parameters. (For those like me who would rather measure something than go cross-eyed looking at a datasheet.)

Since there are more than a handful of op amps, I can imagine there are situations where people select one or re-use one without fully evaluating all of its characteristics. So, that got me thinking, what are some cases where you picked an op-amp for an application, but it was (clearly?) the wrong one… and why?

Bonus question: does anyone still use the ua741 … for anything?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +5
    Regarding the '741, yes : ) It was used for a very high-tech purpose, it was a key component: A Westworld / Futureworld Halloween
  • fmilburn
    fmilburn over 3 years ago +4
    I've been caught out trying to use op-amp as a comparator, although it sometimes works well enough. I have some comparators in my parts bin now. I'd be interested in seeing a small recommended list of…
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +3
    I am currently trying to decode USB-PD CC communication, which is a ~1.6V signal. To sample the signal with a logic analyzer I wanted to amplify it to a high level of 3.3V. My first choice with a component…
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    There is no substitute for risking the cross eyes by reading data sheets.

    There are loads of op amps and they are all different.

    There are a great mass of applications where the choice of op amp is quite flexible, but others are less so.

    In the present times of all sorts of parts being on long delivery it's even worse because availablity trumps everything else !

    To give an example, I have a current job where the key parameters are:

    low voltage noise (< 3nV rtHz @ 5kHz)

    work from 2.7V

    input common mode must include 0V

    rail to rail out

    > 50MHz GBW (200 would be nice)

    low input voltage offset

    less than 3mA supply current

    There are not many options !

    I can't think of any application where a 741 would be a good choice unless you have a tube of them gathering dust.

    The worst things about it, compared with modern op amps, are the limited input common mode range and limited output swing which means that the minimum supply voltage is 6V or +/- 3V (more realistically 10V or +/-5V).

    It is cheap.

    TI recommend the TLV9301, it's quite nice but not as cheap !

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 3 years ago

    There is no substitute for risking the cross eyes by reading data sheets.

    There are loads of op amps and they are all different.

    There are a great mass of applications where the choice of op amp is quite flexible, but others are less so.

    In the present times of all sorts of parts being on long delivery it's even worse because availablity trumps everything else !

    To give an example, I have a current job where the key parameters are:

    low voltage noise (< 3nV rtHz @ 5kHz)

    work from 2.7V

    input common mode must include 0V

    rail to rail out

    > 50MHz GBW (200 would be nice)

    low input voltage offset

    less than 3mA supply current

    There are not many options !

    I can't think of any application where a 741 would be a good choice unless you have a tube of them gathering dust.

    The worst things about it, compared with modern op amps, are the limited input common mode range and limited output swing which means that the minimum supply voltage is 6V or +/- 3V (more realistically 10V or +/-5V).

    It is cheap.

    TI recommend the TLV9301, it's quite nice but not as cheap !

    MK