WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Forum What’s an example of where you picked the wrong Op-Amp … and why?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 113 subscribers
  • Views 5850 views
  • Users 0 members are here
  • op amp
  • operational amplifier
  • multimeter
Related

What’s an example of where you picked the wrong Op-Amp … and why?

baldengineer
baldengineer over 3 years ago

I’m working on an episode about Op Amps and measuring some basic parameters. (For those like me who would rather measure something than go cross-eyed looking at a datasheet.)

Since there are more than a handful of op amps, I can imagine there are situations where people select one or re-use one without fully evaluating all of its characteristics. So, that got me thinking, what are some cases where you picked an op-amp for an application, but it was (clearly?) the wrong one… and why?

Bonus question: does anyone still use the ua741 … for anything?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +5
    Regarding the '741, yes : ) It was used for a very high-tech purpose, it was a key component: A Westworld / Futureworld Halloween
  • fmilburn
    fmilburn over 3 years ago +4
    I've been caught out trying to use op-amp as a comparator, although it sometimes works well enough. I have some comparators in my parts bin now. I'd be interested in seeing a small recommended list of…
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +3
    I am currently trying to decode USB-PD CC communication, which is a ~1.6V signal. To sample the signal with a logic analyzer I wanted to amplify it to a high level of 3.3V. My first choice with a component…
Parents
  • strb
    strb over 3 years ago

    Other that already mentioned bandwidth and slew rate, the one characteristic that once catched me unprepared was the internal compensation of the opamp. I was in lab at university and I had the opportunity to play with a quite fast opamp, so I went for it. But it wasn't single pole compensated! I did not notice it in the datasheet so my mic preamplifier turned out to be a "nice" oscillator :)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • strb
    strb over 3 years ago

    Other that already mentioned bandwidth and slew rate, the one characteristic that once catched me unprepared was the internal compensation of the opamp. I was in lab at university and I had the opportunity to play with a quite fast opamp, so I went for it. But it wasn't single pole compensated! I did not notice it in the datasheet so my mic preamplifier turned out to be a "nice" oscillator :)