WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Documents Win a Tenma Power Supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 19 Sep 2019 2:23 PM Date Created
  • Last Updated Last Updated: 19 Nov 2019 6:47 PM
  • Views 8060 views
  • Likes 15 likes
  • Comments 128 comments
Related
Recommended

Win a Tenma Power Supply

Congratulations to our winners!

Wow! You guys came up with some really creative ideas! There were over 100 individual ideas submitted and they were a blast to read through.

 

The winner of the Tenma Supply is Andrew J!

His submission literally made James laugh out loud: turning the supply into a mouse to scare a cat.

 

Congrats on your new supply!

 

But that's not all! We're going to find some element14 Community swag for the following honorable mentions:

neuromodulator

liamsenior

dougw

javagoza

 

This giveaway is closed.

Now that you know the basics of how to use a power supply, wouldn't it be great to have one to use on your very own bench?  Well, you are so lucky because James has one to give away!

Unsupported video URL format.

James is always looking for novel ideas for how to use the equipment on his work bench. . . so in this contest, he's asking for ideas on the most unique use for a power supply that maybe isn't just using it as a power supply.  (I don't think he means gutting it and using it for a potted plant.)

 

Add your suggestion in the comments below (no later than Friday, November 1) and you're entered with a chance to win.

 

James will select the winner and announce her/him on this page no later than November 14, 2019.

 

Learn More about the Tenma Power SupplyLearn More about the Tenma Power Supply

 

Full Terms and Conditions

  • giveaways
  • ww_giveaway
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 6 years ago +10
    I would like to set this power supply up to be able to rapidly test USB cable performance. I have a large collection of USB cables that is still growing. It seems every device comes with yet another USB…
  • baldengineer
    baldengineer over 6 years ago +9
    Wow! You guys came up with some really creative ideas! There were over 100 individual ideas submitted and they were a blast to read through. The winner of the Tenma Supply is Andrew J ! His submission…
  • Jan Cumps
    Jan Cumps over 6 years ago +8
    That is a very good PSU! also: I encourage baldengineer to give away *all* the equipment that we can see in the video
Parents
  • cyborg73703
    cyborg73703 over 6 years ago

    One of the most interesting ways I've used a benchtop PSU is to clean contacts on micro switches that measure out of spec.

     

    Being able to control current is key.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 6 years ago in reply to cyborg73703

    cyborg73703 Sounds interesting - can you describe your method?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cyborg73703
    cyborg73703 over 6 years ago in reply to dougw

    It takes a few sacrifical switches to figure out at which point of your max current causes damage when the switch contacts arc.

     

    But once you figure that out, set the voltage to the voltage the system runs at that the micro switch is in, and current you've come up with before it causes more harm than good.

     

    Usually micro switches see very little current as they're running relays commonly, so with the current supplied by the power supply this usually cleans corrosion, causing high resistance, off the contacts.

     

    Can be very valuable for expensive or obsolete switches.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 6 years ago in reply to cyborg73703

    Have you ever noticed this technique to have a negative effect, whereby the contact dirt carbonises further causing additional arcing and burning ?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago in reply to cyborg73703

    Hi Kyle,

    Wouldn't any arc capable of blasting off corrosion also produce enough heat to melt the metal of the contact? Then you would have a corroded and arc pitted contact which may not be very dependable. Surprisingly most switches can be taken apart and the contacts cleaned with a typewriter eraser if replacing them with a new switch isn't an option.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 6 years ago in reply to jw0752

    John, that's certainly what we have found on The Bombe which uses plenty of relays.  Any dirt or corrosion is cleaned with a diamond file.  If any contact is arcing it tends to weld those contacts shut!  I think Kyle is talking about sacrificing a few to find out the current where that doesn't happen but I'm amazed it actually cleans the contact.  Interesting....

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 6 years ago in reply to jw0752

    I was also taught to never file or use abrasive cleaners on switchgear contacts as that would damage the plating; doing so would also accelerate future damage. Instead to always use a proper switch cleaner, which I used to pull through on a piece of blotting paper if the dirt was stubborn.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to cyborg73703

    I don't recall any vendor solutions that use arching to clean contacts. Arching on contacts is a condition usually avoided.

     

    I have on occasion, rapped the side of a computer hard drive, in the hope the drive will spin up. The solution has yet to work for me. I have seen the rap technique work on vehicle alternators. I suspect in an system administration crisis lore the solution has unstuck a drive. I have yet to find a vendor that supports this troubleshooting solution. Would you spec the force of the rap in newtons or lbs per inch?

     

    I'm thinking this technique is anecdotal rather than a tried and true troubleshooting technique. In desperation all options are on the table. I would be rather reluctant to use a bench P.S. to arch switch contacts. It seems to be such a brute force solution. Then again, I have banged on the side of a failed hard drive because hope springs eternal.

     

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to 14rhb

    My electronics tickle trunk had a three inch strip of emery cloth tucked away in some obscure pouch. Burnishing the contacts on 48VDC relays after a spritz of contact cleaner was common in the 70's & 80's. Vacuum tubes were also common:) As electronic became more refined the large surface area on contacts of relays disappeared.

     

    I agree the contact surface of most relays or switches for that matter have very little material to apply the burnishing techniques that work in the past. I do recall being told never burnish contacts that were gold. The surface thickness wouldn't tolerate such a brute force technique.

     

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 6 years ago in reply to 14rhb

    I should say that these are 1940s relays!  And we would try and clean them with switch cleaner first.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Andrew J
    Andrew J over 6 years ago in reply to 14rhb

    I should say that these are 1940s relays!  And we would try and clean them with switch cleaner first.