WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Documents Win a Tenma Power Supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 19 Sep 2019 2:23 PM Date Created
  • Last Updated Last Updated: 19 Nov 2019 6:47 PM
  • Views 8541 views
  • Likes 15 likes
  • Comments 128 comments
Related
Recommended

Win a Tenma Power Supply

Congratulations to our winners!

Wow! You guys came up with some really creative ideas! There were over 100 individual ideas submitted and they were a blast to read through.

 

The winner of the Tenma Supply is Andrew J!

His submission literally made James laugh out loud: turning the supply into a mouse to scare a cat.

 

Congrats on your new supply!

 

But that's not all! We're going to find some element14 Community swag for the following honorable mentions:

neuromodulator

liamsenior

dougw

javagoza

 

This giveaway is closed.

Now that you know the basics of how to use a power supply, wouldn't it be great to have one to use on your very own bench?  Well, you are so lucky because James has one to give away!

Unsupported video URL format.

James is always looking for novel ideas for how to use the equipment on his work bench. . . so in this contest, he's asking for ideas on the most unique use for a power supply that maybe isn't just using it as a power supply.  (I don't think he means gutting it and using it for a potted plant.)

 

Add your suggestion in the comments below (no later than Friday, November 1) and you're entered with a chance to win.

 

James will select the winner and announce her/him on this page no later than November 14, 2019.

 

Learn More about the Tenma Power SupplyLearn More about the Tenma Power Supply

 

Full Terms and Conditions

  • giveaways
  • ww_giveaway
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +10
    I would like to set this power supply up to be able to rapidly test USB cable performance. I have a large collection of USB cables that is still growing. It seems every device comes with yet another USB…
  • baldengineer
    baldengineer over 6 years ago +9
    Wow! You guys came up with some really creative ideas! There were over 100 individual ideas submitted and they were a blast to read through. The winner of the Tenma Supply is Andrew J ! His submission…
  • Jan Cumps
    Jan Cumps over 7 years ago +8
    That is a very good PSU! also: I encourage baldengineer to give away *all* the equipment that we can see in the video
Parents
  • dougw
    dougw over 7 years ago

    I would like to set this power supply up to be able to rapidly test USB cable performance. I have a large collection of USB cables that is still growing. It seems every device comes with yet another USB cable.However not all cables are the same and sometimes they don't perform well enough, usually because they incur too much voltage drop when higher currents are drawn. I have tested lots of different USB cables to show how variable they can be, but what I really need is a way to quickly test cables. If the test isn't quick, I won't do it, and when a problem crops up, it always takes too much time to isolate it to the cable and then find a better cable.

    A dual supply allows the input and the output voltage of the cable to be monitored while the cable is in use by a target device. To do this one supply would be set for a voltage of 5V and a current limit of 1 A (or more if needed). The other supply would also be set for 5 V but the current limit would be set very small, say 1 mA. Each supply output would be connected to a USB connector so a cable could be connected between the supplies. The supply set to a small current would also be connected to the target device (but unable to supply enough current to power it) When a test USB cable is connected between supplies, the target device would get enough power to run.

    The target device current would be the sum of the currents from both supplies (basically the high current output plus 1 mA).

    The voltage to the target device would show on the low current supply voltage meter.

    The voltage drop in the cable would be the high current voltage minus the low current voltage.

    The voltage drop could also be determined by shorting the cable at the low current end instead of connecting it to the second supply and the load.

    In that case the high current supply would go into current limit and if the current was 1 A, its voltage display would equal the voltage drop in the cable.

    This application uses 2 supplies and both current meters and both voltage meters. and utilizes both voltage and current set points.

    To make the tests quick I would design a PCB with 2 sets of USB connectors and 2 sets of banana plugs. One set of connectors would have its power pins in parallel and connected to one set of banana plugs while the other set of USB connectors would also be connected in parallel, but connected to the other set of banana plugs. There would also be a switch to short out one side and an output USB connector for a target device.

    The tester would be able to test any cable by itself or any cable powering any target device simply by plugging the cable in or plugging in the cable and the target device.

    Here is a picture showing some of the USB connectors that might be installed on a PCB to mate to arbitrary USB cables:

    image

    Of course these connectors would also allow the power supply to power or charge several USB devices at the same time.

    • Cancel
    • Vote Up +10 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to dougw

    Love the suggestion. How about we combine your idea with mine to support any model of Raspberry Pi connected. An additional port could be added for testing cables.

     

    If we get selected we could do rock paper scissors to see who they ship the unit to:) Maybe it would be Christmas and Santa's elf made extraimage

     

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • colporteur
    colporteur over 6 years ago in reply to dougw

    Love the suggestion. How about we combine your idea with mine to support any model of Raspberry Pi connected. An additional port could be added for testing cables.

     

    If we get selected we could do rock paper scissors to see who they ship the unit to:) Maybe it would be Christmas and Santa's elf made extraimage

     

    Sean