WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Documents Essential Consumables for Building Circuits - Workbench Wednesdays 31
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Matt
  • Date Created: 18 Nov 2020 8:30 PM Date Created
  • Last Updated Last Updated: 25 Nov 2020 8:24 AM
  • Views 5783 views
  • Likes 10 likes
  • Comments 15 comments
Related
Recommended

Essential Consumables for Building Circuits - Workbench Wednesdays 31

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Obviously you need solder to build most circuits. However, before and after soldering a circuit, there is a bunch of other stuff. In this Workbench Wednesdays episode, James looks at the solder, flux, wick, and cleaning supplies needed when working with electronics. Make sure your lab is stocked with these must-have consumables.

 

Supplemental Content:

  • Workbench Wednesday 28: What Passive Components Do You Need?
  • Workbench Wednesday 29: What Active Components Do You Need?
  • Workbench Wednesday 07: Soldering Maintenance Myths

Bill of Material:

Product Name Manufacturer Quantity Buy Now Buy KitBuy Kit
Solder Flux Pen, Rosin, Soldering, Pen Applicator, 9 g CHEMTRONICS 1 Buy Now Buy NowBuy Now
Solder Paste for SMT, SynTECH, 183 °C, 35 g CHIP QUIK 1 Buy Now Buy NowBuy Now
Solder Flux (For SMT), No Clean, Soldering, Syringe, 10 g CHIP QUIK 1 Buy Now Buy NowBuy Now
Solder Flux Paste, No Clean, Soldering, Jar, 2 oz CAIG LABORATORIES 1 Buy Now Buy NowBuy Now
Solder Flux Cleaner ACL STATICIDE 1 Buy Now Buy NowBuy Now
Tape, High Temperate, Silicone Adhesive, PCB Protection, Amber, 2.8 mil (0.07 mm), 108.3 ft, 33 m MULTICOMP 1 Buy Now Buy NowBuy Now
Swab, Cotton Tip, Wood Handle, 1.5 mm Tip, 140 mm Handle, 1000 Pack MULTICOMP 1 Buy Now Buy NowBuy Now
Cleaner, Isopropyl Alcohol Surface, Spray Bottle, 475ml/407g MULTICOMP PRO 1 Buy Now Buy NowBuy Now
SCHMARTBOARD IC Adapter, SC70/SOIC/SOT to DIP, 2.54mm Pitch Spacing, 17.78mm Row Pitch SCHMARTBOARD 1 Buy Now Buy NowBuy Now
SCHMARTBOARD IC Adapter, 8/18/28-SOIC to 8/18/28-DIP, 2.54mm Pitch Spacing, 17.78mm Row Pitch SCHMARTBOARD 1 Buy Now Buy NowBuy Now

 

Workbench Wednesday
element14 presents  |  About James |  Workbench Wednesdays

  • flux remover
  • solder
  • e14presents_baldengineer
  • electronics flux
  • solder flux
  • solder paste
  • workbench wednesdays
  • isopropyl alcohol to clean pcbs
  • solder wick
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +4
    Great episode. I had just been thinking about how you could use surface mount components with a breadboard and you answered my question perfectly. Well done. DAB
  • dougw
    dougw over 5 years ago +3
    I think of heat shrink tubing as an essential consumable. Other stuff I might include are hot glue, silicone, thermal paste, and jumper wire.
  • baldengineer
    baldengineer over 5 years ago in reply to dougw +3
    Bummer, heat shrink would have been a really good one to include. I'll just use the same excuse I do when I solder wires: I forgot to add it until after I was already done.
  • hifromkatie
    hifromkatie over 5 years ago

    I think flux paste is generally for plumbers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago in reply to mentor46

    Hmm. Now I wonder what "shelf life" means in these datasheets. Is that how long it can sit on a distributor's shelf before being opened? Or is it how long it is good for after it has been opened? Or is it only good for 5 years after being manufactured?

     

    Of the three datasheets, none seem to differentiate the shelf life between storage and operation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mentor46
    mentor46 over 5 years ago in reply to baldengineer

    According to their data sheet, the Chemtronics flux pens (CW8100, CW8200) have a shelf life of 5 years?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 5 years ago in reply to therabi

    No, I believe you have these swapped over.

     

    Isopropyl Alcohol (IPA) dissolves oils.

    Denatured alcohol contains additives.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago in reply to therabi

    Sorry, but that is something I have never heard and cannot seem to find a reference. IPA is used throughout the electronics industry.  It is specifically used because it removes the ionic salts left behind by flux residue.

     

    You might notice, I never used the phrase "rubbing alcohol" which may contain additives that make it unsuitable for cleaning electronics.

     

    I do not know of any electronics manufacturer that cleans their boards with denatured alcohol.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • therabi
    therabi over 5 years ago

    Liked the video.  One FYI, Isopropyl Alcohol has oil in it to prevent freezing/ burning your skin.  Denatured alcohol does not have the oil and will not leave a film.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago

    From YouTube,

    Do the flux pens/syringes/pastes need to be refrigerated to extend their shelf life? In the video that was mentioned as required for the flux containing solder paste. I'm only a light hobbyist so I may go many months before soldering or desoldering something, so I've avoided buying any flux thinking it'd expire before I use much of it.

    I mostly use the Kester flu pen and the Chip Quik flux. According to Kester's datasheet, it has a shelf-life of a year at room temperature. While my preferred flux, the Chip Quik SMD291 datasheet says it has a >24 month shelf-life regardless if cooled. And I use my flux up faster than one year.

     

    image

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago

    From YouTube,

    What about washing pcb’s with water? I’ve seen this from a few folks and even some that wash larger boards in a dishwasher. I’ve never done this myself as it just seems wrong, but the results look good on camera and the boards always seem to work. Is there a technical reason that would make this a bad practice?

    There are two reasons I wouldn't recommend using a dishwasher.

     

    1. The flux residue, and other chemicals, may get trapped in the recirculating pump, which would then end up on your dishes. Not all flux is water-soluble.

    2. Water contains minerals that can containment the board.

     

    When washing with water, it is better to use distilled water and ideal to use deionized.

     

    Others may have different opinions, but I won't be putting any boards in a dish washer any time soon.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago in reply to koudelad

    I got thinking, it might be useful with a brush. Maybe a lower-cost alternative to a flux pen.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 5 years ago

    I am also curious about the usage of the flux in a can - it just can't be used effectively IMHO.

     

    Senior engineers might remember transformer soldering iron and they were also used with a solid image flux in a can. People used it in a way that they heated the soldering iron using a button, put it into the can, then released the button, let it cool and then soldered the joint. The trouble is, once the flux is heated for a few seconds, it doesn't work any more, so this worked really random.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>