WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Polls Are the fumes from (soldering) flux harmful?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 27 Mar 2019 11:28 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 6719 views
  • Likes 0 likes
  • Comments 12 comments
Related
Recommended

Are the fumes from (soldering) flux harmful?

To go along with the question on solder types, what about the fumes created from the flux? Most of the smoke you see while soldering is the flux burning away. Is that smoke or the fumes included in it harmful? Let me know what you think below.

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +9
    My fume extractor road test explains a bit about the hazards of solder fumes: https://www.element14.com/community/roadTestReviews/2606/l/fume-extraction-unit-for-soldering-applications-review#commen… I…
  • Gough Lui
    Gough Lui over 7 years ago in reply to dougw +8
    I too sometimes get that ... but not all the time. At one stage I thought I was like a cat-lover with a cat allergy ... telling me to go do something else. Now, I find it changes depending on a number…
  • Gough Lui
    Gough Lui over 7 years ago +6
    Well, if you look at the MSDS of the nearly ubiquitous Multicore 309 solder which element14 also sells, the sheet says the following: The flux fumes given off during reflow will irritate the eyes, nose…
Parents
  • dougw
    dougw over 7 years ago

    My fume extractor road test explains a bit about the hazards of solder fumes:

    https://www.element14.com/community/roadTestReviews/2606/l/fume-extraction-unit-for-soldering-applications-review#commen…

     

    I know I get allergy symptoms from exposure to the smoke fumes produced by heating the rosin in solder - sneezing fits, runny nose and eye irritation.

    My body is trying to tell me something....

    • Cancel
    • Vote Up +9 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to dougw

    I too sometimes get that ... but not all the time. At one stage I thought I was like a cat-lover with a cat allergy ... telling me to go do something else.

     

    Now, I find it changes depending on a number of factors including the solder brand/type of flux - I find rosin stuff smells rather nice but is a bit smokey, but the crystal-flux types tend not to smoke as much. The other factor was actually turning down my iron temperature - initially I had it set high enough that flux splatter could happen occasionally, but since turning it down and sticking to 60/40, I've had no irritation even without a fume extractor. The higher temperature lead-free stuff I have tends to be irritating even though it doesn't seem to visibly smoke ... it made me wonder why lead-free was considered safer although I can't vouch for the accuracy of this source as they are a vendor of soldering-related equipment.

     

    EDIT: We probably should have a poll about "What soldering iron tip temperature are you using?" - I find after using a regulated soldering-station type iron, I set my temperatures lower and that improves tip life, iron handle temperature comfort and reduces smoke ...

     

    - Gough

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 7 years ago in reply to dougw

    I too sometimes get that ... but not all the time. At one stage I thought I was like a cat-lover with a cat allergy ... telling me to go do something else.

     

    Now, I find it changes depending on a number of factors including the solder brand/type of flux - I find rosin stuff smells rather nice but is a bit smokey, but the crystal-flux types tend not to smoke as much. The other factor was actually turning down my iron temperature - initially I had it set high enough that flux splatter could happen occasionally, but since turning it down and sticking to 60/40, I've had no irritation even without a fume extractor. The higher temperature lead-free stuff I have tends to be irritating even though it doesn't seem to visibly smoke ... it made me wonder why lead-free was considered safer although I can't vouch for the accuracy of this source as they are a vendor of soldering-related equipment.

     

    EDIT: We probably should have a poll about "What soldering iron tip temperature are you using?" - I find after using a regulated soldering-station type iron, I set my temperatures lower and that improves tip life, iron handle temperature comfort and reduces smoke ...

     

    - Gough

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 7 years ago in reply to Gough Lui

    Different brands and formulations of the rosin definitely have different toxicity. I have some really old solder that is way worse than the more modern stuff.

    I can tell by the smell - one good whiff of the bad stuff and I know I'm going to suffer.

    • Cancel
    • Vote Up +5 Vote Down