WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Polls Are the fumes from (soldering) flux harmful?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 27 Mar 2019 11:28 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 6720 views
  • Likes 0 likes
  • Comments 12 comments
Related
Recommended

Are the fumes from (soldering) flux harmful?

To go along with the question on solder types, what about the fumes created from the flux? Most of the smoke you see while soldering is the flux burning away. Is that smoke or the fumes included in it harmful? Let me know what you think below.

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +9
    My fume extractor road test explains a bit about the hazards of solder fumes: https://www.element14.com/community/roadTestReviews/2606/l/fume-extraction-unit-for-soldering-applications-review#commen… I…
  • Gough Lui
    Gough Lui over 7 years ago in reply to dougw +8
    I too sometimes get that ... but not all the time. At one stage I thought I was like a cat-lover with a cat allergy ... telling me to go do something else. Now, I find it changes depending on a number…
  • Gough Lui
    Gough Lui over 7 years ago +6
    Well, if you look at the MSDS of the nearly ubiquitous Multicore 309 solder which element14 also sells, the sheet says the following: The flux fumes given off during reflow will irritate the eyes, nose…
  • DAB
    DAB over 6 years ago

    I have inhaled a lot of solder smoke in my day and have not had any ill effects, but that does not mean it is safe.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to jomoenginer

    jomoenginer  wrote:

     

    ....   Anyone with an old bench in a lab will more than likely still have the cigarette burns still on it.

    Those might be solder iron burns. They were there in my school’s lab where smoking has never been alowed.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago

    Lead free or Leaded:

    Short answer: Yes!

    Long answer: Yessssssssssssssssssss!!!!!

     

    However, there were the good old days when folks would smoke at the bench while soldering. It was like the double barrel approach.   Anyone with an old bench in a lab will more than likely still have the cigarette burns still on it.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago

    Why is it that without a fume extraction system the solder fumes always drift towards my head, move my head and they still drift towards it?

     

    Most dusts (natural and manmade) and chemical vapours are IMO harmful: at the lower exposure limits you just don't notice any immediate side-effects but over years/decades some harm is bound to occur. So whatever you can afford, be it a simple 4" extractor to outside, a fan blowing gently away from you, a fume mask or full spec solder fume extractor unit...it will be a worthy investment.

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • msebok
    msebok over 7 years ago

    Like everything fun it is hazardous to our health. Unfortunately I am quite often in a position where an extractor isn't available. I try to limit exposure with open areas. Unfortunately if your standing on your head in the cab of a tractor repairing harnesses that open space is quite limited....

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 7 years ago

    As stated in the previous comments, the fumes are toxic.

    I always try to have the window opened during soldering. And even the cheapest fume extractor like this https://uk.farnell.com/duratool/d00679/fume-extractor-1m3-min-23w-230v/dp/1498369  (or a single fan) massively improves visibility of the solder joint and extracts the smoke so I can breathe freely.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago in reply to Gough Lui

    Different brands and formulations of the rosin definitely have different toxicity. I have some really old solder that is way worse than the more modern stuff.

    I can tell by the smell - one good whiff of the bad stuff and I know I'm going to suffer.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to dougw

    I too sometimes get that ... but not all the time. At one stage I thought I was like a cat-lover with a cat allergy ... telling me to go do something else.

     

    Now, I find it changes depending on a number of factors including the solder brand/type of flux - I find rosin stuff smells rather nice but is a bit smokey, but the crystal-flux types tend not to smoke as much. The other factor was actually turning down my iron temperature - initially I had it set high enough that flux splatter could happen occasionally, but since turning it down and sticking to 60/40, I've had no irritation even without a fume extractor. The higher temperature lead-free stuff I have tends to be irritating even though it doesn't seem to visibly smoke ... it made me wonder why lead-free was considered safer although I can't vouch for the accuracy of this source as they are a vendor of soldering-related equipment.

     

    EDIT: We probably should have a poll about "What soldering iron tip temperature are you using?" - I find after using a regulated soldering-station type iron, I set my temperatures lower and that improves tip life, iron handle temperature comfort and reduces smoke ...

     

    - Gough

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago

    My fume extractor road test explains a bit about the hazards of solder fumes:

    https://www.element14.com/community/roadTestReviews/2606/l/fume-extraction-unit-for-soldering-applications-review#commen…

     

    I know I get allergy symptoms from exposure to the smoke fumes produced by heating the rosin in solder - sneezing fits, runny nose and eye irritation.

    My body is trying to tell me something....

    • Cancel
    • Vote Up +9 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 7 years ago in reply to Gough Lui
    But yeah. Don't forget to breathe in again once the flux has dissipated .... or the consequences might be more catastrophic.

    Always read the full directions before starting a task... image

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
>