WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Quiz Downsizing MLCCs Quiz
  • Episodes
  • Blog
  • Forum
  • Quiz
  • Files
  • Members
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: vijeth_ds
  • Date Created: 3 Nov 2020 1:30 PM Date Created
  • Last Updated Last Updated: 9 Nov 2021 8:21 PM
  • Views 5293 views
  • Likes 19 likes
  • Comments 29 comments
Related
Recommended

Downsizing MLCCs Quiz

profile image

Downsizing MLCCs Quiz

Quiz | Passive Components | MLCCs Downsizing Q&A with Murata | WorkBench Wednesdays image

 

badge name

When downsizing multilayer ceramic capacitors (MLCCs) from larger case sizes down to 0201, there are several considerations. The first is supply chain availability. As customer designs get smaller, so do the requirements for the size of components like capacitors. Therefore, manufacturers like Murata are ramping up their production lines to accommodate smaller case sizes. Second are the design or technical considerations. For background on this topic, watch the following interview between Yang Jiang, Murata Product Manager, and James Lewis, element14 Presents host, as they discuss these considerations. Then watch the Workbench Wednesdays Episode, where James shows how the design considerations affect a 555-timer circuit.

To earn the Downsizing MLCCs Badge, score 100% on the quiz, rate this document, and leave your feedback on the quiz as a comment.

Watch Interview with Yang Jiang - Murata MLCC Product Engineer

WorkBench Wednesdays 30: Ceramic Capacitor Voltage Effect

 

  • e14quiz
  • mlcc
  • workbench_wednesdays
  • multilayer_ceramic_capacitors
  • e14presents_baldengineer
  • yang_jiang
  • quiz
  • murata
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 5 years ago +5
    An interesting interview, Workbench Wednesday episode and quiz.
  • Fred27
    Fred27 over 6 years ago +4
    I like some of the options on the recent quizzes.
  • wolfgangfriedrich
    wolfgangfriedrich over 6 years ago +3
    Some serious content presented on a lighter note. Thanks for putting a smile or two on my face today.
Parents
  • ralphjy
    ralphjy over 6 years ago

    One thing I learned when ESD testing a circuit that had MLCCs providing AC coupling to external (exposed) pins is that manufacturers in general do not specify ESD ratings on capacitors.  We encountered issues where there was large variability in ESD tolerance between manufacturing lots.  MLCCs are more susceptible to ESD damage because of the extremely thin dielectric layers.  We discovered in FA that the cause of the variability was the consistency of the ceramic slurry used in the dielectric.  Larger particulate size created larger gaps and failed at lower voltages.  We ended up sample testing every lot that we used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 6 years ago

    One thing I learned when ESD testing a circuit that had MLCCs providing AC coupling to external (exposed) pins is that manufacturers in general do not specify ESD ratings on capacitors.  We encountered issues where there was large variability in ESD tolerance between manufacturing lots.  MLCCs are more susceptible to ESD damage because of the extremely thin dielectric layers.  We discovered in FA that the cause of the variability was the consistency of the ceramic slurry used in the dielectric.  Larger particulate size created larger gaps and failed at lower voltages.  We ended up sample testing every lot that we used.