Haunted Rover: An ESP32-Powered Halloween IoT Car

Table of contents

Haunted Rover: An ESP32-Powered Halloween IoT Car

Abstract

Meet Haunted Rover, a Halloween-themed IoT car powered by ESP32! Featuring four-wheel drive, wireless control through Blynk, and a spooky custom-built design, this project combines embedded systems, robotics, and creativity.

Haunted Rover: An ESP32-Powered Halloween IoT Car

1. Introduction

Haunted Rover is a DIY four-wheel robotic car that combines IoT, embedded systems, and creative Halloween-themed design.

I started with a basic four-wheel robotic car and decided to transform it into a Halloween pumpkin-themed rover using thermocol (foam sheets).

The car uses an ESP32 microcontroller and the Blynk IoT platform for wireless control. Its pumpkin design features an orange body, a green stem and leaves, and a hand-crafted Jack-o'-Lantern face.

2. Components and Tools

Electronic Components

  • ESP32 development board

  • TB6612FNG dual motor driver

  • Four DC geared motors and wheels

  • 18650 rechargeable batteries and battery holder

  • Tactile self-locking switch

  • Buzzer

  • Jumper wires

Decoration Materials

  • Thermocol sheets

  • Orange and green paint

  • Black sketch pen

  • Fevicol and hot glue gun

  • Cutter and paintbrush

Software

  • PlatformIO

  • Blynk IoT

3. Hardware Design and Construction

The project uses a four-wheel robotic car chassis with the ESP32, motor driver, battery holder, and other electronic components mounted on it.

Before adding the pumpkin decoration, I assembled the basic robotic car and arranged its electronics and wiring. The initial assembly photographs show the original chassis, electronic components, battery holder, and wiring setup.

For the Halloween design, I used thermocol sheets to create a pumpkin-shaped front body.

The construction involved:

  1. Measuring the front section of the existing chassis.

  2. Cutting and assembling thermocol pieces into a pumpkin shape.

  3. Painting the body orange.

  4. Making a green stem and leaves using thermocol.

  5. Drawing the eyes, nose, and mouth using a black sketch pen.

  6. Attaching the finished decoration to the car.

The design keeps the four wheels functional and the rear electronics accessible.

imageimageimageimageimage

4. Electronics and IoT Functionality

The ESP32 acts as the main controller, while the TB6612FNG motor driver controls the four DC motors.

I used the Blynk IoT platform to create a mobile interface for wireless control over Wi-Fi.

The implemented controls include:

  • Forward and backward movement

  • Left and right turning

  • Motor speed control

  • Buzzer Control

The ESP32 receives commands from Blynk and sends the appropriate signals to the motor driver to control the car.

image

5. Challenges and Learning

During development, I faced a few practical challenges:

  • Managing electronics and wiring within the limited chassis space.

  • Keeping jumper wires away from the moving wheels.

  • Designing a pumpkin-shaped body that fits the existing chassis.

  • Keeping the electronics accessible after decoration.

  • Troubleshooting an ESP32 uploading issue.

After completing the project, I encountered a problem uploading updated code to the ESP32. However, the previously uploaded program continued to work, including movement and speed control. I have not yet confirmed the cause of the upload issue.

This project helped me gain practical experience in electronics assembly, motor control, ESP32 programming, wireless communication, and physical prototyping.

6. Future Improvements

Some improvements I would like to explore:

  • Add LED lighting effects to the pumpkin.

  • Introduce obstacle detection using an ultrasonic sensor.

  • Add Halloween sound effects using the buzzer.

  • Improve the pumpkin body's finishing.

  • Explore autonomous driving capabilities.

7. Conclusion

Haunted Rover is my attempt to combine IoT, robotics, and creative DIY design in one project.

Transforming a basic four-wheel robotic car into a Halloween-themed pumpkin rover was a valuable hands-on learning experience. I learned about ESP32 programming, motor control, wireless communication, hardware assembly, and creative prototyping.

This project has encouraged me to explore more ideas and continue building practical electronics and IoT projects.

References

References

Category : project