Halloween
  • Challenges & Projects
  • More
Halloween
Forum Halloween projects anyone?
  • News
  • Forum
  • Projects
  • Past Projects
  • More
  • Cancel
  • New
Join Halloween to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 57 subscribers
  • Views 4015 views
  • Users 0 members are here
Related

Halloween projects anyone?

battlecoder
battlecoder over 2 years ago

So Halloween is around the corner and I was wondering if anyone here had any plans to build or "hack" Halloween decorations for the Spooky season.

Me, personally, I want to do something with a mist maker and a cauldron ... or something. I think that would be fun.

A couple of Halloweens ago I hacked this plastic skull to make it come "alive". I used a regular Arduino Uno to read WAV files from an SD card. WAV files are super easy to decode and play sound samples from, and as long as you play them back at the correct speed, which in this case was accomplished with interrupts. It was a super quick and dirty approach, but I didn't have any sound-playing module. I did have to build a small audio filter and connect it to a tiny "amp" board to drive the speaker, though.

The skull also was supposed to move the jaw while "laughing" but the tiny servo I used died once it was very securely glued in place, and I didn't have the time nor the patience to take it all apart to replace it.

Maybe I'll try to repair this skull for this Halloween too.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel

Top Replies

  • JackUla 🎃
    JackUla 🎃 over 2 years ago +5
    Hey everyone, I thought this might be a good time to say a quick hello as Element14's seasonal temp worker! It's great to see everyone getting in the spirit of things. jobatcliffe (joratcliffe) hasn't…
  • JackUla 🎃
    JackUla 🎃 over 2 years ago in reply to JackUla 🎃 +5
    Jinkies! This year's Halloween competition is now live. Check it out here now (if you dare...) - Halloween14 Competition 2024! - element14 Community
  • genebren
    genebren over 2 years ago +3
    For me, Halloween is a fulltime event. One of my clients 3D prints skulls (and now arm sets) as his side hustle. I provide DMX adapters (transmitters and decoders) that he builds into his products. For…
Parents
  • electronicbiker
    electronicbiker over 2 years ago

    How about a ghost? The white sheet supported on something like a long broom handle, etc., then on the inside you fit a circular ring of wood or metal or even a slightly out-of-fashion hula-hoop, mounted on the vertical broom handle so it all looks like a witches' hat roundabout as seen in play-parks when you take the grandchildren. On the ring you install 5 or 6 small-ish fans which you switch on at random intervals, run for a random time at a random speed, and switch off again. This would make the white sheet move randomly, causing random amounts of fear and distress to any passers-by, tee hee. The fans would be controlled by any random SBC with suitable I/O, the Raspberry Pi and Arduino spring to mind. If the head were made from something like a punctured (and therefore scrap) plastic football with a hole in it for the top of the broom handle, you could cut holes for eyes, and a mouth with suitably jagged teeth, with a randomly flashing bulb inside it. I did think of using an empty pumpkin shell but that would probably be a bit messy and prone to inducing random short circuits by dripping.

    All those fans and lights could all turn on at once, such is the nature of randomness. So the ghost would probably have to be mains-powered and thus for indoor use only. Given enough time you could make four ghosts, dye the sheets in Pac-Man colours, and add randomly-generated "Wakka-Wakka" sound effects before distributing them around the house. I'm sure something could be done with movement detectors too. Laugh a minute or what?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • electronicbiker
    electronicbiker over 2 years ago

    How about a ghost? The white sheet supported on something like a long broom handle, etc., then on the inside you fit a circular ring of wood or metal or even a slightly out-of-fashion hula-hoop, mounted on the vertical broom handle so it all looks like a witches' hat roundabout as seen in play-parks when you take the grandchildren. On the ring you install 5 or 6 small-ish fans which you switch on at random intervals, run for a random time at a random speed, and switch off again. This would make the white sheet move randomly, causing random amounts of fear and distress to any passers-by, tee hee. The fans would be controlled by any random SBC with suitable I/O, the Raspberry Pi and Arduino spring to mind. If the head were made from something like a punctured (and therefore scrap) plastic football with a hole in it for the top of the broom handle, you could cut holes for eyes, and a mouth with suitably jagged teeth, with a randomly flashing bulb inside it. I did think of using an empty pumpkin shell but that would probably be a bit messy and prone to inducing random short circuits by dripping.

    All those fans and lights could all turn on at once, such is the nature of randomness. So the ghost would probably have to be mains-powered and thus for indoor use only. Given enough time you could make four ghosts, dye the sheets in Pac-Man colours, and add randomly-generated "Wakka-Wakka" sound effects before distributing them around the house. I'm sure something could be done with movement detectors too. Laugh a minute or what?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • battlecoder
    battlecoder over 2 years ago in reply to electronicbiker

    That's actually very clever. You would definitely need some sound to disguise the fan sounds though, so I love the idea of making it Pac-man themed with the colors and sound

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to battlecoder

    Another variation might be to place the ghosts on Mecanum wheel bases so as they can freely roam the venue they are in. You can then program them to move in certain ways and to detect people.

    Potential for having a Pac-Man bot that follows a line of cheese balls / popcorn...