555 Timer Madness
  • Challenges & Projects
  • Project14
  • 555 Timer Madness
  • More
  • Cancel
555 Timer Madness
Forum Stayin Alive with the 555
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timer Madness to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 36 subscribers
  • Views 5312 views
  • Users 0 members are here
Related

Stayin Alive with the 555

scottiebabe
scottiebabe over 4 years ago

Many individuals have created a version of this circuit before. So, I take no credit.

Most USB power banks have an auto shutoff feature that is triggered when the output current drops below a threshold value. I am guessing whatever value that is, will vary greatly from unit to unit so you may need to adjust the load resistors.

image

This circuit kept my dollar store power bank from going into auto shutdown.

The oscillation frequency was approximately 1/7 Hz.

So every 7 seconds a ~100mA load is applied for ~100 ms.

image

The advantage of a pulse load circuit like this is that the average load current can be kept low, instead of say a static 100 mA load on your power bank.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 4 years ago +5
    Its the circuit has kept a small amber LED running at 2 mA for some time now!
  • javagoza
    javagoza over 4 years ago in reply to scottiebabe +4
    Two more days adding hardware and you already have a monster for the Halloween competition
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to javagoza +4
    The LED is pumpkin-coloured
Parents
  • scottiebabe
    0 scottiebabe over 4 years ago

    Here is the load current of the 555 load pulser:

    image

    I used 2 10uF MLCC capacitors as the timing capacitor, which have a poor tolerance and strong voltage coefficient. So, the actual timing of the circuit is pretty loosely specified. But so are the specs needed to keep the power bank awake...

    The Vol of the bipolar 555 is approximately 2V:

    image

    So If I really wanted a 100 mA load pulse I should use a 30 Ohm load resistor. Or perhaps 50 ohm resistor in parallel with a 100 ohm resistor would be close enough...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to scottiebabe

    You can use the integrate math function of your scope to calculate the total current consumed by the pulses over a time period.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scottiebabe
    0 scottiebabe over 4 years ago in reply to Jan Cumps

    Yes! This is great advice. Perhaps I will add another plot. Although the quiescent current of the bipolar 555 is nothing to get excited about. If only I had some CMOS 555s.... 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • scottiebabe
    0 scottiebabe over 4 years ago in reply to Jan Cumps

    Yes! This is great advice. Perhaps I will add another plot. Although the quiescent current of the bipolar 555 is nothing to get excited about. If only I had some CMOS 555s.... 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to scottiebabe

    For the Keithley DMM6500, I've written a custom App (what a time to be alive. Lab instruments support Apps) that collects the AmpHours used by an application over time. If the supply voltage is a given constant, it can also calculate the WattHours.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scottiebabe
    0 scottiebabe over 4 years ago in reply to Jan Cumps

    That's very cool! That keithley has much better precision/accuracy and dynamic range than a DS1054!

    To make measurements like that I have to measure the idle/sleep current separately and then stitch everything together in Matlab...