Acoustics
  • Challenges & Projects
  • Project14
  • Acoustics
  • More
  • Cancel
Acoustics
Blog SoundFi - Transmitting Data Using Sound (Ultrasonic Sound)
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Acoustics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: vimarsh_
  • Date Created: 9 Mar 2020 11:45 AM Date Created
  • Views 7604 views
  • Likes 11 likes
  • Comments 2 comments
  • ultrasonic sensor
  • ultrasound
  • sensors
  • nanorama
  • nanoramach
  • data collection
  • sound
  • acousticsch
  • iot
  • arduino
Related
Recommended

SoundFi - Transmitting Data Using Sound (Ultrasonic Sound)

vimarsh_
vimarsh_
9 Mar 2020
image

 

I first saw this discussion and it turned out sound was a good choice to transmit data one way>How to transmit data underwater over 40m  So, I wanted to make a little project that demonstrates that possibility.

 

  • The Idea
  • Procedure
    • The Scrapped Method
    • New idea
    • Part Required
    • Assembling
      • Schematic for receiver. Credit : the hackaday post
      • Schematic for Transmitter is pretty simple:
  • Working
  • Code
  • Setting up Blynk Application - Cloud connectivity
  • Results
    • Speed of Transmission
      • Speed = 8.077 bytes / second
    • Read This
      • Steps
  • Conclusion

 

The Idea

The idea was simple, to transmit data using sound waves. But, not only simple text I wanted to create a device that can demonstrate how we can use sound to take readings in water bodies (oceans) and send it to surface stations.

What I wanted to do was simple. Collect data from BME 280 sensor(measures temperature, humidity and air pressure), send it via sound to a receiver, The receiver takes the data, splits it and sends it to Cloud. I am using Blynk service. It is a very easy to use service to send data and has a simple to use app.

 

Procedure

 

The Scrapped Method

 

 

I originally thought of using ultrasonic sensors I had laying around. I thought of sending pulses long and short depending on 0 and 1 on the string.

On the receiver end I planned to measure the pulse and determine whether it was a 0 or a 1.

 

So, I created some test code to send 0 and 1 as pulses of sound and other for receiver that would measure the duration of the pulse.

 

For the hardware I wired an Arduino Leonardo to transmitting side and an Arduino Uno to receiver ultrasonic sensor. I leaned that the normal ultrasonic sensors don't work at 3.3v so 5v Arduino.s were my only option.

 

Test code for transmitting   https://gist.github.com/vimarsh244/915b261e7961f9b6f5deed4f124ea8f2

Test code for receiving   https://gist.github.com/vimarsh244/ff56771134458e451baf368b33c10485

 

I soon found out that it didn't work. The reason being that ultrasonic sensors work in a very different way. Basically, the echo pin remains high for time from when the pulse was started (when trig pin was hit) to when it received back the pulse. The pulseIn() function in arduino basically thus measures time for which the pin was kept high. Since we cannot remotely trigger a pin without sending, the method cannot work.

 

 

New idea

image

Then I thought to just use transducers of the ultrasonic sensors. I soldered one ultrasonic sensors transmitter pins and other ultrasonic sensor's receiver to jumper cables. The reason was that after the project I could de solder the wires and use it for something else.

 

 

 

 

 

Then I planned to use that as baseline to work on. But soon found out this great way how to do it on Hackaday. https://hackaday.com/2018/06/01/dead-simple-ultrasonic-data-communication/ . This tells us how important research is!

 

Basically what is happening is data is being transmitted by pulses of 2ms and 4ms for 0 and 1 respectively. On receiver side it is being measured as 0 or 1 and being reverses back to ASCII to character and printing it.

 

Part Required

 

  • Arduino Uno // or any other
  • Wemos D1 mini // or any other Wi-Fi enabled uC
  • 2 ultrasonic sensors // or just transducers
  • LM386 //to amplify sound waves
  • LM 393 // as a comparator
  • 10K potentiometer //for fine-tuning
  • 100nF capacitor //to remove noise
  • 10K resistor
  • BME 280 // temperature, humidity, air pressure sensor

 

{gallery} Components

image

Ultrasonic Sensors , moreover ultrasonic transducers

 

image

LM393+LM386

image

Wemos D1 MIni - uC with WiFi

image

Arduino Uno

image

BME280 Sensor

 

 

 

Assembling

 

The schematic for the same is on the Hackaday post. I am just using wemos instead of an Arduino so that the data received can also be sent to the cloud. The only change is supply to comparator which will be 3.3v instead of 5v.

 

Schematic for receiver. Credit : the hackaday post

image

I did not connect the LED as found no practical use to it.

Schematic for Transmitter is pretty simple:

  1. Connect BME 280 sensor via I2C/SPI.  I used I2C because it requires only 2 wires. Also connect VCC/Vin and GND pins of sensor to your development board.
  2. Connect the transducer's one pin to pin 3 and other to GND

 

 

The Transmitterimage

The Receiverimage

 

Working

Here is how it works:

  1. Data us read from BME280 sensor on the transmitter and a string is made in this format : <temperature>,<pressure>,<humidity>,#
  2. The string is then broken into characters and each character into 8 bits ASCII Value.
  3. If it is 1 then the ultrasound pulse of 2ms and if 0 then of 4ms is formed. The "tone()" function of Arduino creates a very high vibrating frequency .
  4. On the receiver side data is received by measuring the time duration of which the pulse is their. Then it is converted to either 1 or 0 based on the pulse duration.
  5. Then the bits are converted to ASCII to characters and finally a string is formed.
  6. This string is then used to separate the temperature, air pressure and humidity values.
  7. The data is then pushed to Blynk cloud on pins V1, V2, V3 respectively.

 

Code

 

Sender Code   https://gist.github.com/vimarsh244/dabe71cf9e18b30b88f72c52e9a638d6

 

Receiver Code   https://gist.github.com/vimarsh244/d3d09b8dcfb82ff1f4a4e30a9d3687a1

 

 

Setting up Blynk Application - Cloud connectivity

 

Blynk is the easiest way to connect your Arduino/Raspberry Pi project to the cloud.

Blynk doesn't offer a webpage from where you can control/monitor your devices. All must happen through the smartphone app.

First step is to download the Blynk app from the Play Store/ App Store.

 

Then follow these steps to complete setting it up.

 

{gallery} Setting up Blynk

image

Once you open the app, you will be greeted with this screen. Click on create a new account.

image

Enter your details and click on Sign Up

image

Here, you get to see that you will only be given 2000 energy. Energy is like a virtual coin in Blynk from which you can get several widgets. Widgets are various input/output graphical elements,

image

Click on new project

image

You will see this. Enter your project name and select correct device. For us that is ESP8266, the chip on the Wemos D1 mini

image

After creating the project you will get your auth token on your email address. Auth Token is a string of character different for every device.

image

Tap anywhere on the screen and you will see this menu from left. Select Value Display/ Labeled Value

image

Add 3 of those to your project.

image

Arrange them in proper place by long pressing then moving it.

image

Click on one widget and name it temperature and select pin to Virtual and then V1

image

You can set text color,size,etc and the ending text after '/pin/'  It will be different for every widget.

image

Do the same for Air Pressure with another widget

image

And the same for humidity

image

Yo can type any symbol at the end.

image

This is how humidity settings will look like

image

And the configured screen. Then go to you Arduino IDE. and upload code.

image

First don't forget to change the Auth token and WiFi Credentials in the code.

image

Then click on play button

image

You will see your data from the sensor being transmitted via sound on your smart phone app.

 

 

Also, because you are using a cloud service. You can download the app on any other phone and also see that data!

imageimage

 

 

Results

 

You can listen to sensor sending data 3 times with one second delay in between: Listen here

Here is the data on the Blynk app:

imageimage

 

I found that the connection link was not stable for esp8266 to Blynk server perhaps because of code in-between which Blynk says no as because of delays the server session may time out.

Also, the distance between sensors and sensitivity may have to be tuned in a better way. Just if I had an oscilloscope!

 

Data being received>

image

Speed of Transmission

I edited the code of receiver to find time it takes to received the full string. I turned out to be around 2600 ms.

 

long initial_time=micros();
...
//existing code
...
long final_time = micros();
long transmit_time= (final_time-initial_time)/1000;
Serial.println(transmit_time);

 

Here is output with that:

image

 

To calculate speed I measured the Bytes being sent and divided it by time it takes.

It is 21 bytes:

image

Dividing it by 2592 milli seconds

 

Speed = 8.077 bytes / second

image

The speed seems quite less and it is compared to WiFi and other RF. But that is still reasonable if we want to send some specific readings.

 

Read This

If you want to see the data on your smartphone which my device is transmitting. Then see the steps>

I will keep it on for some days probably and hopefully it will be transmitting. I live in Gujarat, India. So those are my indoor weather conditions. Also, I have added a button to control the onboard LED on the Wemos D1

 

Steps

{gallery} My Gallery Title

image

Click the QR Button

image

Scan this QR Code

image

Enjoy!

 

Conclusion

 

This was a fun experiment for it. It was easy and a great insight on how to transmit data using sound.

Later I wish to add some sort of encryption and try for two way communication without interference.

 

Checkout my other projects!

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +2
    A good project and a good implementation. I had some good nostalgic feelings seeing serial communications being implemented in this way. Dubbie
  • vimarsh_
    vimarsh_ over 6 years ago +1
    Update: I am disassembling the project, so new updates on the Blynk App will not happen.
Parents
  • dubbie
    dubbie over 6 years ago

    A good project and a good implementation.

     

    I had some good nostalgic feelings seeing serial communications being implemented in this way.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago

    A good project and a good implementation.

     

    I had some good nostalgic feelings seeing serial communications being implemented in this way.

     

    Dubbie