Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog A Digital FM Receiver with Arduino (Including 3W+3W Class-D Stereo Amplifier)
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Hesam.M
  • Date Created: 24 Nov 2020 7:12 AM Date Created
  • Views 3629 views
  • Likes 8 likes
  • Comments 8 comments
  • arduino fm radio
  • tea5767
  • fm receiver
  • fm
  • fm receiver using arduino
  • receiver
  • tea5767 using arduino
Related
Recommended

A Digital FM Receiver with Arduino (Including 3W+3W Class-D Stereo Amplifier)

Hesam.M
Hesam.M
24 Nov 2020

FM transmitters/receivers are among the top favorite circuits of any electronic enthusiast. In this article/video, I have introduced a complete digital FM receiver design that has equipped with an LCD screen and three push-buttons. It can search for the FM signals from 76MHz to 108MHz manually and automatically (Scan mode). The signal strength is also displayed as a bar graph on the LCD screen. The output sound is amplified by a 3W+3W Class-D stereo amplifier that handles high-quality and strong enough audio power. As a controller, I have used the cheap and popular Arduino-Nano board. So let’s get started!

 

YouTube

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

A. Circuit Analysis

Figure 1 shows the schematic diagram of the device. As it is clear, the circuit consists of 3 main parts: Arduino-Nano (Controller), FM receiver module, and the audio amplifier.

image

Figure 1

Schematic diagram of the digital FM receiver

 

A-1. FM Receiver Module

The FM receiver module is based on the TEA5767 [1, 2] chip. It is a well-known module that could be controlled via the I2C bus. It covers the FM frequency range from 76MHz to 108MHz. At the output, it handles L and R stereo audio signals that should be amplified, otherwise, the sound level is weak and can not be heard even by an earphone. The frequency selection and signal-strength measurement tasks are performed by the Arduino-Nano code.

R3, C7, C8, and C9 build a first-order low pass RC filter that reduces the supply noise. R1 and R2 are mandatory pull-up resistors for the I2C bus and CON1 is a UFL connector that provides an antenna connection. Figure 2 shows the TEA5767 module.

image

Figure 2

The TEA5767 FM receiver module

 

A.2 Audio Amplifier

The audio amplifier part consists of the PAM8403 [3, 4] chip. This chip is a 3W+3W HiFi Class-D amplifier that can operate with only a single 5V supply. The maximum output power can be achieved using 4-ohm speakers. According to the datasheet: “The PAM8403 is a 3W, class-D audio amplifier. It offers low THD+N, allowing it to achieve high-quality sound reproduction. The new filterless architecture allows the device to drive the speaker directly, requiring no low-pass output filters, thus saving the system costs and PCB area”.

R7, C13, C14, and C15 build a low pass RC filter to reduce the supply noise as much as possible. R4, R5, C11, and C12 are used to transfer the output audio to the amplifier. Also, they create high-pass RC filters to remove any low-frequency noises. Figure 3 shows the reference circuit of the PAM8403 chip. P2 and P3 are right-angle 2-pin XH connectors that are used to connect the speakers to the board.

image

Figure 3

Datasheet reference circuit of the PAM8403

 

A.3 Controller

The controller of the circuit consists of an Arduino-Nano board (AR1). Figure 4 shows the Arduino-Nano board. The board drives an 8*2 LCD (LCD1) and also reads the status of the SW1, SW2, and SW3 push buttons. It also sends/receives the TEA5767 data through the I2C bus. R6 sets the contrast level of the LCD and C4, C5, and C6 are used to reduce the mechanical push-button noises (debouncing).

image

Figure 4

The Arduino-Nano board

 

A.4 Power Supply

The TS2937 [5, 6] is the main component of the power supply that provides a stable +5V supply for the circuit. C1, C2, and C3 are used to reduce the noise, and POT1 is a 50K 2-way (dual) potentiometer with a switch. The POT1 both turns ON/OFF the device and increases or decreases the sound level. Picture 5 shows a picture of the POT1.

image

Figure 5

2-Way (Dual) potentiometer with Switch

 

B. PCB Layout

Figure 6 shows the PCB layout of the digital FM receiver. It is a 2 layers PCB board, last revision. The Arduino-Nano board is mounted on the bottom side and LCD on the top side of the board, preferably on female pin headers. This is more clear in 3D views and real photos. Figure 7 shows the 3D views of the board. Figure 8 shows the high-quality fabricated PCB boards of the digital FM receiver circuit.

image

Figure 6

The PCB layout of the digital FM receiver

 

image

Figure 7

The top and bottom 3D views of the PCB board

 

image

Figure 8

High quality fabricated PCB boards

 

I used the SamacSys component libraries (for IC1 and IC2) in this PCB project as usual. It saves a lot of time and prevents design mistakes which leads to a lower product cost. All SamacSys component libraries (Schematic symbols, PCB footprints, and 3D models) are FREE and they follow strict industrial IPC footprint standards. You can download and install the libraries from the componentsearchengine.com or you can install them directly using the provided CAD plugins. I used the Altium plugin, however, almost all electronic designing CAD software are supported, such as Eagle, KiCad, OrCAD, Proteus .. etc [7]. Figure 9 shows the supported CAD software and figure 10 shows selected component libraries from the Altium plugin.

image

Figure 9

Supported CAD software by the SamacSys plugin

 

image

Figure 10

Selected PAM8403 and TS2937 libraries from the Altium plugin

 

 

C. Assembly and Test

The smallest component package is 0805. You should not have any problem with soldering the board, however, you can order the professionally assembled board as well. Figure 11 shows the assembled PCB board from the top and figure 12 shows the assembled PCB board from the bottom. The board has been hand-soldered by me. You would also need four 5mm FF spacers to fix the LCD on the PCB board.

image

Figure 11

Assembled PCB board (top view)

 

image

Figure 12

Assembled PCB board (bottom view)

 

 

You should use a UFL to SMA-F connector to connect your antenna to the board. Figure 13 shows this type of connector.

image

Figure 13

UFL to SMA-F connector

 

 

C.1 Arduino Code

The Arduino code is available in the below code block. Just connect your Arduino-Nano to the computer and compile/upload the code.

 

#include <TEA5767.h>
#include <Wire.h>
#include <JC_Button.h>
#include <LiquidCrystal.h>

float frequency = 76.0;
unsigned char buf[5];
unsigned int counter = 0, btn_counter = 0;
unsigned char level = 0;

TEA5767 radio;
const byte RS = 7, EN = 6, D4 = 4, D5 = 5, D6 = 2, D7 = 3;
LiquidCrystal lcd(RS, EN, D4, D5, D6, D7);


byte L1[] = {
  B00000,
  B00000,
  B00000,
  B00000,
  B00000,
  B00000,
  B11111,
  B11111
};

byte L2[] = {
  B00000,
  B00000,
  B00000,
  B00000,
  B00000,
  B11111,
  B11111,
  B11111
};

byte L3[] = {
  B00000,
  B00000,
  B00000,
  B00000,
  B11111,
  B11111,
  B11111,
  B11111
};

byte L4[] = {
  B00000,
  B00000,
  B00000,
  B11111,
  B11111,
  B11111,
  B11111,
  B11111
};

byte L5[] = {
  B00000,
  B00000,
  B11111,
  B11111,
  B11111,
  B11111,
  B11111,
  B11111
};

void setup() {
  Wire.begin();

  lcd.begin(8, 2);
  lcd.createChar(0, L1);
  lcd.createChar(1, L2);
  lcd.createChar(2, L3);
  lcd.createChar(3, L4);
  lcd.createChar(4, L5);
  lcd.clear();

  radio.init();
  radio.set_frequency(frequency);
  DispSigStrenght();
  Freq_Mono_Stereo(frequency);

  pinMode(10, INPUT_PULLUP);
  pinMode(11, INPUT_PULLUP);
  pinMode(12, INPUT_PULLUP);

}

void loop() {

  if (digitalRead(11) == 0 && frequency < 108.0)
  {
    btn_counter++;
    if (btn_counter == 5000) {
      frequency += 0.1;
      radio.set_frequency(frequency);
      Freq_Mono_Stereo(frequency);
      btn_counter = 0;
    }
  }

  if (digitalRead(12) == 0 && frequency > 76.0)
  {
    btn_counter++;
    if (btn_counter == 5000) {
      frequency -= 0.1;
      radio.set_frequency(frequency);
      Freq_Mono_Stereo(frequency);
      btn_counter = 0;
    }
  }

  if (digitalRead(10) == 0)
  {
    btn_counter++;
    if (btn_counter == 5000) {
      if (frequency >= 108.0)
      {
        frequency = 76.0;
        radio.set_frequency(frequency);
      }
      radio.read_status(buf);
      radio.search_up(buf);
      radio.process_search (buf, TEA5767_SEARCH_DIR_UP);
      frequency =  floor (radio.frequency_available (buf) / 100000 + .5) / 10;
      Freq_Mono_Stereo(frequency);
      btn_counter = 0;
    }

  }

  counter ++;

  if (counter == 15000)
  {
    counter = 0;
    DispSigStrenght();
  }

}


void DispSigStrenght()
{

  lcd.setCursor(0, 1);
  radio.read_status(buf);
  level = radio.signal_level(buf);
  switch (level)
  {

    case 1 ... 3:
      lcd.print("\x08");
      lcd.setCursor(1, 1);
      lcd.print("    ");
      break;

    case 4 ... 6:
      lcd.print("\x08\x01");
      lcd.setCursor(2, 1);
      lcd.print("   ");
      break;

    case 7 ... 9:
      lcd.print("\x08\x01\x02");
      lcd.setCursor(3, 1);
      lcd.print("  ");
      break;

    case 10 ... 12:
      lcd.print("\x08\x01\x02\x03");
      lcd.setCursor(4, 1);
      lcd.print(" ");
      break;

    case 13 ... 15:
      lcd.print("\x08\x01\x02\x03\x04");
      break;
  }
}


void Freq_Mono_Stereo(float freq)
{

  lcd.clear();
  lcd.setCursor(0, 0);
  lcd.print(String(frequency, 1) + "MHz");

  radio.read_status(buf);
  if (radio.stereo(buf))
  {
    lcd.setCursor(6, 1);
    lcd.print("ST");
  }
  else
  {
    lcd.setCursor(6, 1);
    lcd.print("MN");
  }
}

 

 

C.2 Testing

The lower limit of the frequency is 76.0MHz and the upper limit is 108.0MHz. You can increase or decrease the frequency by 0.1MHz by pressing the Up and Down buttons. Similarly, if you long-press these buttons, the frequency will be increased/decreased continuously. So it is pretty easy to fix the receiver on your desired frequency (FM station). Moreover, the Scan button can automatically search for powerful-enough FM stations and fix the receiver on the frequencies. To search for the next station, you should press the Scan button again.

The strength of the FM signal is displayed on the LCD screen as a bar graph. In figure 14, the receiver has been set on a powerful FM station, at 100.0MHz frequency.

image

Figure 14

The receiver has been set on a powerful FM station at 100.0MHz frequency

 

D. Bill of Materials

Figure 15 shows the bill of materials. Build the device and have fun!

image

Figure 15

Bill of materials (BOM)

 

 

References

Article: https://bit.ly/3pQ7WoG

[1]: TEA5767 Datasheet: https://www.sparkfun.com/datasheets/Wireless/General/TEA5767.pdf

[2]: TEA5767 Schematic Symbol, PCB Footprint, and 3D Model: https://componentsearchengine.com/part-view/TEA5767HN%2FV3%2C118/Nexperia

[3]: PAM8403 Datasheet: https://www.mouser.com/datasheet/2/115/PAM8403-247318.pdf

[4]: PAM8403 Schematic Symbol, PCB Footprint, and 3D Model: https://componentsearchengine.com/part-view/PAM8403DR/LITTELFUSE

[5]: TS2937 Datasheet: https://www.mouser.com/datasheet/2/395/TS2937_D13-522475.pdf

[6]: TS2937 Schematic Symbol, PCB Footprint, and 3D Model: https://componentsearchengine.com/part-view/TS2937CW-5.0%20RP/Taiwan%20Semiconductor

[7]: CAD Plugins: https://www.samacsys.com/library-loader-help

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 5 years ago +3
    There are a couple of mistakes in your design/description: 1) The power amplifier can't drive 3W into each of two speakers with a 10 ohm resistor (R7) in the power supply feed. 2) R4, R5, C11, and C12…
  • dougw
    dougw over 5 years ago +2
    Very nice project. Thanks for posting.
  • Hesam.M
    Hesam.M over 5 years ago in reply to michaelkellett +2
    Hi, 1) Close to 3W for maximum, because the total current consumption of the unit for audible sound is less than 100mA. more than half of this is for LCD, FM Module, and Arduino. So the voltage on the…
  • Hesam.M
    Hesam.M over 5 years ago in reply to michaelkellett

    The current draw increases if the output power increases by the volume. I think it is better that those resistors be 0R for more power. stationary current reading with strong enough audible sound was around 100mA. Anyway this project is opensource, you are free to edit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    Very interesting project.

     

    Well done.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to Hesam.M

    Hesam.M  wrote:

     

    Hi,

     

    1) Close to 3W because the total current consumption of the unit is less than 100mA. more than half of this is for LCD, FM Module, and Arduino. So the voltage on the chip would not be lower than 4.6V to 4.7V.

    ..........

     

     

    I'm sorry but this is completely wrong.

    From the data sheet the efficiency is about 85%, even at 1W per channel it would need an input power of

    2.35W, needing 470mA, which would drop 4.7V across the 10R resistor - and so quite impossible.

    Actually the most you could expect it to work with a 10R series resistor is with a supply current of 200mA, giving a Vdd

    of 3V and an input power of 600mW, about 250mW per channel.

    Even if you reduce R7 to zero the maximum output of the current is only 500mA, which will limit the maximum input

    power to the amplifier chip to about 2W.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 5 years ago

    I mean to be critical. Is this material for Project14 or is this a product placement?

     

    After reviewing the material I did a google search on MyVanitar and discovered a number of kits and the same post on a PCB marketing site.

     

    I feel this is a product, disguised as a project, to slip under the filters of leveraging the site for marketing. If the site has an area for marketing then that is the location for this material.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Hesam.M
    Hesam.M over 5 years ago in reply to dougw

    Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>