Project14
  • Challenges & Projects
  • More
Project14
Make a Connection Meshtastic Solar Hat Node
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 5 Sep 2026 12:49 AM Date Created
  • Views 299 views
  • Likes 12 likes
  • Comments 8 comments
  • solar hat
  • off grid
  • XIAO ESP32S3 & Wio-SX1262 Kit
  • XIAO nRF52840 & Wio-SX1262 Kit
  • L76K GNSS
  • Wio Tracker L1 E-ink
  • meshtastic
Related
Recommended

Meshtastic Solar Hat Node

ralphjy
ralphjy
5 Sep 2026

Meshtastic Solar Hat Node

Introduction

Back in July, cstanton  posted The world's on fire - embrace solar punk in the Design Challenges Forum about the Meshtastic network and communicating "off grid".  I just did a project with a present I got for Christmas Solar Power Hat Fan and I've also been wanting to do something with a mesh network, so I thought that the Make a Connection Competition would be a good opportunity to do a Meshtastic project with a solar tracker node.

I decided that I should have at least 2 nodes, maybe 3.  I would start with a Base Station Node that I would leave in my office at home.  Then I would have a couple of remote mobile nodes that I could track.  

Base Station Node

For the Base Station I saw a nice kit from Seeed Studio - Wio Tracker L1 that includes a 2.13" E-ink display and GPS module.  I figured that the display would be nice to display messages from the remote nodes.

All the required components other than a case and the joystick and button covers in a nice box.

image

The included components:

  1. Device PCB assembly
  2. LoRa antenna
  3. GNSS antenna
  4. E-ink Display
  5. Flat cable extender for optional display positioning

image

The working assembly - the flat cable can be folded to allow positioning the display over the PCB for mounting in an enclosure.  To start this project I am using it without an enclosure.  The GNSS antenna is upside down in this picture.  

image

The board comes preprogrammed so it powers up immediately.

There are no other nodes detected (heard).  There is also no battery, so I'm not sure what the ADC is measuring - I'll need to check this later.

image

You can operate and configure this node using the GUI with the button and joystick, but because I haven't built a case yet - it is much easier using the Meshtastic mobile app.  I am using iOS since I don't have an Android device capable of running a recent OS.

Connecting to the device via Bluetooth starts configuration with LoRa settings.  I have left the node name as default (last 4 characters of MAC address) - thought it best to start somewhat anonymous.  The app indicates that there is a firmware update available - good news is that it can be done via Bluetooth.  If the device ever gets bricked, then you need to reflash it using the Meshtastic Flasher over USB.

image

image

image

The node shows in the node list:

image

At this point in the process the GNSS doesn't have a good fix, but the node has heard a second node to the west.  The blue dot is my current position (iPhone position), but the node (yellow dot) thinks it is somewhere to the west and the unknown node (brown dot) is west of it.

image

And now both nodes showing in the list.

image

Letting the setup run for a day, the node heard 52 other nodes.  Many in my immediate area, but some over 20 miles away.

image

image

Meshtastic Flasher

Two of my nodes are nRF52840 based and my extra node is ESP32S3 based.  I had an issue connecting to the ESP32S3 node, so I needed to use the Meshtastic Flasher.

Meshtastic has prebuilt firmware for most of the device configurations that you can buy.  The Meshtastic Web Flasher allows you to select the target device and firmware version to be flashed.  I stayed with the latest stable version and my 3 device types were available.  It turns out that you need to be at firmware version 2.7.x for it to work with the mobile app.

image

image

imageimageimage

image

Solar Hat Node (Xiao nRF52840 + Wio-SX1262)

I decided to use the XIAO nRF52840 & Wio-SX1262 Kit for Meshtastic for the solar hat node.  This is a piggy-back configuration of a Xiao nRF52840 on a Wio-SX1262 for Xiao.  This assembly does not include a GNSS, but my intent is to use my iPhone as the messaging interface and I will use the phone GPS for position.

image

I needed to attach the node assembly to the hat, so I printed a housing that I could clamp on to the voltage regulator/connector unit that is mounted on the underside of the back brim of the hat.

image

image

image

image

Extra Node (Xiao ESP32S3 + Wio-SX1262)

I also wanted to have a 2nd remote node - this one would have a GNSS unit.  It turns out that for Xiao the GNSS unit is not plug compatible with either the ESP32S3 or nRF52840 versions of the Xiao.  And the standard Xiao Wio-SX1262 is not compatible with the Xiao ESP32S3.  I guess with only 14 available header pins, compatibility with everything is hard to do.  The Xiao ESP32-S3 Sense has a camera header connector that can be used with a special version of the Wio-SX1262.  Even with that, there are pins that have to be removed from the standard header to accommodate the GNSS module.  I have tried out the ESP32-S3 configuration without the GNSS, but have decided to leave the GNSS for a later project.

XIAO ESP32S3 & Wio-SX1262 Kit for Meshtastic & LoRa

image

Meshtastic iOS App

image

One thing that I discovered is that the iOS version of the Meshtastic app is missing a lot of capabilities relative to being able to configure the device.  I could not even set a fixed position (lat/long) for the device.  it would be beneficial for the base node.  I have heard that the Android app is much better at configuration but can't currently try that.  There is a CLI API that should allow me to configure all aspects of the device over USB from a host PC, but that's something I'll need to learn.

Messaging

I would like my messaging to be private for this particular set of nodes, so I am changing the primary channel for these nodes.  My understanding is that if I stay with the default region frequency that the default is that my encrypted messages will still be rebroadcast unless other nodes are explicitly set to not rebroadcast encrypted messages.  So much to learn...

Here are my 3 nodes that I've marked as Favorites (yellow star).

    0db3 is the Solar Hat

    f2ca is the Base Station

    85a4 is the ESP32S3 (it's not really 1.3 miles away - that's what it defaults to if no GPS is available)

image

I set up a private channel named RLOOP on slot 66

image

image

And sent a test message.

image

image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

And the response:

image

A stroll on a cloudy day to test tracking

So, as a final test I wanted to see if the Solar Hat Node could handle route tracking.  Summer has taken a break this week and we've had rain and cloudy days - which are great for the wildfires and smoke.  One issue with my Solar Hat Node is that it has no battery, so I'm somewhat concerned that the power might drop out on a cloudy day like today - especially when I'm walking under trees.

The app has a Route Recorder that will save a route that can be displayed on the map.


image

image

image

The first route was a quick test to see if it was recording.  The second was a short walk around the neighborhood.

image

image

  • Sign in to reply
  • javagoza
    javagoza 4 days ago

    Thanks for sharing this project, ralphjy ! I wasn't familiar with Meshtastic before reading your project, so it was great to learn about this type of communication network and see a practical implementation. I always enjoy projects that introduce new technologies and ideas to the community. Thanks for taking the time to document and share your work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB 20 days ago

    Very nice post.

    It looks like you had a lot of fun putting it all together and running the tests.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy 20 days ago in reply to beacon_dave

    My stroll wasn’t a good test of the mesh repeating capabilities.  My nodes were communicating directly.  I need to drive somewhere further away or maybe wait for a dog walk when my grandson isn’t along.  Not sure when I’ll be in a rural area next.  Haven’t had much opportunity for fishing this year Worried.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave 20 days ago

    Nice overview for getting up and running with Meshtastic and nice use of the solar powered hat.

    ( If we spot you wearing a sombrero, we will know that you are scaling up Slight smile )

    Interesting that the d5a4 node is showing up as being 22 miles away but isn't showing any hops.

    image

    Is that because it just isn't being reported for that client or perhaps it is leveraging 'Zero-Cost Hops' via preferred relays ? Or perhaps on an airborne drone, so actually has line-of-sight.

    It would be interesting to know how many nodes were being relied upon in typical deployment scenarios. Do you see the number of hops back to base logged when you are out for a stroll ?

    One thing the system will likely be reliant upon in emergencies is for static relays to have back-up power in case of a local power outage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave 20 days ago in reply to embeddedguy

    I think that would depend on the placement of nodes. Potential for better line-of-sight in rural areas so longer distances between nodes. Potential for strategically placed repeater nodes e.g. on tops of hills. Potential for a lot of sensor node deployments to act as repeaters.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>