Back to Analog
  • Challenges & Projects
  • Project14
  • Back to Analog
  • More
  • Cancel
Back to Analog
Blog Hiraga PreAmp .. build 4
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Back to Analog to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 12 Dec 2018 6:54 AM Date Created
  • Views 1011 views
  • Likes 4 likes
  • Comments 0 comments
  • inrush current-limitation
  • diy audio
  • 12ax7
  • sscr
  • pre-amplifier
  • arduino
  • diy electronics
  • hiragra
Related
Recommended

Hiraga PreAmp .. build 4

phoenixcomm
phoenixcomm
12 Dec 2018

Well, life really sucks a good friend of mine is dying and I have been out of town for the last week or so. And I am going back tomorrow. The Gorilla Brake did not work for the two smaller boxes so pop-rivets will work. The power supply is a nightmare and I will get around to that later. For the time being, I plan on using the power outputs from my beloved Dynakit Stereo 70 which has power take-off sockets on the rear 360vac-0-360vac. I will most likely use both sides of the transformer so that I will have 2 bridges with the center tap being common.  The Stereo 70 only uses 6-volt tubes, so I will have to tie them together or use two 12-volt wall warts for the heaters. I lost one of my tube sockets and had to re-order it from eBay.  I completed most of the drilling and mounting please see the picture below.

Mounting the tubes was a piece of cake by using a 7/8" hole saw. .I will most likely put a 5-pin DIN female connector on one rear end for power. The other side has blue tube shields and black RCA jacks.image

I will be using a one-pair shield wire for the tube heaters. I will also have my output gain controls on the rear by the output sockets. Also on the rear, there is a 5-pin female DIN socket as well, which can be used for a USB audio stream for recording, etc.image

For the layout, I used some basic tools, a good speed square, Permanente Markers by Milwaukee, a ruler, and blue painter's tape. The two black squares are for aux power. As you can see there is an auxiliary power supply that provides soft-start power. It currently provides 12vdc which powers the main relay on the PCB and a 9vdc 3 lead regulator for the Arduino.  I will also have to add a voltage doubler to get the 24vdc for the bypass resistors for startup.image

image

In recap on the power supply when finished I will be using an SSCR turning on at the peak voltage also the bypass relay will be energized with a resistor limiting current flow to about 1 amp after about 2 or 3 seconds I can release the relay and short out the resistor.  So both right and left amps were laid out the same I took some duct tape and taped them together so I just need to layout it out and drill it once. I did not need to use painter's tape on them as one side had a thin plastic film on it.

SOFTWARE OVERVIEW:

  1. Arduino wakes up.
  2. turns-on lamp (power)
  3. Energize all three bypass relays via optocouplers.
  4. Start voltage monitor (looking for Vmax!)
  5. Enter Loop. // for( circuit = 0; circuit < 4; circuit++)
    1. when Vmax found turn-on SSCR(circuit)
    2. wait for n seconds.
    3. turn-off relay(circuit)
    4. turn-on lamp(circuit)