Back to Analog
  • Challenges & Projects
  • Project14
  • Back to Analog
  • More
  • Cancel
Back to Analog

Blog

  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Back to Analog to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Hiraga PreAmp .. build 5

    phoenixcomm
    phoenixcomm
    And the planet spins and life goes on. This has been a build from hell, nothing is normal, no chassis, or priced out of sight. My two preamp modules are 6" x 3" x 1.5" first I tried the guerrilla break which was very disappointing. I had the right Id...
    • 17 Mar 2019
  • Hiraga PreAmp .. build 5 - software for a tube amp?

    phoenixcomm
    phoenixcomm
    Well, life is still not on a good keel. I picked up at Fry's a proto shield, and some optocouplers. So the world keeps spinning and I am using a software-controlled power-supply I don't have a formal sketch but this is what it will do: Cod...
    • 20 Dec 2018
  • Pulse Hunter

    sunnyiut
    sunnyiut
    This blog post is intended for Project14 - 'Back to Analog'. ooops... I think I missed the deadline :-(   When I started this project, I posted a status update and 14rhb suggested to share it into the 'Back to Analog'. Unfortunately I forgot an...
    • 15 Dec 2018
  • Hiraga PreAmp .. build 4

    phoenixcomm
    phoenixcomm
    Well, life really sucks a good friend of mine is dying and I have been out of town for the last week or so. And I am going back tomorrow. The Gorilla Brake did not work for the two smaller boxes so pop-rivets will work. The power supply is a nightmar...
    • 12 Dec 2018
  • CVBoard: new way to play with modular synths

    costantinorizzuti
    costantinorizzuti
    CVBoard is a board designed to generate two Control Voltage (CV) signals using Arduino. This prototype is destinated to analog synths and EuroRack modules enthusiast. CVBoard  has two jack outputs from which it is possible to take the CV signal...
    • 3 Dec 2018
  • LED fade in/out effect

    kk99
    kk99
      The basic idea was to create a simple LED fade in/out effect circuit. I have used here a single dual op-amp NJM4556 which first stage is configured in comparator mode and second stage is configured as integrator. Triangular wave from integra...
    • 1 Dec 2018
  • Hiraga PreAmp .. build 3  Gorilla Brake

    phoenixcomm
    phoenixcomm
    Normally I would have just bought some aluminum boxes but the prices are ridiculous, and I did not have a finger break to make my own. Having no real metal brake, I had to improvise. and the results were better than I had hoped for. So here is what w...
    • 30 Nov 2018
  • 555 Timer Voltage Inverter

    fmilburn
    fmilburn
    I still have work to do on my Kelvin (4-wire) Milliohm Meter project, one item of which is to improve the accuracy of the meter when measuring below 3 milliohms.  I suspect the problem may be that the instrument amp is too close to the ground r...
    • 28 Nov 2018
  • Tube Amp on a PCB

    dougw
    dougw
    Long, long ago in a far away place outside of the box, I was challenged to build a tube amp to explore the sound of tubes clipping. The idea was to make a tube amp that could clip at low volume so we didn't have to wake up the neighborhood to explor...
    • 27 Nov 2018
  • Hiraga PreAmp .. build 2a

    phoenixcomm
    phoenixcomm
    Well, Christmas or Hanukkah came early this year! These parts are what I call almost unobtainium! I wish to thank Tariq and the E-14 family for this dotation. Whoopie! Now to just get this thing built and tested. Fins!   Back to the Monthly Inde...
    • 19 Nov 2018
  • Hiraga PreAmp .. build 2

    phoenixcomm
    phoenixcomm
    As you all know I have been stripping a SONY Cassette Player/Recorder TC-188SD. After stripping I still have tons of room to stuff my 3 toroids,  power supply, 6 relays, Caps, 4x 12AX7, in nice colored shields, a TI MSP430 for control, and a pa...
    • 18 Nov 2018
  • Hiraga Pre-amp: Build part 1

    phoenixcomm
    phoenixcomm
    Well, at last, I found my donor, a SONY TC-188SD Cassette Player. The cassette door will be clear plexiglass so can see the tubes glow. If I can get the parts, I will have a rather unique power supply that you only see in very exotic stuff. There a...
    • 8 Nov 2018
  • RIAA Pre Amp

    phoenixcomm
    phoenixcomm
    Times are a changing! I just ordered 4 ciramic tube sockets and 4 shield sets ( two in blue, and two in red ). I was asked why the two colors? "Because I can." Was my answer hey right and left chanels. I have a older Sony cassette player, I think it ...
    • 5 Nov 2018
  • Pseudo random number generator

    kk99
    kk99
    Back to AnalogEnter Your Electronics & Design Project for a chance to win a $100 Shopping Cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme Poll The basic idea was to create simple circuit with usage transistors, ...
    • 14 Oct 2018