Back to Analog
  • Challenges & Projects
  • Project14
  • Back to Analog
  • More
  • Cancel
Back to Analog
Blog Hiraga PreAmp .. build 5 - software for a tube amp?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Back to Analog to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 20 Dec 2018 5:07 AM Date Created
  • Views 643 views
  • Likes 3 likes
  • Comments 0 comments
  • analog pin
  • hiraga
  • diy audio
  • computer controled
  • power supply
  • software development
  • 12ax7
  • inrush current-limiter
  • pre-amplifier
  • arduino
  • diy electronics
Related
Recommended

Hiraga PreAmp .. build 5 - software for a tube amp?

phoenixcomm
phoenixcomm
20 Dec 2018

Well, life is still not on a good keel. I picked up at Fry's a proto shield, and some optocouplers. So the world keeps spinning and I am using a software-controlled power-supply
I don't have a formal sketch but this is what it will do:

Code ?

setup () {

     int relay[] = { pin2, pin3, pin4 };

     int sscr[] = { pin5, pin6, pin7};

     int lamps[] = { pin8, pin9, pin10, pin11 };

     int TRUE = 1;

     int ON = 1;

     int OFF = 0;

     delay(30000);

     int part;

     for ( part = 0; part < 3; part++ ) {

         relay[part] = ON; }

     lamps[3] = ON; // CPU IS UP}

 

loop () {

    for ( part = 0; part < 3; part++ ) {

         if( Vmax() == TRUE ) {

             sscr[part] = ON;

             delay(10000);

             relay[part] = OFF;

             lamps[part] = ON;}}

    idel();

    return; }

 

void idel() {

    // just keep awake;

    do {

         delay(60000);  // this is a sixty second sleep for ever

         while (TRUE);  }}

 

int Vmax() {} // have to check on the code still.

When the unit is turned on, by depressing the power switch in, that powers up the auxiliary power which provides 12vdc, 9vdc, and 24vdc via voltage doubler.

  1. The Arduino will come up and wait for about 5 seconds (to stabilize power)
  2. The Arduino will turn on relays 1 through 3 to apply to a resistive load to the toroids.
  3. The Arduino will loop through each toroid by using a counter in a for loop.
    1. The Arduino looks at AC voltage input (analog) and waits for max voltage when it sees the start of the drop
    2. The SSCR is now turned on.
    3. The Arduino waits 5-10 seconds
    4. The Arduino releases the bypass relay.
    5. The Arduino lights a status lamp

    Fins But Not Done

    I have a problem deriving Vmax AC with an analog input anybody out there knows how? Using a digital pin an optoisolator will not work as I get very small pulses at z-cross. So I have to do it the hard way. I, guess I will use a wall wart taken apart, as I don't need the case or plugs. and I will use a small resistor to limit voltage and current to about 4 volts ac and apply it to an analog pin.