Back to Analog
  • Challenges & Projects
  • Project14
  • Back to Analog
  • More
  • Cancel
Back to Analog
Blog Hiraga PreAmp .. build 5
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Back to Analog to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 17 Mar 2019 8:59 PM Date Created
  • Views 1024 views
  • Likes 5 likes
  • Comments 2 comments
  • pop-rivits
  • audio
  • 12ax7
  • anodized
  • hiraga pre-amp
Related
Recommended

Hiraga PreAmp .. build 5

phoenixcomm
phoenixcomm
17 Mar 2019
image
image

And the planet spins and life goes on. This has been a build from hell, nothing is normal, no chassis, or priced out of sight. My two preamp modules are 6" x 3" x 1.5" first I tried the guerrilla break which was very disappointing. I had the right Idea but I should have / could have mounted some hinges and that should have made a nice bend. So shell out more $$ on aluminum and pop rivet gun (the first one was defective, oh joy) the Arrow Gun does not always release the mandrel or stem of the rivet so you have to beet it out will a hammer. image

One of my pet peeves is that my drill press is sloppy! It is from Harbor Freight and cheaply made. The big problem with is the shaft or the quill I have seen some fixes ie drill and tap the head (cast whatever) and use screws of sorts to center it. this is something for a later day. and I would not use screws plastic or otherwise. I would use some Allen or Torx setscrews, as that's what they're used for.

The two preamps are mechanically done but need more work. image The front panel plexiglass is cut and now my belt sander's (porta-cable 371) belt broke hey it is 2.5" x 14"  and nobody has them. The back panel has to be drilled for the fuses and the auxiliary power outlets cut out (tomorrow) and the power has to be mounted along with the Arduino which I will mount under the power supply.

NOW MARCH

I have recently found how to remove all the paint from the front of the panel (Tech Tip III) I think while this is in an unassembled state I might send out the bare bright aluminum to be anodized (if it does not cost an arm and a leg!). And my power supply keeps blowing fuses.

The damn torids are a real pain in the ass! I'm going to have to see if I can get some samples from Ametherm. I have rigged a power supply on my desk and the damn things on start go from almost a dead short to full load in a few blinks of an eye.

Not Quite Disgusted quite Yet.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +1
    Now you know why people are going to laser cut wood construction. DAB
Parents
  • DAB
    DAB over 7 years ago

    Now you know why people are going to laser cut wood construction.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to DAB

    Yes, or PLA, but, 12AX7 x 4 I'm not looking for a fire!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to DAB

    Yes, or PLA, but, 12AX7 x 4 I'm not looking for a fire!!