Better World with Arduino
  • Challenges & Projects
  • Project14
  • Better World with Arduino
  • More
  • Cancel
Better World with Arduino
Blog Polite Passing and Safer Bicycling – the talking bike helmet with turn signals ** Version 1 **
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Better World with Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: robogary
  • Date Created: 23 Apr 2022 1:37 AM Date Created
  • Views 13379 views
  • Likes 12 likes
  • Comments 9 comments
  • better world with Arduino
  • arduino
  • betterworldch
Related
Recommended

Polite Passing and Safer Bicycling – the talking bike helmet with turn signals ** Version 1 **

robogary
robogary
23 Apr 2022

Make the World a Better Place : Polite Passing and Safer Bicycling – the courteous talking bike helmet with turn signals 

My wife asked if I was really going out in public with the helmet....... I did.

Then she asked if I really rode a bike in public with this helmet.......... I did.

She thinks I've totally lost my mind and have no shame.

The short video including field trials  

https://youtu.be/sLN3rrYaoKE

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The Polite Passing talking bicycle helmet helps improve traffic safety and promote proper greenway etiquette. People enjoy nature better and safer with polite & consistent greenway audio communication.

  • While bicycling, repeating “passing on your left”grows weary after awhile, especially getting frustrated with road hogs, inattentive pedestrians, runners and bikers on the phone or listening to music.
  • Bicycles are pretty quiet and can be fast. They surprise distracted people enjoying the outdoors and nature. Lets keep them safe.
  • LED turn signal flashers on the rear give warning to other traffic approaching you from behind. 

Version 1 – Arduino Nano control.   DFPlayer audio + 3W amp + speaker, activated manually with small pushbuttons mounted in helmet.  

imageimageimageimage

Why version 1 ? If time permits there could be a version 2 and a version 3, .....incorporating a Nicla  Sense ME using gyro signals for activation rather than pushbuttons. 

imageimageimageimage

The code: 

#include "Arduino.h"
#include "SoftwareSerial.h"
#include "DFRobotDFPlayerMini.h"

SoftwareSerial mySoftwareSerial(10, 11); // RX, TX
DFRobotDFPlayerMini myDFPlayer;
void printDetail(uint8_t type, int value);

int PassLeftPB; // LOW STATE is PB is pressed
int PassRightPB; // = digitalRead(3); // read the input pin, LOW STATE is PB is pressed
int ApproachingBehindPB; //= digitalRead(4); // read the input pin, LOW STATE is PB is pressed
int GoodDayPB; // = digitalRead(5); // read the input pin, LOW STATE is PB is pressed
int MrSofteePB; // = digitalRead(6); // read the input pin, LOW STATE is PB is pressed
int LeftTurnLED;
int RightTurnLED;


void setup()
{
/// add these digital inputs and outputs specific for the Polite Passing Helmet

pinMode(2,INPUT_PULLUP); // Pin 2 is PASS ON LEFT PB activate on 0
pinMode(3,INPUT_PULLUP); // Pin 3 is PASS ON Right PB activate on 0
pinMode(4,INPUT_PULLUP); // Pin 4 is approaching from BEHIND PB activate on 0
pinMode(5,INPUT_PULLUP); // Pin 5 is have a good day PB activate on 0
pinMode(6,INPUT_PULLUP); // Pin 6 is the Mister Softee Ice Cream Truck Theme activate on 0
pinMode(8,OUTPUT); // Pin 8 is the Left turn signal output
pinMode(9,OUTPUT); // Pin 9 is the Right turn signal output

mySoftwareSerial.begin(9600);
Serial.begin(115200);

// Serial.println();
// Serial.println(F("DFRobot DFPlayer Mini Demo"));
// Serial.println(F("Initializing DFPlayer ... (May take 3~5 seconds)"));

if (!myDFPlayer.begin(mySoftwareSerial)) { //Use softwareSerial to communicate with mp3.
Serial.println(F("Unable to begin:"));
Serial.println(F("1.Please recheck the connection!"));
Serial.println(F("2.Please insert the SD card!"));

while(true){
delay(0); // Code to compatible with ESP8266 watch dog.
}
}

// Serial.println(F("DFPlayer Mini online."));

myDFPlayer.setTimeOut(500); //Set serial communictaion time out 500ms

//----Set volume----
myDFPlayer.volume(10); //Set volume value (0~30).
myDFPlayer.volumeUp(); //Volume Up
myDFPlayer.volumeDown(); //Volume Down

//----Set different EQ----
myDFPlayer.EQ(DFPLAYER_EQ_NORMAL);

//----Set device we use SD as default----
myDFPlayer.outputDevice(DFPLAYER_DEVICE_SD);

//----Mp3 control----
// myDFPlayer.sleep(); //sleep
// myDFPlayer.reset(); //Reset the module
// myDFPlayer.enableDAC(); //Enable On-chip DAC
// myDFPlayer.disableDAC(); //Disable On-chip DAC
// myDFPlayer.outputSetting(true, 15); //output setting, enable the output and set the gain to 15

//----Mp3 play commands ----
// myDFPlayer.next(); //Play next mp3
// delay(1000);
// myDFPlayer.previous(); //Play previous mp3
// delay(1000);
myDFPlayer.play(4); //Play GDay as a test
delay(5000);
// myDFPlayer.loop(1); //Loop the first mp3
// delay(1000);
// myDFPlayer.pause(); //pause the mp3
// delay(1000);
// myDFPlayer.start(); //start the mp3 from the pause
// delay(1000);
// myDFPlayer.playFolder(15, 4); //play specific mp3 in SD:/15/004.mp3; Folder Name(1~99); File Name(1~255)
// delay(1000);
// myDFPlayer.enableLoopAll(); //loop all mp3 files.
// delay(1000);
// myDFPlayer.disableLoopAll(); //stop loop all mp3 files.
// delay(1000);
// myDFPlayer.playMp3Folder(4); //play specific mp3 in SD:/MP3/0004.mp3; File Name(0~65535)
// delay(1000);
// myDFPlayer.advertise(3); //advertise specific mp3 in SD:/ADVERT/0003.mp3; File Name(0~65535)
// delay(1000);
// myDFPlayer.stopAdvertise(); //stop advertise
// delay(1000);
// myDFPlayer.playLargeFolder(2, 999); //play specific mp3 in SD:/02/004.mp3; Folder Name(1~10); File Name(1~1000)
// delay(1000);
// myDFPlayer.loopFolder(5); //loop all mp3 files in folder SD:/05.
// delay(1000);
// myDFPlayer.randomAll(); //Random play all the mp3.
// delay(1000);
// myDFPlayer.enableLoop(); //enable loop.
// delay(1000);
// myDFPlayer.disableLoop(); //disable loop.
// delay(1000);

//----Read imformation----
// Serial.println(myDFPlayer.readState()); //read mp3 state
// Serial.println(myDFPlayer.readVolume()); //read current volume
// Serial.println(myDFPlayer.readEQ()); //read EQ setting
// Serial.println(myDFPlayer.readFileCounts()); //read all file counts in SD card
// Serial.println(myDFPlayer.readCurrentFileNumber()); //read current play file number
// Serial.println(myDFPlayer.readFileCountsInFolder(3)); //read file counts in folder SD:/03
}

void loop()
{
// static unsigned long timer = millis();

// if (millis() - timer > 3000) {
// timer = millis();
// myDFPlayer.next(); //Play next mp3 every 3 second.
// }

// if (myDFPlayer.available()) {
// printDetail(myDFPlayer.readType(), myDFPlayer.read()); //Print the detail message from DFPlayer to handle different errors and states.
// }

//------- my code starts here -----------------------
PassLeftPB = digitalRead(2); // read the input pin, LOW STATE is PB is pressed
PassRightPB = digitalRead(3); // read the input pin, LOW STATE is PB is pressed
ApproachingBehindPB = digitalRead(4); // read the input pin, LOW STATE is PB is pressed
GoodDayPB = digitalRead(5); // read the input pin, LOW STATE is PB is pressed
MrSofteePB = digitalRead(6); // read the input pin, LOW STATE is PB is pressed

if (PassLeftPB==LOW)
{
for (int i=0; i<4; i++)
{
digitalWrite(8, HIGH); // sets the LED on
delay(150); // waits for a second
digitalWrite(8, LOW); // sets the LED off
delay(100); // waits for a second
}

Serial.println(F("PASSING LEFT"));
myDFPlayer.play(1); //Play left turn
delay(2000);

for (int i=0; i<9; i++)
{
digitalWrite(8, HIGH); // sets the LED on
delay(150); // waits for a second
digitalWrite(8, LOW); // sets the LED off
delay(100); // waits for a second
}

}

if (PassRightPB==LOW)
{
for (int i=0; i<4; i++)
{
digitalWrite(9, HIGH); // sets the LED on
delay(150); // waits for a second
digitalWrite(9, LOW); // sets the LED off
delay(100); // waits for a second
}
myDFPlayer.play(2); //Play right turn
delay(2000);

for (int i=0; i<9; i++)
{
digitalWrite(9, HIGH); // sets the LED on
delay(150); // waits for a second
digitalWrite(9, LOW); // sets the LED off
delay(100); // waits for a second
}

}

if (ApproachingBehindPB==LOW)
{
myDFPlayer.play(3); //Play from behind
delay(5000);
}

if (GoodDayPB==LOW)
{
myDFPlayer.play(4); //Play from behind
delay(5000);
}
if (MrSofteePB==LOW)
{
myDFPlayer.play(5); //Play from behind
delay(31000);
}

}

void printDetail(uint8_t type, int value){
switch (type) {
case TimeOut:
Serial.println(F("Time Out!"));
break;
case WrongStack:
Serial.println(F("Stack Wrong!"));
break;
case DFPlayerCardInserted:
Serial.println(F("Card Inserted!"));
break;
case DFPlayerCardRemoved:
Serial.println(F("Card Removed!"));
break;
case DFPlayerCardOnline:
Serial.println(F("Card Online!"));
break;
case DFPlayerUSBInserted:
Serial.println("USB Inserted!");
break;
case DFPlayerUSBRemoved:
Serial.println("USB Removed!");
break;
case DFPlayerPlayFinished:
Serial.print(F("Number:"));
Serial.print(value);
Serial.println(F(" Play Finished!"));
break;
case DFPlayerError:
Serial.print(F("DFPlayerError:"));
switch (value) {
case Busy:
Serial.println(F("Card not found"));
break;
case Sleeping:
Serial.println(F("Sleeping"));
break;
case SerialWrongStack:
Serial.println(F("Get Wrong Stack"));
break;
case CheckSumNotMatch:
Serial.println(F("Check Sum Not Match"));
break;
case FileIndexOut:
Serial.println(F("File Index Out of Bound"));
break;
case FileMismatch:
Serial.println(F("Cannot Find File"));
break;
case Advertise:
Serial.println(F("In Advertise"));
break;
default:
break;
}
break;
default:
break;
}

}

  • Sign in to reply
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    You may need to add a "No, Passing on your other left / right" for those who struggle with their left & right and start to move in the wrong direction  Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago in reply to beacon_dave

    For sure. I've had that happen. Someone was wandering on the greenway deep in imagination land, I announced I was passing on the right. The guy pivoted on his right foot turning to look behind, doing a 180 degree turn rather than just turning his head, stepped  right in front of me. I avoided hitting the nomad, but went over the handlebars and dislocated my collarbone. Lucky I had a helmet on.  At that point I put the 90 dB sirens on my bicycles. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to robogary

    With two sound projectors you could play with the 'precedence effect'. Delay the sound to the opposite channel by 10-20ms so that you maintain volume level but localise perception to the side you intend to pass on.

    Not sure what you do if you plan to pass two people by taking the centre line ? boost level from 90 to 120dBspl perhaps Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago in reply to beacon_dave

    phased 3D sound with an echo chip, thats an idea. Really screw with perception.

    If two people are hogging the centerline, which is often a young buck focused on a doe on a cycling date, I play the ice cream truck music. 

    ..........Now that really gets people attention.

    If that fails..............then the 90 dB siren. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 4 years ago in reply to beacon_dave

    phased 3D sound with an echo chip, thats an idea. Really screw with perception.

    If two people are hogging the centerline, which is often a young buck focused on a doe on a cycling date, I play the ice cream truck music. 

    ..........Now that really gets people attention.

    If that fails..............then the 90 dB siren.