Cheer Us Up
  • Challenges & Projects
  • Project14
  • Cheer Us Up
  • More
  • Cancel
Cheer Us Up
Blog make robot friend. Bender
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cheer Us Up to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 12 Apr 2021 12:42 AM Date Created
  • Views 7634 views
  • Likes 20 likes
  • Comments 35 comments
  • cheerusupch
  • robot
  • national robotics week
  • diy
  • servo
  • ws2812
  • mkr1010
  • project14
  • bender
  • futurama
  • arduino
  • 3d print
Related
Recommended

make robot friend. Bender

fmilburn
fmilburn
12 Apr 2021

I've been unable to get together with my technically minded friends and talk about interests.  And so, I decided to make robot friend.  Bender.

image

As everyone knows, Bender shot to fame on the Futurama television show that aired from March 28, 1999 to August 10, 2003.  I decided to build him because of all the robots on television, the movies and comic books he is the most human like.  Bender was built in the year 2996 and designated Bending Unit 22, unit number 1,729, serial number 2716057.  The Unit Number 1,729 is significant in that it is the smallest number expressible as the sum of two cubes in two different ways.  But I digress.  His human like characteristics include extreme narcissism, over confidence in his abilities, and ill-tempered rudeness.  Sometimes I really miss the workplace.

 

Building Bender

 

Bender is a 3d printed project with servos, WS2812b LEDs, and DFRobot sound module driven by an Arduino MKR1010.  He was designed in Fusion360 and printed on an Anycubic i3 Mega.  The exterior is "silky" silver PLA and unpainted.  There are 6 main structural parts:

  • Lower head
  • Middle head
  • Mouth carousel
  • Eye box
  • Upper head
  • Antenna

image

The lower head holds the mouth carousel in place and has a central pin that it rotates on.  The carousel design was inspired by a very interesting build by James Bruton.

image

The middle head holds the eye box in place and slips on with a friction fit to the lower head.  There is also a motor bracket and servo to rotate the mouth carousel.  Not shown are the 3D printed mounting attachments and brackets for the microcontroller, battery, speaker, and so on.

image

The eye box holds the 3d printed ovoid eyes (printed in two pieces and glued together), two servos, and associated motor mounting hardware.  It slides into the middle head and is held in place with a dab of hot glue.

image

The upper head and antenna are printed in two pieces and slip over the middle head.

image

According to my research Bender's is 5 feet 6 inches (1.68 m) tall and a little over 6 feet (1.8 m) with the antenna.  This build is a 1:1 scale reproduction.  The lower head and middle head took about 8 hours to print and the upper head 16 hours.  The other pieces took between 15 minutes and 4 hours to print so the printer has been busy and was working around 35 hours total.

 

Electronics

 

Bender runs on alcohol which he uses to produce electricity.  In this reproduction a 18650 battery is used to power the Arduino MKR1010 microcontroller, 3 servos, 5 WS2812b LEDs, and DFRobot DFMini Pro sound unit as shown in the schematic below.

image

The Arduino and DFPlayer Mini are mounted on a prototyping board which also contains headers for the servos and LEDs for easy assembly and repair.  Not shown is a WeMos boost converter and charging PCB for a 18650 battery.  The servos and LEDs are powered directly off of the 5V supply of the boost converter.  The Arduino receives USB power from the boost converter and supplies 3V3 to the sound module.

image

Assembly

 

Below we see Bender on the factory floor in various stages of assembly and testing.  The WS2812b LEDs are mounted on PCB strips that were designed by me some time back for toys for the grandkids and can be snapped apart at mouse bites to the desired length.  The paper mouth inserts into a slot that can be seen in the mouth carousel.  Bender is fairly easily disassembled and reassembled for such things as parts replacements and repair when needed.

{gallery} Assembly on the Factory Floor

image

Ready for Assembly

image

Eye Box Assembly

image

Preparing for Brain Transplant

image

Brains

image

Assembly complete

 

Code

 

The Arduino sketch used to control Bender over WiFi is very similar to what was used in Cat Commander.  Feel free to look through and use it but it is over 600 lines and a total hack.  Even for me it is a total hack.  There are 9 facial expressions and 32 phrases that can be controlled although more could be easily added.

/* make robot friend Bender
 * developed on Arduino MKR 1010
 * 
 * WiFi control - Add arduino_secrets.h with following lines to set up
 *    #define SECRET_SSID "SSID"
 *    #define SECRET_PASS "password"
 * Eye and mouth movement using 3 servos
 * Lights eyes and mouth with six WS2812 LEDs
 * Speech using DFRobot DFPlayer Mini
 * 
 * by fmilburn April 2021
 * 
 * This code is in the public domain
 */


#include "arduino_secrets.h"
#include <WiFiNINA.h>
#include <WiFiUdp.h>
#include <Adafruit_NeoPixel.h>
#include <Servo.h>
#include <DFRobotDFPlayerMini.h>


// Miscellaneous
const int DEBUG = false;       // true turns on serial print to terminal
const int DELAYMOVE =  1000;   // pause during expressions


// Pixels
const int PIXELPIN  =  6;
const int NUMPIXELS =  6;                                                                                          


// Eye Servos
const int LEFTEYEPIN = 4;
const int RIGHTEYEPIN = 5;
const int SLOW      =   30;   // servo movement speeds
const int MEDIUM    = 15;
const int FAST      = 5;
const int LEFTADJ =     35;   // variables to adjust servo error
const int RIGHTADJ =    20;
const int SERVOFRONT =  90;   // unadjusted servo eye direction positons
const int SERVORIGHT =  50;
const int SERVOLEFT =   130;


// Mouth Servo
const int MOUTHPIN = 7;
const int MOUTHRIGHT = 70;    // mouth movements during speech
const int MOUTHLEFT = 110;


// Speech
const int VOLUME = 20;        // volume in range 1 to 30
const int TRACKS = 35;        // number of tracks
unsigned long trackLength[TRACKS]={     // stores the track length in milliseconds
  trackLength[0] = 0,         // not used
  trackLength[1] = 2300,      // Bite
  trackLength[2] = 2100,      // Evil laugh
  trackLength[3] = 2200,      // A cake
  trackLength[4] = 5700,      // Afterlife
  trackLength[5] = 1600,      // All the money
  trackLength[6] = 3400,      // Bad computer
  trackLength[7] = 1200,      // You kidding
  trackLength[8] = 4500,      // Beer
  trackLength[9] = 1900,      // Bring it on
  trackLength[10] = 6400,     // Cheers me up
  trackLength[11] = 3700,     // Compare
  trackLength[12] = 1600,     // Death to humans
  trackLength[13] = 1700,     // Dream on
  trackLength[14] = 2400,     // Enjoying it
  trackLength[15] = 3100,     // Everyone else's fault
  trackLength[16] = 1800,     // Hello peasants
  trackLength[17] = 2600,     // Hilarity unit
  trackLength[18] = 7500,     // Hitting them
  trackLength[19] = 1200,     // I'm Bender
  trackLength[20] = 2600,     // Lawsuit
  trackLength[21] = 2200,     // Like best
  trackLength[22] = 3000,     // Lovable Rascal
  trackLength[23] = 5200,     // Mechanical heart
  trackLength[24] = 7000,     // Nanosecond
  trackLength[25] = 1600,     // Nerds
  trackLength[26] = 1000,     // No thanks
  trackLength[27] = 2400,     // Noise hole
  trackLength[28] = 2600,     // None of your business
  trackLength[29] = 900,      // Oh my god
  trackLength[30] = 1800,     // So beautiful
  trackLength[31] = 1800,     // Square
  trackLength[32] = 1500,     // Terrible shame
  trackLength[33] = 1400,     // Thank you
  trackLength[34] = 7300};    // The end


// WiFi
char ssid[] = SECRET_SSID;        // network SSID (name)
char pass[] = SECRET_PASS;        // network password
int keyIndex = 0;                 // network key Index number (needed for WEP)
int status = WL_IDLE_STATUS;


// Server
int track = 0;
int expression = 0;


// Instantiation
WiFiServer server(80);            // server socket
WiFiClient client = server.available();
DFRobotDFPlayerMini speech;
Adafruit_NeoPixel pixels(NUMPIXELS, PIXELPIN, NEO_GRB + NEO_KHZ800);
Servo leftEye;
Servo rightEye;
Servo mouth;


// -----------------------------------------------------------------
// setup
// -----------------------------------------------------------------
void setup(){


  if (DEBUG == true){
    Serial.begin(115200);                                           
    while(!Serial);
    Serial.println("Started!");
  }
  
  initWifi();
  if (DEBUG == true){
    printWifiStatus();              
  }


  Serial1.begin(9600);                      // Speech on Serial1
  while(!Serial1);
  while (!speech.begin(Serial1));

  pixels.begin();                           // WS2812 / neopixels
  pixels.clear();


  leftEye.attach(LEFTEYEPIN);               // servos
  rightEye.attach(RIGHTEYEPIN);
  mouth.attach(MOUTHPIN);


  // intro
  showPixels(60, 0, 0,   200, 1200, 80);    // red, yellow
  waggleEyes(MEDIUM);
  playTrack(2, VOLUME, trackLength[2], MEDIUM);
  showPixels(50, 40, 10, 200, 1200, 80);    // yellow, yellow
}


// -----------------------------------------------------------------
// loop
// -----------------------------------------------------------------
void loop(){


  client = server.available();
  if (client){
    webPage();
    if (expression > 0){
      playExpression(expression);
      expression = 0;
    }
    if (track > 0){
      playTrack(track, VOLUME, trackLength[track], MEDIUM);
      track = 0;
    }
  }
}


// -----------------------------------------------------------------
// showPixels
// -----------------------------------------------------------------
void showPixels(int redEye, int greenEye, int blueEye,
                int redMouth, int greenMouth, int blueMouth){
                  
  pixels.setPixelColor(0, pixels.Color(redMouth, greenMouth, blueMouth));
  pixels.setPixelColor(1, pixels.Color(redMouth, greenMouth, blueMouth));
  pixels.setPixelColor(2, pixels.Color(redMouth, greenMouth, blueMouth));
  pixels.setPixelColor(3, pixels.Color(redMouth, greenMouth, blueMouth));
  pixels.setPixelColor(4, pixels.Color(redEye, greenEye, blueEye));
  pixels.setPixelColor(5, pixels.Color(redEye, greenEye, blueEye));
  pixels.show(); 
}


// -----------------------------------------------------------------
// lookFrontToLeft
// -----------------------------------------------------------------
void lookFrontToLeft(unsigned long eyePause){
  
  int servoPos;
  for (servoPos = SERVOFRONT; servoPos <= SERVOLEFT; servoPos += 1){
    leftEye.write(servoPos+LEFTADJ);
    rightEye.write(servoPos+RIGHTADJ);
    delay(eyePause);                     
  }
}


// -----------------------------------------------------------------
// lookLeftToFront
// -----------------------------------------------------------------
void lookLeftToFront(unsigned long eyePause){
  
  int servoPos;
  for (servoPos = SERVOLEFT; servoPos >= SERVOFRONT; servoPos -= 1){
    leftEye.write(servoPos+LEFTADJ);
    rightEye.write(servoPos+RIGHTADJ);
    delay(eyePause);                      
  }
}


// -----------------------------------------------------------------
// lookFrontToRight
// -----------------------------------------------------------------
void lookFrontToRight(unsigned long eyePause){
  
  int servoPos;
  for (servoPos = SERVOFRONT; servoPos >= SERVORIGHT; servoPos -= 1) {
    leftEye.write(servoPos+LEFTADJ);
    rightEye.write(servoPos+RIGHTADJ);
    delay(eyePause);                     
  }
}


// -----------------------------------------------------------------
// lookRightToFront
// -----------------------------------------------------------------
void lookRightToFront(unsigned long eyePause){
  
  int servoPos;
  for (servoPos = SERVORIGHT; servoPos <= SERVOFRONT; servoPos += 1){
    leftEye.write(servoPos+LEFTADJ);
    rightEye.write(servoPos+RIGHTADJ);
    delay(eyePause);                      
  }
}


// -----------------------------------------------------------------
// waggleEyes
// -----------------------------------------------------------------
void waggleEyes(unsigned long eyePause){
  
  int servoPos;
  for (servoPos = SERVOFRONT; servoPos <= 115; servoPos += 1){
    leftEye.write(servoPos+LEFTADJ);
    rightEye.write(servoPos+RIGHTADJ);  
    delay(eyePause);                
  }
  for (servoPos = 115; servoPos >= 65; servoPos -= 1){
    leftEye.write(servoPos+LEFTADJ);
    rightEye.write(servoPos+RIGHTADJ);     
    delay(eyePause);             
  }
  for (servoPos = 65; servoPos <= SERVOFRONT; servoPos += 1){
    leftEye.write(servoPos+LEFTADJ);
    rightEye.write(servoPos+RIGHTADJ);  
    delay(eyePause);                 
  }
}


// -----------------------------------------------------------------
// waggleMouth
// -----------------------------------------------------------------
void waggleMouth(int trackLen, unsigned long mouthSpeed){


  unsigned long stopWaggle = millis() + trackLen;
  int servoPos = SERVOFRONT;
  int servoDir = 1;
  while (millis() <= stopWaggle){
    if (servoPos > MOUTHLEFT && servoDir == 1){
      servoDir = -1;
    }
    if (servoPos < MOUTHRIGHT && servoDir == -1){
      servoDir = 1;
    }
    servoPos = servoPos + servoDir;
    mouth.write(servoPos);
    delay(mouthSpeed);                
  }
  mouth.write(SERVOFRONT);
}


// -----------------------------------------------------------------
// playExpression
// -----------------------------------------------------------------
void playExpression(int expressionNo){


  if (DEBUG == true){
    Serial.print("Expression ");
    Serial.print(expressionNo);
    Serial.println(" requested");
  }
  if (expressionNo == 1){
    showPixels(50, 40, 10, 200, 1200, 80);    // yellow, yellow
  }
  if (expressionNo == 2){
    showPixels(60, 0, 0,   200, 1200, 80);    // red, yellow
  }
  if (expressionNo == 3) {
    showPixels(50, 40, 10, 200, 1200, 80);    // yellow, yellow
    lookFrontToRight(FAST);
    delay(DELAYMOVE*2);
    lookRightToFront(SLOW);
  }
    if (expressionNo == 4) {
    showPixels(60, 0, 0, 200, 1200, 80);      // red, yellow
    lookFrontToRight(FAST);
    delay(DELAYMOVE*2);
    lookRightToFront(SLOW);
  }
    if (expressionNo == 5) {
    showPixels(50, 40, 10, 200, 1200, 80);    // yellow, yellow
    lookFrontToLeft(FAST);
    delay(DELAYMOVE*2);
    lookLeftToFront(SLOW);
  }
    if (expressionNo == 6) {
    showPixels(60, 0, 0, 200, 1200, 80);      // red, yellow
    lookFrontToLeft(FAST);
    delay(DELAYMOVE*2);
    lookLeftToFront(SLOW);
  }
  if (expressionNo == 7) {
    showPixels(50, 40, 10, 200, 1200, 80);    // yellow, yellow
    waggleEyes(SLOW);
  }
  if (expressionNo == 8) {
    showPixels(60, 0, 0, 200, 1200, 80);      // red, yellow
    waggleEyes(SLOW);
  }
  if (expressionNo == 9) {
    waggleMouth(1000, MEDIUM);
  }
}


// -----------------------------------------------------------------
// playTrack
// -----------------------------------------------------------------
void playTrack(int trackNo, int volume, int trackLen, unsigned long mouthSpeed){


  if (DEBUG == true){
    Serial.print("Track ");
    Serial.print(trackNo);
    Serial.println(" requested");
  }
  
  speech.volume(volume);  //Set volume from 0 to 30
  speech.play(trackNo);


  unsigned long stopWaggle = millis() + trackLen;
  int servoPos = SERVOFRONT;
  int servoDir = 1;
  while (millis() <= stopWaggle){
    if (servoPos > MOUTHLEFT && servoDir == 1){
      servoDir = -1;
    }
    if (servoPos < MOUTHRIGHT && servoDir == -1){
      servoDir = 1;
    }
    servoPos = servoPos + servoDir;
    mouth.write(servoPos);
    delay(mouthSpeed);                
  }
  mouth.write(SERVOFRONT);
}
  
// -----------------------------------------------------------------
// initialize WiFi and start server
// -----------------------------------------------------------------
void initWifi(){
  
  // check for the WiFi module:
  if (WiFi.status() == WL_NO_MODULE) {
    while (true){
      // print error msg here
    }
  }


  // attempt to connect to Wifi network:
  while (status != WL_CONNECTED) {
    // Connect to WPA/WPA2 network. Change this line if using open or WEP network:
    status = WiFi.begin(ssid, pass);
    // wait 10 seconds for connection:
    delay(10000);
  }
  server.begin();
}




// -----------------------------------------------------------------
// webPage
// -----------------------------------------------------------------
void webPage() {
  
  if (client) {                             // check if there is a cllent
    String currentLine = "";                // string to hold incoming data from the client
    while (client.connected()) {            // loop while the client's connected
      if (client.available()) {             // check for byte to read from the client,
        char c = client.read();             // read a byte, then
        if (c == '\n') {                    // respond only when there is new line


          // if the current line is blank there were two newline characters in a row.
          // that's the end of the client HTTP request, so send a response:
          if (currentLine.length() == 0) {


            // standard response header
            client.println("HTTP/1.1 200 OK");
            client.println("Content-Type: text/html");
            client.println("Connection: close");
            client.println();


            // web page
            client.println("<!DOCTYPE html>");
            client.println("<html>");
            client.println("<head>");
            client.println("<title>Bender</title>");
            client.println("</head>");
            
            client.println("<body>");
            // Title
            client.println("<h1>Bender</h1>");


            client.print("------------- Expressions -------------<br>");
            client.print("<a href=\"/NORMAL\">Normal</a> eyes<br>");                   // 1 
            client.print("<a href=\"/ANGRY\">Angry</a> eyes<br>");                     // 2
            client.print("<a href=\"/NORMAL_R\">Right</a> look normal<br>");           // 3
            client.print("<a href=\"/ANGRY_R\">Right</a> look angry<br>");             // 4
            client.print("<a href=\"/NORMAL_L\">Left</a> look normal<br>");            // 5
            client.print("<a href=\"/ANGRY_L\">Left</a> look angry<br>");              // 6
            client.print("<a href=\"/NORMAL_EYE_WAGGLE\">Waggle</a> eyes normal<br>"); // 7
            client.print("<a href=\"/ANGRY_EYE_WAGGLE\">Waggle</a> eyes angry<br>");   // 8
            client.print("<a href=\"/MOUTH_WAGGLE\">Waggle</a> mouth<br>");            // 9


            client.print("<br>---------------- Phrases ---------------<br>");
            client.print("<a href=\"/BITE\">1 Bite my shiny</a><br>"); 
            client.print("<a href=\"/EVIL\">2 Evil laugh</a><br>");
            client.print("<a href=\"/ACAK\">3 A cake you want</a><br>");
            client.print("<a href=\"/AFTE\">4 Afterlife</a><br>");
            client.print("<a href=\"/ALLT\">5 All the money</a><br>");
            client.print("<a href=\"/BADC\">6 Bad computer</a><br>");
            client.print("<a href=\"/YOUK\">7 You kidding</a><br>");
            client.print("<a href=\"/BEER\">8 Beer</a><br>");
            client.print("<a href=\"/BRIN\">9 Bring it on baby</a><br>");
            client.print("<a href=\"/CHEE\">10 Cheers me up</a><br>");
            client.print("<a href=\"/COMP\">11 Compare</a><br>");
            client.print("<a href=\"/DREA\">12 Dream on</a><br>");
            client.print("<a href=\"/EVER\">13 Everyone elses fault</a><br>");
            client.print("<a href=\"/HELLO\">14 Hello peasants</a><br>");
            client.print("<a href=\"/HILA\">15 Hilarity</a> <br>");
            client.print("<a href=\"/HITT\">16 Hitting them</a><br>");
            client.print("<a href=\"/IMBE\">17 I'm Bender</a><br>");
            client.print("<a href=\"/LAWS\">18 Lawsuit</a><br>");
            client.print("<a href=\"/LIKE\">19 Like best</a><br>");
            client.print("<a href=\"/LOVA\">20 Lovable rascal</a><br>");
            client.print("<a href=\"/MECH\">21 Mechanical heart</a><br>");
            client.print("<a href=\"/NANO\">22 Nanosecond</a><br>");
            client.print("<a href=\"/NERD\">23 Nerds</a> <br>");
            client.print("<a href=\"/NOTH\">24 No thanks</a><br>");
            client.print("<a href=\"/NOIS\">25 Noise hole</a><br>");
            client.print("<a href=\"/NONE\">26 None of your business</a><br>");
            client.print("<a href=\"/OHMY\">27 Oh my god</a><br>");
            client.print("<a href=\"/SOBE\">28 So beautiful</a><br>");
            client.print("<a href=\"/SQUA\">29 Square</a> <br>");
            client.print("<a href=\"/TERR\">30 Terrible shame</a><br>");
            client.print("<a href=\"/THAN\">31 Thank you</a><br>");
            client.print("<a href=\"/THEE\">32 The end</a><br>");


            //client.println("<\h2>");
            //client.println();
            client.println("</body>");
            
            client.println("</html>");   
                    
            // break out of the while loop:
            break;
          }
          else {      // if you got a newline, then clear currentLine:
            currentLine = "";
          }
        }
        else if (c != '\r') {    // if you got anything else but a carriage return character,
          currentLine += c;      // add it to the end of the currentLine
        }
        
        if (currentLine.endsWith("GET /NORMAL")) { 
          expression = 1;
        }
        if (currentLine.endsWith("GET /ANGRY")) {
          expression = 2;
        }
        if (currentLine.endsWith("GET /NORMAL_R")) {
          expression = 3;
        }
        if (currentLine.endsWith("GET /ANGRY_R")) {
          expression = 4;
        }
        if (currentLine.endsWith("GET /NORMAL_L")) {
          expression = 5;
        }
        if (currentLine.endsWith("GET /ANGRY_L")) {
          expression = 6;
        }
        if (currentLine.endsWith("GET /NORMAL_EYE_WAGGLE")) {
          expression = 7;
        }
        if (currentLine.endsWith("GET /ANGRY_EYE_WAGGLE")) {
          expression = 8;
        }
        if (currentLine.endsWith("GET /MOUTH_WAGGLE")) {
          expression = 9;
        }
        if (currentLine.endsWith("GET /BITE")) {
          track = 1;
        }
        if (currentLine.endsWith("GET /EVIL")) {
          track = 2;
        }
        if (currentLine.endsWith("GET /ACAK")) {
          track = 3;
        }
        if (currentLine.endsWith("GET /AFTE")) {
          track = 4;
        }
        if (currentLine.endsWith("GET /ALLT")) {
          track = 5;
        }
        if (currentLine.endsWith("GET /BADC")) {
          track = 6;
        }
        if (currentLine.endsWith("GET /YOUK")) {
          track = 7;
        }
        if (currentLine.endsWith("GET /BEER")) {
          track = 8;
        }
        if (currentLine.endsWith("GET /BRIN")) {
          track = 9;
        }
        if (currentLine.endsWith("GET /CHEE")) {
          track = 10;
        }
        if (currentLine.endsWith("GET /COMP")) {
          track = 11;
        }
        if (currentLine.endsWith("GET /DEAT")) {
          track = 12;
        }
        if (currentLine.endsWith("GET /DREA")) {
          track = 13;
        }
        if (currentLine.endsWith("GET /ENJO")) {
          track = 14;
        }
        if (currentLine.endsWith("GET /EVER")) {
          track = 15;
        }
        if (currentLine.endsWith("GET /HELLO")) {
          track = 16;
        }
        if (currentLine.endsWith("GET /HILA")) {
          track = 17;
        }
        if (currentLine.endsWith("GET /HITT")) {
          track = 18;
        }
        if (currentLine.endsWith("GET /IMBE")) {
          track = 19;
        }
        if (currentLine.endsWith("GET /LAWS")) {
          track = 20;
        }
        if (currentLine.endsWith("GET /LIKE")) {
          track = 21;
        }
        if (currentLine.endsWith("GET /LOVA")) {
          track = 22;
        }
        if (currentLine.endsWith("GET /MECH")) {
          track = 23;
        }
        if (currentLine.endsWith("GET /NANO")) {
          track = 24;
        }
        if (currentLine.endsWith("GET /NERD")) {
          track = 25;
        }
        if (currentLine.endsWith("GET /NOTH")) {
          track = 26;
        }
        if (currentLine.endsWith("GET /NOIS")) {
          track = 27;
        }
        if (currentLine.endsWith("GET /NONE")) {
          track = 28;
        }
        if (currentLine.endsWith("GET /OHMY")) {
          track = 29;
        }
        if (currentLine.endsWith("GET /SOBE")) {
          track = 30;
        }
        if (currentLine.endsWith("GET /SQUA")) {
          track = 31;
        }
        if (currentLine.endsWith("GET /TERR")) {
          track = 32;
        }
        if (currentLine.endsWith("GET /THAN")) {
          track = 33;
        }
        if (currentLine.endsWith("GET /THEE")) {
          track = 34;
        }
      }
    }
    // close the connection:
    client.stop();
  }
}




// -----------------------------------------------------------------
// print the WiFi Status
// -----------------------------------------------------------------
void printWifiStatus() {
  
  IPAddress ip = WiFi.localIP(); 
  
  if (DEBUG == true){
    // print the SSID of the network you're attached to:
    Serial.print("SSID: ");
    Serial.println(WiFi.SSID());
  
    // print your board's IP address:
    Serial.print("IP Address: ");
    Serial.println(ip);
  
    // print the received signal strength:
    long rssi = WiFi.RSSI();
    Serial.print("signal strength (RSSI):");
    Serial.print(rssi);
    Serial.println(" dBm");


  }
}

 

Video Demonstration

 

In this short 2 1/2 minute video I interview Bender and he gives us a taste of what the Robot Overlords will really be like.  Excuse his crude manners, he knows not better.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Conclusion

 

I'm out of time so need to publish.  This project will serve as my National Robotics Week contribution (it ends today) as well as a belated Arduino Day celebratory project.  And hopefully it cheers you up a little.  I need to use my inkjet printer for the mouth instead of freehand drawing and that can be easily done and changed out.  The WiFi user interface is a bit rough.  The eye servos are cheap and metal gears with less backlash would be better.  The mouth carousel is noisy and a proper bearing should be used.  Other than that there are a few changes that could be done to make assembly easier but I like the way it turned out.  And my videos are amateurish.  If you made it this far thanks for reading and as always questions, comments and suggestions are appreciated.

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 5 years ago in reply to ralphjy +7
    Thanks Ralph. It has taken a while but I am finally getting comfortable with Fusion 360 although there are areas I haven't looked into like modeling kinematic motion which would be interesting. I had a…
  • javagoza
    javagoza over 5 years ago +7
    It looks great and is super funny. I think he's asking you for a BendërBrau.
  • ralphjy
    ralphjy over 5 years ago +6
    Very nice build. Especially like the effect of the silver PLA. Great construction. I still haven't taken the time to learn Fusion 360... I should. On a funny related note, I just swapped over to using…
Parents
  • dubbie
    dubbie over 5 years ago

    Frank,

     

    A great 3D design and build. I also like Bender - well he is a robot. I especially like the two eye blls, particularly when he goes a bit cross eyed. Was that effect intentional?

     

    Are you now planning to buiid the rest of him?

     

    Dubbie

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago in reply to dubbie

    Hi Dubbie and thanks.  It wasn't intentional to have his eyes wonky.  There was play in the mechanism due to my connection design between the servos and the eye.  I made some modifications and reprinted them which removed a lot of it but there is still some remaining.  In addition to play in the connection I think the plastic gears and maybe nonlinearity in the pots contribute.  In the end I kind of liked the effect as well and left it as is.

     

    I don't plan to build the rest of him.  I am afraid of what a 6 foot robot would do when I am not around to watch him :-)

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 5 years ago in reply to dubbie

    Hi Dubbie and thanks.  It wasn't intentional to have his eyes wonky.  There was play in the mechanism due to my connection design between the servos and the eye.  I made some modifications and reprinted them which removed a lot of it but there is still some remaining.  In addition to play in the connection I think the plastic gears and maybe nonlinearity in the pots contribute.  In the end I kind of liked the effect as well and left it as is.

     

    I don't plan to build the rest of him.  I am afraid of what a 6 foot robot would do when I am not around to watch him :-)

    • Cancel
    • Vote Up +6 Vote Down