Control Systems
  • Challenges & Projects
  • Project14
  • Control Systems
  • More
  • Cancel
Control Systems
Blog Running in circles ? Make it perfect circles with regulators
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Control Systems to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: robogary
  • Date Created: 7 Oct 2020 12:20 AM Date Created
  • Views 2963 views
  • Likes 7 likes
  • Comments 3 comments
  • controlsystemsch
Related
Recommended

Running in circles ? Make it perfect circles with regulators

robogary
robogary
7 Oct 2020

Try to run a 2 motor robot in a perfect circle by itself.......It wont  :-(

 

There are many variables that prevent perfection:

wheel friction, wheel motor speed mismatches, gear backlash, wheel slip,

wheel diameter mismatches, varying battery voltage, motor differences,

AND resolution of the PWM controlling the motor speed.

 

However ....applying a simple error correction system while the robot circles...the results are pretty amazing.

 

First, let's understand how the robot drives in a circle.

In this illustration , the left hand side wheel has to go faster and further than the right hand side wheel to get back to the starting line.

The ratio of left side speed to right side speed sets the circle diameter (turning radius).

 

 

image

 

Theoretically, tracing out a circle should be easy, its just a ratio of wheel position (and speeds)

The ratio is difficult to maintain precisely, and there are so many variables.....

BUT by using motor encoder to regulate motor speed or use the distance traveled of the to adjust the motor speed to keep that circle perfect.

 

My control solution is determining the traveled position of each wheel ( which also has to be be at the same ratio of inner circle to outer circle diameter).  if the traveled position of the right side wheel is not as calculated for a perfect circle to what the left wheel has traveled, it's speed reference can be sped up or slowed down, applying a correction to compensate for errors. 

 

 

The Arduino program speeds up or slows down the right hand side wheel speed by 2% when the actual encoder counts are + or - 10 counts

off from calculated value. 

This robot has a MKR1000 for brains, a motor carrier shield for variable speed motor control, and

inputs for the motor encoders.

( For more info on encoders, here is place https://dronebotworkshop.com/rotary-encoders-arduino/  )

image

 

Here is a video of the robot's vigorous circular motion https://youtu.be/Z20punl1SeQ

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

" with a vigorous Circular motion hitherto unknown to the people of this area, but destined To take the place of the mudshark in your mythology

Here it goes, the circular motion, now rub it!" sorry, I couldnt resist exerpt from *** Nanook Rubs It by Frank Zappa ****

 

 

 

The Robot Wheel Diameter inches = 3.5625   

The Robot Wheel circumference inches 11.19181

One turn of the wheel measured 1190 encoder counts (measured value as info on PPR, actual gear ratio or motor top speed is not available)

The robot width (to the centerline of each wheel ) is 3.25 inches.

 

For simple testing, a 12 inch circle diameter was chosen for the robot's path.

The left side wheel path diameter is 13.625 inches, the right side wheel path diameter is 10.375 inches.

The ratio of inner path to outer path is ~  .76146788990825688073394495412844

 

Running a baseline value of speed ratios with the hardware, and the calculated values didnt quite work as calculated.

The motors are so different at the slow speed points being operated at, and the small circle diameter the speed ratio had to be empirically set for .55 ( 11 / 20) 

 

Using the MKRMotorCarrier Arduino library, the motor control is set as an integer PWM Duty Cycle,   -100 to 100. 

1% is the best resolution speed reference that can be written for PWM.

 

 

 

#include <MKRMotorCarrier.h>   

#define INTERRUPT_PIN 6

 

//Variable to store the battery voltage

static int batteryVoltage;

 

//Variable to change the motor speed and direction

static int duty = 50;

int TestRevs=5;

int M3Duty=11;

int M4Duty=20;

int SpeedRef=50;

int M3_Enc1_Counts=0;

int M4_Enc2_Counts=0;

float M3_Enc1_Counts_Float=0;

float M4_Enc1_Counts_Float=0;

 

float CircleDiameterInches = 12.0; ///centerline of tracking diameter

float InnerTrackDiameter = 1.00000;  ///from centerline of tracking diameter

float OuterTrackDiameter = 1.00000;  ///from centerline of tracking diameter

float TrackingSpeedRatio = 1.00000;  ///

float M4_Enc2_CountsFloat=0.00000; // counts converterd to float

float M3_Enc1_CountsFloat=0.00000; // counts converterd to float

float deadbandFloat = 10.0;

int SpeedTrim = 0; // speed trim to the Mx Duty Cycle

 

 

void setup()

{

//  Serial port initialization

  Serial.begin(115200);

//  while (!Serial);

 

  //Establishing the communication with the motor shield

controller.begin();

 

// if (controller.begin())

  //  {

//     Serial.print("MKR Motor Shield connected, firmware version ");

//     Serial.println(controller.getFWVersion());

  //  }

//  else

//   {

     // Serial.println("Couldn't connect! Is the red led blinking? You may need to update the firmware with FWUpdater sketch");

     // while (1);

//    }

 

 

  // Reboot the motor controller; brings every value back to default

// Serial.println("reboot");

  controller.reboot();

  delay(500);

 

 

  // Reset the encoder internal counter to zero (can be set to any initial value)

//  Serial.println("reset counters");

  encoder1.resetCounter(0);

  encoder2.resetCounter(0);

 

  //Take the battery status

//  float batteryVoltage = (float)battery.getConverted();

//  Serial.print("Battery voltage: ");

//  Serial.print(batteryVoltage);

//  Serial.print("V, Raw ");

//  Serial.println(battery.getRaw());

 

delay (3000);

 

/// calculate global tracking constants

float InnerTrackDiameter = (CircleDiameterInches-(1.625*2));  ///from centerline of tracking diameter

float OuterTrackDiameter = (CircleDiameterInches+(1.625*2));  ///from centerline of tracking diameter

float TrackingSpeedRatio = OuterTrackDiameter/InnerTrackDiameter;  /// ratio of wheel travel diameters

 

}

 

void loop() {

 

  //Take the battery status

// float batteryVoltage = (float)battery.getConverted();

// Serial.println("battery = ");

// Serial.println(batteryVoltage);

  M3_Enc1_Counts=encoder1.getRawCount();

  M4_Enc2_Counts=encoder2.getRawCount();

  M3_Enc1_CountsFloat =  M3_Enc1_Counts; // save to a floating point register

  M4_Enc2_CountsFloat =  M4_Enc2_Counts; // save to a floating point register

   // compare Enc2 outer wheel counts to inner wheel counts* speed ratio

      // if inner wheel enc1 has too many counts , then slow down M3Duty

      // if outer wheel enc2 has too many counts, then speed up M3Duty

      // if counts are within a deadband, then M3Duty stays as default

float InnerTrackDiameter = (CircleDiameterInches-(1.625*2));  ///from centerline of tracking diameter

float OuterTrackDiameter = (CircleDiameterInches+(1.625*2));  ///from centerline of tracking diameter

float TrackingSpeedRatio = OuterTrackDiameter/InnerTrackDiameter;  /// ratio of wheel travel diameters

 

 

//    Serial.println("M3_Enc1_CountsFloat=");

//    Serial.println(M3_Enc1_CountsFloat);

//     Serial.println(" ");

//        Serial.println("M4_Enc2_CountsFloat=");

//    Serial.println(M4_Enc2_CountsFloat);

//     Serial.println("");

//     Serial.print("TrackingSpeedRatio=");

//       Serial.println(TrackingSpeedRatio);

 

       // M4 is set faster than M3 . if M4 is 10 encoder counts more than the inner encoder*circle ratio then speed up the inner wheel M3

 

    if ((M4_Enc2_CountsFloat) > ((TrackingSpeedRatio*M3_Enc1_CountsFloat)+ deadbandFloat))

       { SpeedTrim=1; } //slowdown the inner wheel duty cycle

  

       // M4 is set faster than M1 . if M4 is 10 encoder counts less than the inner encoder*circle ratio then slow down the inner wheel M3

 

    else if ((M4_Enc2_CountsFloat) < ((TrackingSpeedRatio*M3_Enc1_CountsFloat)- deadbandFloat))

       { SpeedTrim= -1; } //slowdown the inner wheel duty cycle

 

    else { SpeedTrim= 0; } //if encoder counts are within +- 10 counts, then dont trim M3 speed ref

 

       if (M4_Enc2_Counts < (5211))

   {

    M3.setDuty(M3Duty+SpeedTrim);

    M4.setDuty(M4Duty);

           

                //   Serial.print("Encoder2 Pos [counts]: ");

                //   Serial.println(M4_Enc2_Counts);

                ///Serial.print("Encoder1 Pos [counts]: ");

                //   Serial.println(M3_Enc1_Counts);

                //    delay (10);

   }

else if ((M4_Enc2_Counts >= (5211)) && (M4_Enc2_Counts <(6500)))

    {

    M3.setDuty(0);

    M4.setDuty(0);

    }

    else

      { M3.setDuty(0);

       M4.setDuty(0);

    //Chose the encoder to use:encoder1(default) or encoder2

//   Serial.print("Encoder1 Pos [counts]: ");

//    Serial.println(encoder1.getRawCount());

//    Serial.print("Encoder1 vel [counts/sec]: ");

//   Serial.println(encoder1.getCountPerSecond());

//Serial.print("Encoder2 vel [counts/sec]: ");

//    Serial.println(encoder2.getCountPerSecond());

//   Serial.print("Encoder2 Pos [counts]: ");

//    Serial.println(encoder2.getRawCount());

     delay(5000);

    }

 

 

//  }

 

  //Keep active the communication MKR1000 & MKRMotorCarrier

  //Ping the samd11

  controller.ping();

  //wait

  delay(50);

}

  • Sign in to reply

Top Comments

  • robogary
    robogary over 6 years ago +1
    Wow. You make running in circles sound good.
  • jw0752
    jw0752 over 6 years ago +1
    Hi Gary, I found your experiment and work to get the robot to drive a circle fascinating. It reminded me of a book that I read 27 years ago called "Fuzzy Logic" by Daniel McNeill and Paul Freiberger. It…
Parents
  • jw0752
    jw0752 over 6 years ago

    Hi Gary,

     

    I found your experiment and work to get the robot to drive a circle fascinating. It reminded me of a book that I read 27 years ago called "Fuzzy Logic" by Daniel McNeill and Paul Freiberger. It was a concept of dealing with problems, not in a binary On Off fashion but more in the line of thinking of degrees of On or degrees of Off. The idea was invented in the US by Lotfi Zadeh but more commercially developed by the Japanese. I believe that your approach to solving the circle drive problem falls in the Fuzzy Logic category.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 6 years ago

    Hi Gary,

     

    I found your experiment and work to get the robot to drive a circle fascinating. It reminded me of a book that I read 27 years ago called "Fuzzy Logic" by Daniel McNeill and Paul Freiberger. It was a concept of dealing with problems, not in a binary On Off fashion but more in the line of thinking of degrees of On or degrees of Off. The idea was invented in the US by Lotfi Zadeh but more commercially developed by the Japanese. I believe that your approach to solving the circle drive problem falls in the Fuzzy Logic category.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • robogary
    robogary over 6 years ago in reply to jw0752

    Thanks - Its not quite fuzzy yet :-)  I guess it could be fuzzy if it had 2 levels of error correction with 2 different gains based on how far off the actual tracking position was to the calculated path.