Crazy Arduino Automations
  • Challenges & Projects
  • Project14
  • Crazy Arduino Automations
  • More
  • Cancel
Crazy Arduino Automations
Crazy Arduino Automations Blog Raising the Bridge...Automation with Arduino
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Crazy Arduino Automations to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: colporteur
  • Date Created: 27 Mar 2023 8:22 PM Date Created
  • Views 3783 views
  • Likes 7 likes
  • Comments 23 comments
  • crazyarduinoautomationch
Related
Recommended

Raising the Bridge...Automation with Arduino

colporteur
colporteur
27 Mar 2023

image

This design challenge presented itself at an opportune time. The model railroaders are putting the finishing touches on a bridge that requires some automation.

On the other side of the bridge is a turn-about that the tug (A) needs to reach in order to change direction. I have been asked to create the following automation sequence.

Tug triggers sensor (A) to indicate the bridge needs to raise.

Gate (B) lowers indicate no traffic to enter bridge

Bus (C) stops.

Ramp (D) re-aligns to make room for bridge movement

Bridge (E) raises.

I suspect a button (no letter on the image) on the turn-about side will be required to indicate when the tug has completed it transition and the bridge can be restored.

My initial assessment is two inputs and four outputs.

Inputs

Tug Trigger

Operations Trigger

Outputs

Motor control bridge gate

Power interruption bus

Motor control bridge ramp

Motor control bridge

I am hoping to use a Arduino Uno for the project. If you have an extra to spare you can throw it my way.

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 3 years ago +1
    Bonus points if you can make the bus jump the bridge as it is being raised... 'Blues Brothers' meets 'Speed'.
Parents
  • dougw
    dougw over 3 years ago

    Looks like quite a setup. I've never seen a bus move in a model railroad much less a boat.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to dougw

    The bus is part of a Faller Car System. https://www.faller.de/en/car-system/ Self-powered vehicles steer themselves around the model roads following a steel wire buried just under the surface of the road. Inside the bus is a reed switch that removes power if it encounters magnetic field. The vendor sells and expensive solution for triggering the switch. An earth magnet on an arm attached to a servo motor works just as good and for a lot less.

    The tug is plastic model on a locomotive assembly. The ocean has track that the tug navigates. There is a large barge that the tug pushes and pulls between two loading terminals. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • colporteur
    colporteur over 3 years ago in reply to dougw

    The bus is part of a Faller Car System. https://www.faller.de/en/car-system/ Self-powered vehicles steer themselves around the model roads following a steel wire buried just under the surface of the road. Inside the bus is a reed switch that removes power if it encounters magnetic field. The vendor sells and expensive solution for triggering the switch. An earth magnet on an arm attached to a servo motor works just as good and for a lot less.

    The tug is plastic model on a locomotive assembly. The ocean has track that the tug navigates. There is a large barge that the tug pushes and pulls between two loading terminals.