Crazy Arduino Automations
  • Challenges & Projects
  • Project14
  • Crazy Arduino Automations
  • More
  • Cancel
Crazy Arduino Automations
Crazy Arduino Automations Blog Raising the Bridge...Automation with Arduino: Design Update
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Crazy Arduino Automations to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: colporteur
  • Date Created: 18 May 2023 3:06 PM Date Created
  • Views 3257 views
  • Likes 12 likes
  • Comments 14 comments
  • arduino automation
  • arduino
Related
Recommended

Raising the Bridge...Automation with Arduino: Design Update

colporteur
colporteur
18 May 2023

My automation project has provided some challenges. I’m continuing to work at it, but I needed some design changes to accomplish raising and lowering the bridge automatically without failures.

It has been a while since the challenge was kicked off and an equal amount of time since I made my post. I am working to completing the project before the end of May. Other retirement stuff is taking up my time.

image

The current design divides the layout into four areas A, B, C, & D. The letter designation reference the island side area, B the ramp area, C the bridge area and D mainland side area for descriptions.

Each area has sensors and/or animation devices (i.e. motors, light and sound) referenced by the numbers.

A1: is a magnetic attached to a servomotor. Raising the magnetic stops the vehicle at the approach. The magnet triggers a reed switch in the vehicle to kill power.
A2: is a barrier raised and lowered by a servo.
B1: has a servo that raises and lowers the ramp.
B2: is a magnetic sensor triggered by an earth magnet attached to the ramp to detect if the ramp is up or down.
C1: is an IR sensor to stop the bridge on maximum rise.
C2: is a geared DC motor to raise and lower the bridge (the bride has left the building:))
C3: a magnetic sensor triggered by an earth magnet attached to the bridge to detect if the bridge is up or down.
D1: barrier on mainland side of bridge.
D2: vehicle stop magnet on mainland side of bridge.

My original plan was to use on one Arduino to animate the scenario of sound alarm with lights, lower the barriers, stop the bus, raise the ramp and raise the bridge. Then reverse the scenario. I have since added an Arduino dedicated to managing sensor readings and bridge movement.

I discovered during motor testing to raise and lower the bridge there are many things can go wrong. When little humans (i.e children) are involved a lot more can go wrong. Wrong would cause damage to the structures. To prevent things from going wrong, I added some sensors. The sensors provide feedback to establish logic that can control the bridge's action.

Given sufficient resources, I feel the complete animation could be done with one Arduino. Using Nano’s (i.e. what I have on hand) I have limited I/O pins. Added the additional Nano provided more I/O.

The extra Nano enabled me to divide the animation between two microcontroller devices. One controller is now responsible for the bridge motor guided by sensor readings, the other can look after the servos and playing sound.

I just completed the sensor installs. The other animation devices are in place and working. I have a scenario coding to raise and lower the bridge with the bridge coding section absent. I’ve just started work on coding the bridge up and down sequence. Hopefully without a catastrophic failure.

  • Sign in to reply
Parents
  • dang74
    dang74 over 3 years ago

    "When little humans (i.e children) are involved a lot more can go wrong. Wrong would cause damage to the structures. To prevent things from going wrong, I added some sensors."

    You are so nice.  You opted for sensors when a 'no children allowed' sign would have been so much easier. Wink 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to dang74

    There are both grandchildren and children of the people that visit. The kids are very discovery oriented. They also point by touching. Stopping a moving bridge is a risk I have to anticipate. That is one of the reason I have a code test to confirm the bridge is actually up before doing a down instruction set. "Oh poppy, i lowered the bridge myself" as the motor is trying to drive the deck through the table because it raised the bridge therefore it has to be up. Right?

    I've told the railroad guys it is no different than real life. I suspect the safety protocol involved in raising structures of several tonnes is excessive:) I occasionally read of people being crushed by moving machinery. I pass excavators working in my area all the time. I stop and wait for them to indicate I can pass. I think I might annoy them at times. I figure that bucket coming through my window can't be nice. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to colporteur

    I'm a bit worried about 'C2'

    image

    I suspect that the groom may be as well Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dang74
    dang74 over 3 years ago in reply to beacon_dave

    LOL.  I hadn't noticed the typo earlier.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to colporteur

    If you drive the bridge rotation via a 4-bar linkage then you can limit the possible rotation to 90 degrees. You wouldn't need to reverse the motor as it would automatically start raising after it was fully lowered and start lowering after it was fully raised.

    It perhaps simplifies the control as you just keep driving the motor in the one direction until the appropriate limit switch has been reached.

    If you drive the output shaft through a spring coupling then if anyone tries lowering it manually against the motor it would just give and then spring back to the last motor driven position when released. If the limit switch is on the bridge side of the spring, then your code needs to take into account that it may have been activated in this manner as it would initially stop the motor but upon release, the bridge would no longer be in the lowered state so the motor would have to be turned back on to complete the lowering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 3 years ago in reply to colporteur

    If you drive the bridge rotation via a 4-bar linkage then you can limit the possible rotation to 90 degrees. You wouldn't need to reverse the motor as it would automatically start raising after it was fully lowered and start lowering after it was fully raised.

    It perhaps simplifies the control as you just keep driving the motor in the one direction until the appropriate limit switch has been reached.

    If you drive the output shaft through a spring coupling then if anyone tries lowering it manually against the motor it would just give and then spring back to the last motor driven position when released. If the limit switch is on the bridge side of the spring, then your code needs to take into account that it may have been activated in this manner as it would initially stop the motor but upon release, the bridge would no longer be in the lowered state so the motor would have to be turned back on to complete the lowering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • robogary
    robogary over 3 years ago in reply to beacon_dave

    maybe the bridge can use a small rubber band belt with pulleys on the motor and mechanism to raise and lower the bridge. If someone plays with the bridge manually, the belt will allow mechanical slip with no damage. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to robogary

    Pneumatics might also be another approach.