Crazy Arduino Automations
  • Challenges & Projects
  • Project14
  • Crazy Arduino Automations
  • More
  • Cancel
Crazy Arduino Automations
Crazy Arduino Automations Blog Raising the Bridge...Automation with Arduino: Pin Count
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Crazy Arduino Automations to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: colporteur
  • Date Created: 28 Mar 2023 11:22 PM Date Created
  • Views 3653 views
  • Likes 6 likes
  • Comments 21 comments
  • crazyarduinoautomationch
Related
Recommended

Raising the Bridge...Automation with Arduino: Pin Count

colporteur
colporteur
28 Mar 2023

image

The comments posted from my initial blog entry got me to thinking. Did I size this correctly?

The bridge spans the Mainland to Island. At either end of the bridge is a gate, an area to halt the bus and warning lights flashing when the bridge is closed. In addition to the lights, I've added a warning sound. At one end of the bridge is a ramp that enables the bridge to avoid the road bed as it rises. A trigger to raise the bridge will be the Tug and to lower the bridge the Turn-About. The bridge motor is using a L298 module and the bus halts, gates and ramp are servo motors. All toll I'm counting 14 pins required.

D2 Bridge Up limit
D3~ Ramp Servo
D4 Bridge Down Limit
D5~ Island Gate Servo
D6~ Mainland Gate Servo
D7 Bridge L298 Motor IN2
D8 Bridge L298 Motor IN1
D9~ Bridge L298 Motor EN A
D10~ Island Bus Halt Servo
D11~ Mainland Bus Halt Servo
D12 Warning Sound JQ6500
D13 Tug Sensor
D14 Turn-about Button
D15/A0 Island Warning Light
D16/A1 Mainland Warning Light
  • Sign in to reply
  • beacon_dave
    beacon_dave over 3 years ago

    "...Did I size this correctly?..."

    If not,  "You're going to need a bigger bridge..."  Slight smile

    So I take it that no the bridge lowers briefly whilst the turnaround takes place then opens again once the turnaround is complete and the boat is ready to set sail ?

    How are you doing the logic with single switches either side ? Are you keeping track of the boat direction, toggling based on the current state of the limit switches, or just toggling raise/lower each time you hit a switch and hope you don't ever get out of sync ?

    Do you need to control the points motor so that the boat departs on the other track than it arrives on or does that rely on the railroad team ? I assume it is basically a loop track with a turnaround siding. Likewise, do you need to control the turnaround ?

    Does the LED signage need triggering when the bridge is closed to traffic ?

    Perhaps trigger some sea shanties whilst on the turnaround Notes

     "...You will have a fishy on a little dishy; you will have a fishy when the boat comes in..." Shark

    What's that ? I'm banned from the model railroad club for life ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<