DIY Test Instrumentation
  • Challenges & Projects
  • Project14
  • DIY Test Instrumentation
  • More
  • Cancel
DIY Test Instrumentation
Blog IRRF 2000 the IR and RF Tester
  • Blog
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DIY Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gam3t3ch
  • Date Created: 3 Aug 2021 4:59 AM Date Created
  • Views 2114 views
  • Likes 10 likes
  • Comments 4 comments
  • diytestinstrumentationch
Related
Recommended

IRRF 2000 the IR and RF Tester

gam3t3ch
gam3t3ch
3 Aug 2021

image

 

 

Sometimes there is just no tool that will get the job done quickly and efficiently so sometimes we have to modify an existing tool or create our own to accomplish what we need in much less time then prior methods.

 

I work primarily in medical supplies as a technician for repairing things from scooters to oxygen machines and so on.  One of the things that sticks with me the most is the amount of time I spend trying to test clean and replace IR and RF remotes for devices.  Usually you have to have the device near you to test to see if it will work.  Well in covid times if someones hospital bed remote isn't working it would take us probably a half hour to get gowned up and run through all the tests to be able to see the bed.  Now if it doesn't work and you have to come back more then a few times it can be very wasteful in time.  Plus we want to get the device working for the client the first time so that way their devices they rely on for their day to day mobility needs are met without and big struggles or battles.

 

Thus the IRRF-2000 was born.

 

I wanted something that a client could drop off their remote and I would be able to have a tester to make sure all the buttons where functioning correctly and that way I would just have to drop it off at the front desk if they were in a facility or if at home limit the amount of contact I had with them.

 

So with this I started on a breadboard making my mock up of my circuit which seemed to work then when I was searching around I found a great idea about adding some 1SS86 Diodes to a circuit and it would actual pick up the RF Frequency enough to light a led.  Well I haven't tested it but I thought when I go to design my board that I would add it into my design to add an extra feature so now I would be able to test both IR and RF remotes.  This was a win win in my books.

 

imageimage

 

Assembly List

Label Part Type Properties
100k 100kΩ Resistor pin spacing 400 mil; bands 4; package THT; tolerance ±5%; resistance 100kΩ
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
1SS86 Zener Diode power dissipation 0.5W; package 300 mil [THT]; type Zener; breakdown voltage 3.6V; part # 1N4732A
9V Battery block 9V voltage 9V
IR-LED Red (633nm) LED package 5 mm [THT]; color Red (633nm); leg yes
LM7805 Voltage Regulator - 5V voltage 5V; package TO220 [THT]
RF-LED Red (633nm) LED package 5 mm [THT]; color Red (633nm); leg yes
SWITCH BLOCK Screw terminal - 2 pins pin spacing 0.1in (2.54mm); hole size 1.0mm,0.508mm; package THT; pins 2
TSOP-1738 TSOP312.., 314.. pin spacing 0.1in (2.54mm); row single; package THT; pins 3

 

 

 

image

I really enjoyed this project it taught me a lot. I tossed it in my tool kit at work and the very next day I ended up using it saving me a ton of time in diagnosis of the remote I had brought into me.

well now its on to the full video on this here:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

There will be some more photos and small update on here soon.

 

imageimage

  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +1
    Nice useful project. DAB
  • javagoza
    javagoza over 5 years ago in reply to dubbie +1
    I always use the mobile camera to see if the IR LEDs light up on the remote control.
Parents
  • dubbie
    dubbie over 5 years ago

    This looks useful. Quite recently I was trying to use an IR Tx Rx pairing and I was getting nowhere - they were intelligent modules and only responded to the correct inputs. I had no idea if IR was being produced or not, it was driving me crazy!. Something like this tester would have been useful then.

     

    In the end the solution came to me when sleeping, which I find is a rather unreliable method of fault-finding.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 5 years ago in reply to dubbie

    I always use the mobile camera to see if the IR LEDs light up on the remote control.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • javagoza
    javagoza over 5 years ago in reply to dubbie

    I always use the mobile camera to see if the IR LEDs light up on the remote control.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dubbie
    dubbie over 5 years ago in reply to javagoza

    Enrique,

     

    I've tried this but with the camera I use unless the IR source is pointing directly into the camera it isn't detected (maybe there is too much IR filtering on the camera) and even then it is pretty dim and not easily visible.

     

    Dubbie